As title, we have a bit order now, but stock this problem almost 2 months now, we're worry and feel bad, please help us to fix this problem.
KERNEL: 3.14.52
Platform: IMX7 customer board
OS: Yocto 3.14.52
Camera: OV5640 mipi camera
it's initial success in kernel:
mxc_mipi-csi 30750000.mipi-csi: Registered sensor subdevice: ov5640_mipi 2-003c
camera ov5640_mipi is found
but when I issue this command:
root@imx7dsabresd:~# gst-launch-1.0 imxv4l2src device=/dev/video1 ! imxv4l2sink
====== IMXV4L2SRC: 4.0.8 build on Jan 5 2016 19:59:24. ======
====== IMXV4L2SINK: 4.0.8 build on Jan 5 2016 19:59:24. ======
Setting pipeline to PAUSED ...
display(/dev/fb0) resolution is (800x480).
Pipeline is live and does not need PREROLL ...
Setting pipeline to PLAYING ...
New clock: GstSystemClock
Chandling interrupt.
Interrupt: Stopping pipeline ...
Execution ended after 0:05:02.488665625
Setting pipeline to PAUSED ...
and stock here..... it sometime works, anyway, very unstable.. (this camera works using IMX6 platform)
It works when I using videotestsrc.. Does anyboday has useful debug method??
I also trace the driver, why can't I dump CSICR3 register?
it always show 0x00, dma issue??
I don't want to missing this order, please help us, thank you!
Hi,
I want to bring up the ov5640 mipi camera using imx-warp7 So i have configured the configuration using imx reference guide in menuconfig but I am getting error while building image using bitbake core-image-minimal So is there any configuration has to be made in local.conf file the error logs and reference guide is attached So please find the attachments.
Your suggestions are apreciated Thank you
regards
Vinod
Hi May Queen,
I have seen so many instruction for upgrading the BSP in community but i am not getting which i have to follow So can you please suggest me which are the steps to upgrade the BSP because i am new to the WARP7.
Thanks with regards
Vinod
uh... ok! download the u-boot first.
git clone git://git.freescale.com/imx/uboot-imx.git
then switch to 2015.04 branch
then download the kernel.
git clone git://git.freescale.com/imx/linux-imx.git
switch to 4.1.15_2.0.0 branch
And you can start re-porting again!
Maybe this log has some help to debug??
root@imx7dsabresd:~# v4l2-ctl -d /dev/video1 --all
Driver Info (not using l2):
Driver name : mx6s-csi
Card type : i.MX6S_CSI
Bus info : platform:30710000.csi
Driver version: 3.14.52
Capabilities : 0x04000001
Video Capture
Streaming
Video input : 0 (Camera: ok)
Format Video Capture:
Width/Height : 640/480
Pixel Format : ''
Field : None
Bytes per Line: 0
Size Image : 614400
Colorspace : Unknown (00000000)
Crop Capability Video Capture:
Bunds : Left 0, Top 0, Width 0, Height 0
Default : Left 0, Top 0, Width 0, Height 0
Pixel Aspect: 0/0
Crop: Left 0, Top 0, Width 0, Height 0
Streaming Parameters Video Capture:
Capabilities : timeperframe
Frames per second: 15.000 (15/1)
Read buffers : 0
Hello May,
It is possible that there is something wrong with differential resistance of MIPI on PCB layout, So you can check it !
In addtion , you can also try to reduce resoluton of preview , to see if preview is normal.
If you have i.mx7d evaluation board, you can validate camera on evk at first, The method can help you confirm where the issue is from.
Regards,
Weidong
Thank you weidong:
1. I also think the MIPI signal is unstable, but if it's a HW issue, how can I verify or measure it?
2. How to reduce resolution using gst-launch-1.0, I know default is 640x480 (VGA), the driver also need to modify?
3. I don't have evk board, but the customer board HW design is refer from evk board!
Thank you!
May
Hello May,
for your questions:
1. I also think the MIPI signal is unstable, but if it's a HW issue, how can I verify or measure it?
[weidong] I feel the possibility HW issue is greater. Resistance of MIPI differential signals on PCB should be reviewed at first .
2. How to reduce resolution using gst-launch-1.0, I know default is 640x480 (VGA), the driver also need to modify?
[weidong] if 640x480 was tested and result was not good, don't try to reduce resolution again.
3. I don't have evk board, but the customer board HW design is refer from evk board!
[weidong] EVK board can help you find issue quickly, so i suggest you test the camera on it.
Best Regards,
Weidong