State of iMX28 in Linux 3.x Kernels?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

State of iMX28 in Linux 3.x Kernels?

973 Views
mwill
Contributor I

Greetings all,

Im having a bunch of performance issues using recent 3.x linux kernels (slow uSD, USB, linuxfb, etc performance).

It also appears cpufreq, powersaving, etc functions are not availiable.

Is there any Freescale support/maintenance of the iMX28 in the 3.x kernels, or would i be better off moving back to 2.6.35 with related Freescale patches?

Thanks in advance,

Labels (2)
0 Kudos
5 Replies

688 Views
fabio_estevam
NXP Employee
NXP Employee

Mark,

Which kernel version did you use? It would be nice if you could report the issues you noticed in the linux-arm-kernel mailing list, so that people could be aware of them and eventually fix them.

0 Kudos

688 Views
mwill
Contributor I

I'm using 3.17.4, and have tried a few previous 3.x versions as well.

By "people" im guessing you mean the community, and not Freescale?

0 Kudos

688 Views
fabio_estevam
NXP Employee
NXP Employee

Yes, I mean the community. If you report the issues in details in the mailing lists, then maybe someone can try to fix them.

688 Views
igorpadykov
NXP Employee
NXP Employee

Hi Mark

I think you are right, since officially supported only releases located

on Freescale i.MX product web pages, like below

i.MX28 Evaluation Kit|Freescale

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos

688 Views
mwill
Contributor I

So does that mean Freescale has stopped maintaining Linux support for the iMX2x?

0 Kudos