Sim Card support in IMX6Q sabre SD board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Sim Card support in IMX6Q sabre SD board

495 Views
senthilkumar_s1
Contributor II

Hi, all we are developing solution using IMX6Q sabre SD board. It contains one Sim card Slot. But slot is not working while using android Kitkat and lolipop downloaded from free scale site. We need some help regarding how to use that sim slot,even if some extra hardware is required please mention that also.

Thanks in advance.

Labels (2)
0 Kudos
1 Reply

378 Views
igorpadykov
NXP Employee
NXP Employee

Hi Senthil

that sim slot can be used by usb gsm module (like EM770W)

produced with PCI-e interface.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos