Secure boot verifying bootloader and kernel: Same DTB file in both?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Secure boot verifying bootloader and kernel: Same DTB file in both?

1,283件の閲覧回数
Dial
Contributor I

Hello:

I am trying to set up a secure boot for the bottloader and kernel in the iMX8MP following the instructions in the URL https://source.codeaurora.org/external/imx/uboot-imx/tree/doc/imx/habv4/guides/mx8m_mx8mm_secure_boo...

According to the instructions, a DTB file is required to assembly the signed bootloader:

1.3 Preparing the fit image
----------------------------

The imx-mkimage project is used to combines all the images in a single
flash.bin binary, the following files are required:

- U-Boot:
  u-boot.bin
  u-boot-nodtb.bin
  u-boot-spl.bin
  U-Boot DTB file (e.g. fsl-imx8mq-evk.dtb)

 

But then a DTB file is also required with the kernel, as can be seen in the CSF file in https://source.codeaurora.org/external/imx/uboot-imx/tree/doc/imx/habv4/csf_examples/additional_imag...

[Authenticate Data]
    # Key slot index used to authenticate the image data
    Verification index = 2
    # Authenticate Start Address, Offset, Length and file
    Blocks = 0x80800000 0x00000000 0x006EA000 "zImage", \
	     0x83800000 0x00000000 0x0000B927 "imx7d-sdb.dtb", \
	     0x84000000 0x00000000 0x000425B8 "uTee-7dsdb"

 

Are these DTB files the same file? If not, which are the differences?

 

Thank you very much in advance and best regards.

 

ラベル(1)
タグ(1)
0 件の賞賛
返信
0 返答(返信)