SD/MMC manufacture mode

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SD/MMC manufacture mode

804件の閲覧回数
tsung-chihwang
Contributor III

Hi Yuri,

I was wondering if you could tell me how to do these:
1. How to check the SD/MMC manufacture mode is enabled or not? 

2. How can I read the value of this bit "Disable SDMMC Manufacture mode" on u-boot?

    md 0x470 1?

EIM_Boot_Fusemap.png

BR,

carter

1 返信

688件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

   by default SD/MMC Manufacture Mode is enabled. 

For access to the fuses - base address i.MX 6ULL OCOTP is 0x021B_C000.

So, 0x021B_C470 may be used for read.

Have a great day,
Yuri

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------