RMII Support

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RMII Support

1,974 Views
pelegk
Contributor I

hey,

i want to use 2 RMII channels in MIMXRT1061CVJ5A.

does pin GPIO_B1_00 for example suitable as RX_ER for RMII mode in channel 2?

pastedImage_1.png

as you can see here:

pastedImage_2.png

in channel 1, written so its clear that the io support both modes.

same as EX_ER, the question is about all this pins:

  • REF_CLK - GPIO_B0_15(ALT9).
  • MDC & MDIO - GPIO_B0_00 & GPIO_B0_01  (ALT8).
  • TX0+1 - GPIO_B1_14 & GPIO_B1_14, 2  (ALT8).
  • RX0+1 - GPIO_B1_02& GPIO_B1_01, 2 . (ALT8).
  • CRS - GPIO_B0_10 (ALT8).
  • RX_ER -GPIO_B1_00.(ALT8).
    • TX_EN - GPIO_B0_14. (ALT8).

thank you!

0 Kudos
Reply
1 Reply

1,918 Views
Sabina_Bruce
NXP Employee
NXP Employee

Hello Peleg,

Hope you are doing well.

Yes, the ENET2 has the same functionality as the ENET, with the corresponding pins. The table which describes the external signals only specifies the ENET. However, you can find that all the registers say ENETx_..., this means that the configuration applies to both.

I would recommend to use the table 41-2 as a reference for the mode and description then find the corresponding pin on enet 2.

Best Regards,

Sabina

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

----------------------------------------------------------------------------------------------------------------------- 

0 Kudos
Reply