Hai Sir,
how can build Qt 5.5 latest source code in yocto project for imx6q sabresd board
Hello,
You may build QT5, using FSL L3.14.38 BSP. Please refer to
“Freescale_Yocto_Project_User's_Guide.pdf” in documentation.
http://www.freescale.com/webapp/Download?colCode=L3.14.38_6UL_LINUX_DOCS
Note It may be recommended to use 64-bit Linux host with big amount of memory
(say, ~6GB ).
As an example ;
$ MACHINE=imx6qsabresd source fsl-setup-release.sh –b build-fb –e fb
$ bitbake core-image-minimal
$ bitbake fsl-image-qt5
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------