Problems running U-Boot from USB on i.MX6 Solo

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Problems running U-Boot from USB on i.MX6 Solo

跳至解决方案
887 次查看
ralph__
Contributor IV

Hi, I have a Boundary Devices Nitrogen6 Lite board which I've flashed a bad U-Boot image to (like this: http://boundarydevices.com/i-mx-6dq-u-boot-updates/). I need to recover this bricked device and I read here that the way to do it is connect my PC to the dev board with a USB A/USB A cable. I've done this however I cannot see my dev board when I plug it into my PC.

I have another board with the same CPU (i.MX6 Solo) that does appear on my PC (when I type lsusb) when I plug it into USB however my Nitrogen6 Lite dev board does not appear.

How can I flash a new U-Boot image on if USB doesn't work? I've tried using different combinations of the boot switches but no luck. It looks like the USB bootloader is broken on my board....

Thanks,
Ralph

1 解答
642 次查看
ralph__
Contributor IV

Fixed this now. I was using the USB host port when I should have been using the USB OTG port.

在原帖中查看解决方案

2 回复数
643 次查看
ralph__
Contributor IV

Fixed this now. I was using the USB host port when I should have been using the USB OTG port.

642 次查看
jamesbone
NXP TechSupport
NXP TechSupport

This good news let us know if you need help in anything else!

0 项奖励