Plug usb 3.0 camera into imx8mq get error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Plug usb 3.0 camera into imx8mq get error

983 Views
charleshuang
Senior Contributor II

Hi
BSP : Yocto 4.14.98_2.0.0

I plug an usb 3.0 camera into imx8mqevk board , it will get error as below

[  204.132368] usb usb2-port1: Cannot enable. Maybe the USB cable is bad?

[  205.808374] usb usb2-port1: Cannot enable. Maybe the USB cable is bad?

Could you tell me how to fix this issue?

Labels (1)
Tags (1)
0 Kudos
4 Replies

882 Views
charleshuang
Senior Contributor II

Hi

But we have already test different cable as below

USB 3.0 cable(3m/50cm) , it's fail

Then we insert USB 3.0 HDD, it's okay

And we test the camera on i.MX 8X , it's work well

Are there any other suggestions?

thanks

0 Kudos

882 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello Charles,

I have verified USB 3.0 device connecting to USB 3.0 port on MX8M, there is no problem, it worked normally.

 

Probably there is problem with USB cable, we have several USB cables, some can work, but some cannot. and that error appears.

Regards

0 Kudos

255 Views
solve_this
Contributor II
 
0 Kudos

252 Views
solve_this
Contributor II

Did you solve this one brother

0 Kudos