Playback Video of 1080p @ 30fps on 2 Video ports of I.MX6Q

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Playback Video of 1080p @ 30fps on 2 Video ports of I.MX6Q

521 Views
pratik0403
Contributor I

Hi,

We have a requirement where, We want to play two video of resolution 1080p @ 30fps (worst case 1080p @ 24fps) on two different video ports (which are connected to two different LCDs) simultaneously.

So, My first question would be, Is this possible to playback 2 videos of 1080p simultaneously on two different port?

If that is possible then, Which of the below option is feasible or supported?

1) Using two RGB ports.

2) Using 1 RGB and 1 dual LVDS port.

Video type of 1080p @ 30fps is h264 for which we want to perform above operation.

Thanks,

Pratik

0 Kudos
1 Reply

412 Views
Yuri
NXP Employee
NXP Employee

Hello,

  Please refer to the following Dual 1080p video playback in sabresd-imx6d 

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos