Non used LDO in MMPF0100 F3

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Non used LDO in MMPF0100 F3

559 次查看
semirfazlagic
Contributor III

In our IMX6 design we will use MMPF0100F3  (OTP)

I have two questions:

1) What about non used LDO ? I don't need all 6 LDO.

My space is critic and I want to eliminate as more as possible components

(for example CAP in and CAP out).

For example I need only VGEN4 , Can I simple not mount input and output CAP

for all other LDO.

2) for MMPF0100F3ANES in preprogrammed OTP configuration for some LDO

(VGEN2,VGEN3,VGEN6)  in field "default voltage" we gave  sign "-".

Does it mean that default these LDO are disabled ?

Thank in advance

标签 (2)
标记 (1)
0 项奖励
1 回复

469 次查看
art
NXP Employee
NXP Employee

1) For the information on the MMPF0100 unused pins connection, please refer to the Table 1 of the AN4717 Rev.3.0 App Note document, available on the MMPF0100 Documentation web page:

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=MMPF0100&nodeId=01435974404881F744&fp...

2) The "-" status of the MMPF0100 power supplies in the "Start-up configuration" table of the MMPF0100 Data Sheet document means that these supplies are not turned on during initial start-up. They can be turned on in software later.

Have a great day,

Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励