Hi NXP,
I'm working in a project where I need to send the sensor data from i.MX 8M Mini EVKB to ESP32 module. I enabled Bluetooth in IMX8 and can able to connect it with my mobile. But when I try to connect it to ESP32 it shows error like this in linux terminal.
Attempting to connect to 7C:9E:BD:35:F2:7A
[CHG] Device 7C:9E:BD:35:F2:7A Connected: yes
[CHG] Device 7C:9E:BD:35:F2:7A ServicesResolved: yes
Failed to connect: org.bluez.Error.NotAvailable
[CHG] Device 7C:9E:BD:35:F2:7A ServicesResolved: no
[CHG] Device 7C:9E:BD:35:F2:7A Connected: no
I can able to pair and trust my ESP32 but can't able to establish a connection in between them.
So, can you guys please help me how to connect and exchange the data between imx8 and ESP32
note: I need to implement in my project ASAP.