Nand Flash in IMX6ULL EVK

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Nand Flash in IMX6ULL EVK

4,534 Views
crcn
Contributor I

Hi,

I'm using IMX6ULL EVK and mount one Nand Flash (TC58NVG2SOHTA00).

By default the kit have mounted the SDcard and one NOR.

To support the nand:

   >> add UBOOT_CONFIG = "nand" to local.conf.

   >> change imx6ull-14x14-evk.dts

&gpmi {

pinctrl-names = "default";
    pinctrl-0 = <&pinctrl_gpmi_nand_1>;
    status = "okay";
    nand-on-flash-bbt;
  };

 

&iomuxc {
    imx6ull-evk-gpmi-rework {
        pinctrl_gpmi_nand_1: gpmi-nand-1 {
            fsl,pins = <
                MX6UL_PAD_NAND_CLE__RAWNAND_CLE         0xb0b1
                MX6UL_PAD_NAND_ALE__RAWNAND_ALE         0xb0b1
                MX6UL_PAD_NAND_WP_B__RAWNAND_WP_B       0xb0b1
                MX6UL_PAD_NAND_READY_B__RAWNAND_READY_B 0xb000
                MX6UL_PAD_NAND_CE0_B__RAWNAND_CE0_B     0xb0b1
                MX6UL_PAD_NAND_CE1_B__RAWNAND_CE1_B     0xb0b1
                MX6UL_PAD_NAND_RE_B__RAWNAND_RE_B       0xb0b1
                MX6UL_PAD_NAND_WE_B__RAWNAND_WE_B       0xb0b1
                MX6UL_PAD_NAND_DATA00__RAWNAND_DATA00   0xb0b1
                MX6UL_PAD_NAND_DATA01__RAWNAND_DATA01   0xb0b1
                MX6UL_PAD_NAND_DATA02__RAWNAND_DATA02   0xb0b1
                MX6UL_PAD_NAND_DATA03__RAWNAND_DATA03   0xb0b1
                MX6UL_PAD_NAND_DATA04__RAWNAND_DATA04   0xb0b1
                MX6UL_PAD_NAND_DATA05__RAWNAND_DATA05   0xb0b1
                MX6UL_PAD_NAND_DATA06__RAWNAND_DATA06   0xb0b1
                MX6UL_PAD_NAND_DATA07__RAWNAND_DATA07   0xb0b1
            >;
        };
    };
};

 

I program the micro with MFG TOOLS, and I have this debug in uboot:

 

U-Boot 2016.03-imx_v2016.03_4.1.15_2.0.0_ga+g0ec2a01 (Jun 16 2017 - 14:51:48 +0200)

CPU: Freescale i.MX6ULL rev1.0 at 396MHz
CPU: Commercial temperature grade (0C to 95C) at 43C
Reset cause: POR
Board: MX6ULL 14x14 EVK
I2C: ready
DRAM: 512 MiB
NAND: 512 MiB
MMC: FSL_SDHC: 0, FSL_SDHC: 1
cannot support the NAND, missing necessary info
Display: TFT43AB (480x272)
Video: 480x272x24
In: serial
Out: serial
Err: serial
Net: FEC1
Normal Boot
Hit any key to stop autoboot: 0

 

Why u-boot don't recognize the nand (cannot support the NAND, missing necessary info)?

 

Another question, the environments variables from u-boot are saved in address 0x3c00000 (by default).

I need to change one of them in userspace, so I try to install u-boot-fw-utils and have this error:

Can't find default configuration "arch/../configs/mx6ull_14x14_evk_nand_defconfig"!

It seems that u-boot-fw-utils don support imx6ull? It's true?

 

So I tried to read/write the flash in that direction (nanddump and nandwrite command) and I see correct values until position 0x3c000200. After this position the data seems to be corrupted. See attachment..

 

If read/write in another direction (for example 0x3e000000) I don't have this issue. Why this happens?

 

Thanks.

 

 

 

 

 

Original Attachment has been moved to: imx6ull-14x14-evk.dts.zip

Labels (2)
0 Kudos
Reply
2 Replies

1,993 Views
igorpadykov
NXP Employee
NXP Employee

Hi

please verify that this nand record is present in uboot/drivers/mtd/nand/nand_ids.c,

for mx6ull_14x14_evk_nand_defconfig please check

http://git.freescale.com/git/cgit.cgi/imx/uboot-imx.git/tree/configs?h=imx_v2016.03_4.1.15_2.0.0_ga&...
http://git.freescale.com/git/cgit.cgi/imx/uboot-imx.git/tree/configs/mx6ull_14x14_evk_nand_defconfig...

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,993 Views
crcn
Contributor I

Resolved.

I need to put in uboot/mtd/drivers/nand/nand_ids.c this:

{"TC58NVG2S0H 4G 3.3V 8-bit",
{ .id = {0x98, 0xdc, 0x90, 0x26, 0x76, 0x16, 0x08, 0x00} },
SZ_4K, SZ_512, SZ_256K, 0, 8, 256, NAND_ECC_INFO(8, SZ_512) },

Thanks.

0 Kudos
Reply