Nand Flash Controller Driver for iMX257PDK 3stack

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Nand Flash Controller Driver for iMX257PDK 3stack

1,106件の閲覧回数
ZaheerAhmad
Contributor II

Hi,

I am developing my own nand flash controller driver for iMX257PDK and having some issue while reading a page. I am using the default development board. It has K9LBG08U0D-PCB0:

 

1 Page = (4K + 218)Bytes

1 Block = (4K + 218)B x 128 Pages = (512K +27.25K) Bytes

1 Device = (4K + 218)B x 128 Pages x 8,192 Blocks = 34,512 Mbits

1,024K Pages = 8,192 Blocks

 

I have configured the NFC controller and implemented the read/write page APIs. Right now I am able to write 1 page and read it successfully but I am getting ECC errors (ECC_STATUS_RESULT1, ECC_STATUS_RESULT2) when trying to read the second page of same block. 95% data I read is correct but read page operation disturb some bytes thats why NFC return ECC error (0xFFFF) in both status registers. 

 

Is there any chip errata for NFC? 

 

WinCE has implemented SwapBBI function and it has the following comments for this function:

/ *This function implements the BBI(Bad Block Information) swap workaround for the NFC design flaw. */

Please tell me what is meant by this flaw in NFC design?

タグ(1)
0 件の賞賛
返信
0 返答(返信)