Meaning of PCIe RC reg RESR error Multiple ERR_COR Received

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Meaning of PCIe RC reg RESR error Multiple ERR_COR Received

669件の閲覧回数
shefft
Contributor IV

iMX6SDL, single core

In the RC mode register RESR at 1FF_C130h I'm seeing a multiple ERR_COR Received being reported, but what does that mean and how can I trouble shoot?  This error does not appear with the same HW running the working Linux pcie driver (and endpoint).  The PL DEBUG1 register shows xmlh_training_rst_n LTSSM-negotiated link reset is set, continually.

ラベル(2)
0 件の賞賛
1 返信

579件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Tyler

error is described in sect.48.3.5.2 PCIe Baseline Capability  i.MX6DQ RM

http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6DQRM.pdf

Reporting of errors by a downstream port to the RC is achieved by sending an error message. The decision

to send an error message is controlled by a complex set of associated control and status bits. For more

details, see the flow diagram in Section 6.2.6, “Error Message Controls” of the PCI Express Base 3.0

Specification, revision 1.0. Messages sent to the RC are of the ERR_CORR, ..

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛