Marvell 88W8787 module support for Wi-Fi over SDIO Interface with i.Mx6Q

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Marvell 88W8787 module support for Wi-Fi over SDIO Interface with i.Mx6Q

2,426件の閲覧回数
nanjundam
Contributor II

Hi,

I'm using Taiyo Yuden module WYSBMVGX4 (which has Marvell SoC 88W8787 module integrated), for Wifi interface with i.Mx6Q (MCIMX6Q6AVT10AD) over SDIO interface.

Has anybody used WYSBMVGX4 module for interfacing the with i.Mx6Q for Wifi interface ?

Does it support i.Mx6Q for Linux OS ??

Can anybody please help me with details.

ラベル(4)
0 件の賞賛
返信
2 返答(返信)

1,146件の閲覧回数
igorpadykov
NXP Employee
NXP Employee
0 件の賞賛
返信

1,146件の閲覧回数
weidong_sun
NXP TechSupport
NXP TechSupport

Hello Nanjunda,

      You should port your WIFI to i.MX6Q linux BSP. For hardware, there are 4 uSDHC ports, you select one to connect your WIFI. By default, on evaluation board, your wifi is not supported in BSP, but don't worry about it.

(1) Ask for WIFI driver from your provider

(2) add GPIO control signals on your circuit to BSP file.( For example, power control, wakeup control etc)

(3) add the driver to linux kernel and compile it as a module(.ko)

(4) use modprobe xxx.ko / insmod xxx.ko to load wifi driver.

(5) test steps

--using wpa_supplicant & wpa_cli to debug your wifi .

or

--using wireless-tools to debug it.(you can download latest source code and compile it)

Regards,

Weidong

0 件の賞賛
返信