Marvell 88W8787 module support for Wi-Fi over SDIO Interface with i.Mx6Q

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Marvell 88W8787 module support for Wi-Fi over SDIO Interface with i.Mx6Q

2,304 次查看
nanjundam
Contributor II

Hi,

I'm using Taiyo Yuden module WYSBMVGX4 (which has Marvell SoC 88W8787 module integrated), for Wifi interface with i.Mx6Q (MCIMX6Q6AVT10AD) over SDIO interface.

Has anybody used WYSBMVGX4 module for interfacing the with i.Mx6Q for Wifi interface ?

Does it support i.Mx6Q for Linux OS ??

Can anybody please help me with details.

0 项奖励
2 回复数

1,024 次查看
igorpadykov
NXP Employee
NXP Employee
0 项奖励

1,024 次查看
weidong_sun
NXP TechSupport
NXP TechSupport

Hello Nanjunda,

      You should port your WIFI to i.MX6Q linux BSP. For hardware, there are 4 uSDHC ports, you select one to connect your WIFI. By default, on evaluation board, your wifi is not supported in BSP, but don't worry about it.

(1) Ask for WIFI driver from your provider

(2) add GPIO control signals on your circuit to BSP file.( For example, power control, wakeup control etc)

(3) add the driver to linux kernel and compile it as a module(.ko)

(4) use modprobe xxx.ko / insmod xxx.ko to load wifi driver.

(5) test steps

--using wpa_supplicant & wpa_cli to debug your wifi .

or

--using wireless-tools to debug it.(you can download latest source code and compile it)

Regards,

Weidong

0 项奖励