I've got a Buildroot-based system running on my iMX Solo evaluation board.
I have Gstreamer installed along with all the iMX libs and iMX patches applied to Buildroot as per Buildroot (busybox) - [PATCH 0/14 v3] freescale: update userspace packages (branch yem/fsl-imx)
Whenever I run gstreamer to try and play back an MP3 I get this output (N.B. My GST_PLUGIN_PATH has been set up correctly):
gplay /usr/sample.mp3
(gst-plugin-scanner:216): GStreamer-CRITICAL **: gst_element_class_add_pad_template: assertion 'GST_IS_PAD_TEMPLATE (templ)' failed
(gst-plugin-scanner:216): GStreamer-WARNING **: Failed to load plugin '/usr/lib/gstreamer-0.10/libmfw_gst_h264dec.so': lib_H264_dec_arm11_elinux.so.2: cannot open shared object file: No such file or directory
MAX resolution 1920x1080
(gst-plugin-scanner:216): GStreamer-WARNING **: Failed to load plugin '/usr/lib/gstreamer-0.10/libmfw_gst_audio_pp.so': lib_peq_arm11_elinux.so.1: cannot open shared object file: No such file or directory
(gst-plugin-scanner:216): GStreamer-CRITICAL **: gst_element_class_add_pad_template: assertion 'GST_IS_PAD_TEMPLATE (templ)' failed
(gst-plugin-scanner:216): GStreamer-WARNING **: Failed to load plugin '/usr/lib/gstreamer-0.10/libmfw_gst_mpeg4aspdec.so': lib_MPEG4ASP_dec_arm11_elinux.so.1: cannot open shared object file: No such file or directory
(gst-plugin-scanner:216): GStreamer-WARNING **: Failed to load plugin '/usr/lib/gstreamer-0.10/libmfw_gst_mp3enc.so': lib_mp3_enc_arm12_elinux.so.2: cannot open shared object file: No such file or directory
(gst-plugin-scanner:216): GStreamer-WARNING **: Failed to load plugin '/usr/lib/gstreamer-0.10/libmfw_gst_mpeg2dec.so': lib_mpeg2_dec_arm11_elinux.so.2: cannot open shared object file: No such file or directory
(gst-plugin-scanner:216): GStreamer-WARNING **: Failed to load plugin '/usr/lib/gstreamer-0.10/libmfw_gst_amrdec.so': lib_nb_amr_dec_arm9_elinux.so.2: cannot open shared object file: No such file or directory
(gst-plugin-scanner:216): GStreamer-WARNING **: Failed to load plugin '/usr/lib/imx-mm/audio-codec/lib_src_ppp_arm11_elinux.so': /usr/lib/imx-mm/audio-codec/lib_src_ppp_arm11_elinux.so: undefined symbol: src_up2_prefilter_proc
(gst-plugin-scanner:216): GStreamer-WARNING **: Failed to load plugin '/usr/lib/imx-mm/audio-codec/wrap/lib_vorbisd_wrap_arm12_elinux.so': lib_oggvorbis_dec_arm11_elinux.so.2: cannot open shared object file: No such file or directory
(gst-plugin-scanner:216): GStreamer-WARNING **: Failed to load plugin '/usr/lib/imx-mm/audio-codec/wrap/lib_mp3d_wrap_arm12_elinux.so': lib_mp3_dec_arm12_elinux.so.2: cannot open shared object file: No such file or directory
(gst-plugin-scanner:216): GStreamer-WARNING **: Failed to load plugin '/usr/lib/imx-mm/audio-codec/wrap/lib_aacd_wrap_arm11_elinux.so': lib_aac_dec_arm11_elinux.so.3: cannot open shared object file: No such file or directory
(gst-plugin-scanner:216): GStreamer-WARNING **: Failed to load plugin '/usr/lib/imx-mm/audio-codec/wrap/lib_aacd_wrap_arm12_elinux.so': lib_aac_dec_arm12_elinux.so.3: cannot open shared object file: No such file or directory
(gst-plugin-scanner:216): GStreamer-WARNING **: Failed to load plugin '/usr/lib/imx-mm/audio-codec/wrap/lib_aacd_wrap_arm9_elinux.so': lib_aac_dec_arm9_elinux.so.3: cannot open shared object file: No such file or directory
(gst-plugin-scanner:216): GStreamer-WARNING **: Failed to load plugin '/usr/lib/imx-mm/audio-codec/wrap/lib_vorbisd_wrap_arm11_elinux.so': lib_oggvorbis_dec_arm11_elinux.so.2: cannot open shared object file: No such file or directory
(gst-plugin-scanner:216): GStreamer-WARNING **: Failed to load plugin '/usr/lib/imx-mm/audio-codec/wrap/lib_mp3d_wrap_arm9_elinux.so': lib_mp3_dec_arm9_elinux.so.2: cannot open shared object file: No such file or directory
(gst-plugin-scanner:216): GStreamer-WARNING **: Failed to load plugin '/usr/lib/imx-mm/audio-codec/wrap/lib_mp3d_wrap_arm11_elinux.so': lib_mp3_dec_arm11_elinux.so.2: cannot open shared object file: No such file or directory
(gst-plugin-scanner:216): GStreamer-WARNING **: Failed to load plugin '/usr/lib/gstreamer-0.10/libmfw_gst_h264dec.so': lib_H264_dec_arm11_elinux.so.2: cannot open shared object file: No such file or directory
(gst-plugin-scanner:216): GStreamer-WARNING **: Failed to load plugin '/usr/lib/gstreamer-0.10/libmfw_gst_audio_pp.so': lib_peq_arm11_elinux.so.1: cannot open shared object file: No such file or directory
(gst-plugin-scanner:216): GStreamer-WARNING **: Failed to load plugin '/usr/lib/gstreamer-0.10/libmfw_gst_mpeg4aspdec.so': lib_MPEG4ASP_dec_arm11_elinux.so.1: cannot open shared object file: No such file or directory
(gst-plugin-scanner:216): GStreamer-WARNING **: Failed to load plugin '/usr/lib/gstreamer-0.10/libmfw_gst_mp3enc.so': lib_mp3_enc_arm12_elinux.so.2: cannot open shared object file: No such file or directory
(gst-plugin-scanner:216): GStreamer-WARNING **: Failed to load plugin '/usr/lib/gstreamer-0.10/libmfw_gst_mpeg2dec.so': lib_mpeg2_dec_arm11_elinux.so.2: cannot open shared object file: No such file or directory
(gst-plugin-scanner:216): GStreamer-WARNING **: Failed to load plugin '/usr/lib/gstreamer-0.10/libmfw_gst_amrdec.so': lib_nb_amr_dec_arm9_elinux.so.2: cannot open shared object file: No such file or directory
(gst-plugin-scanner:218): GStreamer-WARNING **: Failed to load plugin '/usr/lib/gstreamer-0.10/libmfw_gst_mpeg2dec.so': lib_mpeg2_dec_arm11_elinux.so.2: cannot open shared object file: No such file or directory
(gst-plugin-scanner:218): GStreamer-WARNING **: Failed to load plugin '/usr/lib/gstreamer-0.10/libmfw_gst_amrdec.so': lib_nb_amr_dec_arm9_elinux.so.2: cannot open shared object file: No such file or directory
playbin2 is employed!
fsl_player_init(): Successfully initialize!
fsl_player_set_media_location(): filename=/usr/sample.mp3
[Stopped ][Vol=01][00:00:00/00:00:00][fps:0]state change failed from 2 to 4
try to play failed
FSL_PLAYER_01.00_LINUX build on Sep 29 2014 22:06:59
[h]display the operation Help
[p]Play
[s]Stop
[e]Seek
[a]Pause when playing, play when paused
[v]Volume
[m]Switch to mute or not
[>]Play next file
[<]Play previous file
[r]Switch to repeated mode or not
[f]Set full screen or not
[z]resize the width and height
[t]Rotate
[c]Setting play rate
[i]Display the metadata
[x]eXit
[Stopped ][Vol=01][00:00:00/00:00:00][fps:0] Aborted by signal[2] Interrupt...
FSL_PLAYER_UI_MSG_EXIT
fsl_player_stop()
player_exit(): No more multimedia files, exit.
Aborted by signal[2] Interrupt...
Aborted by signal[2] Interrupt...
Aborted by signal[2] Interrupt...
Aborted by signal[2] Interrupt...
g_main_loop_thread_fun() quit!
fsl_player_deinit
When I run gst-inspect-0.10 I get:
# gst-inspect-0.10 | grep imx
beep.imx: ac3: ac3
beep.imx: 3ca: ac3
beep.imx: beepdec: beep audio decoder
isink.imx: mfw_isink: IPU-based video sink
tvsrc.imx: tvsrc: v4l2 based tv src
vpu.imx: vpudec: VPU-based video decoder
vpu.imx: vpuenc: VPU-based video encoder
aiur.imx: webm: webm
aiur.imx: aiurdemux: aiur universal demuxer
ipucsc.imx: mfw_ipucsc: IPU-based video converter
v4lsrc.imx: mfw_v4lsrc: v4l2 based camera src
v4lsink.imx: mfw_v4lsink: v4l2 video sink
But most people seem to have beep.mp3 there too. Any idea why it isn't there?
Finally, here is my list of blacklisted plugins in case it helps anyone diagnose my problem:
# gst-inspect-0.10 -b
Blacklisted files:
libmfw_gst_amrdec.so
libmfw_gst_mpeg2dec.so
libmfw_gst_mp3enc.so
libmfw_gst_mpeg4aspdec.so
libmfw_gst_audio_pp.so
libmfw_gst_h264dec.so
lib_g.729ab_dec_arm11_elinux.so
lib_g.723.1_dec_arm11_elinux.so
lib_wb_amr_dec_arm9_elinux.so
lib_g.726_enc_arm11_elinux.so
lib_mp3_enc_arm9_elinux.so
lib_g.726_dec_arm11_elinux.so
lib_mp3_dec_arm12_elinux.so
lib_mp3_dec_arm9_elinux.so
lib_g.729ab_enc_arm11_elinux.so
lib_g.711_dec_arm11_elinux.so
lib_bsac_dec_arm11_elinux.so
lib_g.723.1_dec_arm9_elinux.so
lib_mp3d_wrap_arm11_elinux.so
lib_mp3d_wrap_arm9_elinux.so
lib_vorbisd_wrap_arm11_elinux.so
lib_aacd_wrap_arm9_elinux.so
lib_aacd_wrap_arm12_elinux.so
lib_aacd_wrap_arm11_elinux.so
lib_mp3d_wrap_arm12_elinux.so
lib_vorbisd_wrap_arm12_elinux.so
lib_sbc_enc_arm11_elinux.so
lib_g.711_enc_arm11_elinux.so
lib_nb_amr_enc_arm9_elinux.so
lib_g.729ab_dec_arm9_elinux.so
lib_peq_arm11_elinux.so
lib_g.726_enc_arm9_elinux.so
lib_nb_amr_dec_arm11_elinux.so
lib_g.711_dec_arm9_elinux.so
lib_g.726_dec_arm9_elinux.so
lib_aac_dec_arm12_elinux.so
lib_g.729ab_enc_arm9_elinux.so
lib_wb_amr_enc_arm9_elinux.so
lib_g.723.1_enc_arm11_elinux.so
lib_mp3_enc_arm12_elinux.so
lib_nb_amr_enc_arm11_elinux.so
lib_flac_dec_arm9_elinux.so
lib_oggvorbis_dec_arm11_elinux.so
lib_src_ppp_arm11_elinux.so
lib_nb_amr_dec_arm9_elinux.so
lib_g.723.1_enc_arm9_elinux.so
lib_aac_dec_arm9_elinux.so
lib_aac_dec_arm11_elinux.so
lib_flac_dec_arm11_elinux.so
lib_sbc_enc_arm9_elinux.so
lib_mp3_dec_arm11_elinux.so
lib_mp3_enc_arm11_elinux.so
lib_g.711_enc_arm9_elinux.so
lib_gif_dec_arm11_elinux.so
lib_MPEG4ASP_dec_arm11_elinux.so
lib_H264_dec_arm11_elinux.so
lib_jpeg_dec_arm11_elinux.so
lib_H264_dec_arm9_elinux.so
lib_bmp_dec_arm11_elinux.so
lib_MPEG4ASP_dec_arm9_elinux.so
lib_png_dec_arm11_elinux.so
lib_jpeg_enc_arm11_elinux.so
lib_mpeg2_dec_arm11_elinux.so
lib_deinterlace_arm11_elinux.so
lib_jpeg_dec_arm9_elinux.so
Many thanks.
Ralph
已解决! 转到解答。
I've finally got this working after a somewhat epic struggle.
Basically, the gst-fsl-plugins 3.0.11 makefile was not including the mp3decoder directory when it was being built and so.... the mp3 decoder never got built.
After this it was just a matter of getting the build dependencies right between qt and the gstreamer packages.
In the end, beepdec.mp3 was not the correct mp3 plugin to use and in fact the correct plugin to use was mfw_mp3decoder. I have no idea why other people are using this beepdec.mp3 plugin as it seems deprecated.
Finally, I had wrong paths in my beep_registry.arm12.cf file. Slightly confusing how this was required even though I wasn't using the beepdec.mp3 codec.
Hello Ralph,
Besides checking the gstreamer group I would recommend checking which BSP and images are showing the complete list to compare and determine where the difference may rely. There are some considering differences between the Community BSP and the BSP Release as I mentioned but also on packages available on each image.
Let us know if you are able to compare these images with the correct plugin list!
I managed to get mp3s playing using an old Yocto image:
http://boundarydevices.com/yocto-kernel-3-10-17-beta/#comment-591212
which is a start.
I then went back to my own build system and through much googling realised that the Makefile for gst-fsl-plugins was missing some important paths for MP3 decode.
In gst-fsl-plugins/Makefile.am, I added MP3DEC_DIR to line 930 (below the "if PLATFORM_IS_MX6" line):
SUBDIRS = $(AUDIODIRS) $(LIBSDIRS) $(BASEDIRS) $(VPUWRAPDIRS) $(WMA8ENC_DIR) $(MP3ENC_DIR) $(MP3DEC_DIR) \
$(H264DEC_DIR) $(MPEG2DEC_DIR) $(MPEG4DEC_DIR) $(WMV9MPDEC_DIR) $(WMV78DEC_DIR) \
$(DOWNMIX_DIR) $(AMRDEC_DIR) $(IPUDIRS) $(TOOLDIRS)
When I rebuilt and rebooted the system I now had "beepdec.mp3" listed in my plugins using gst-inspect-0.10. The output from gst-inspect-0.10 beepdec.mp3 was even identical to the output on the working Yocto image system, except the codec version number had increased from 3.0.10 (on Yocto) to 3.0.11 on my system.
# gst-inspect-0.10 beepdec.mp3
Factory Details:
Long name: MP3 decoder
Class: Codec/Decoder/Audio
Description: Decode MP3 compressed audio to raw data
Author(s): Multimedia Team <shmmmw@freescale.com>
Rank: secondary + 2 (130)
Plugin Details:
Name: beep.imx
Description: universal audio codec
Filename: /usr/lib/gstreamer-0.10/libmfw_gst_beep.so
Version: 3.0.11
License: LGPL
Source module: gst-fsl-plugins
Binary package: Freescle Gstreamer Multimedia Plugins
Origin URL: http://www.freescale.com
GObject
+----GstObject
+----GstElement
+----GstBeepdec1
Pad Templates:
SINK template: 'sink'
Availability: Always
Capabilities:
audio/mpeg
mpegversion: 1
SRC template: 'src'
Availability: Always
Capabilities:
audio/x-raw-int
width: { 16, 24, 32 }
depth: { 16, 24, 32 }
rate: { 7350, 8000, 11025, 12000, 16000, 22050, 24000, 32000, 44100, 48000, 64000, 88200, 96000 }
channels: [ 1, 8 ]
Element Flags:
no flags set
Element Implementation:
Has change_state() function: gst_beepdec_state_change
Element has no clocking capabilities.
Element has no indexing capabilities.
Element has no URI handling capabilities.
Pads:
SRC: 'src'
Implementation:
Has custom eventfunc(): gst_pad_event_default
Has custom queryfunc(): gst_pad_query_default
Provides query types:
(2): duration (Total duration)
Has custom iterintlinkfunc(): gst_pad_iterate_internal_links_default
Has getcapsfunc(): gst_pad_get_fixed_caps_func
Has acceptcapsfunc(): gst_pad_acceptcaps_default
Pad Template: 'src'
SINK: 'sink'
Implementation:
Has chainfunc(): gst_beepdec_chain
Has custom eventfunc(): gst_beepdec_sink_event
Has custom queryfunc(): gst_pad_query_default
Has custom iterintlinkfunc(): gst_pad_iterate_internal_links_default
Has setcapsfunc(): gst_beepdec_setcaps
Has acceptcapsfunc(): gst_pad_acceptcaps_default
Pad Template: 'sink'
Element Properties:
name : The name of the object
flags: readable, writable
String. Default: "beepdec10"
resync-threshold : set threshold for resync timestamp: -1, disable resync
flags: readable, writable
Integer64. Range: -1 - 9223372036854775807 Default: 2000000000
reset-when-resync : enable/disable reset when resync
flags: readable, writable
Boolean. Default: true
set-layout : enable/disable set output channel layout
flags: readable, writable
Boolean. Default: true
Sadly, I still can't play back MP3s using gplay (or using Qt for that matter). Here is the output:
# gplay /usr/sample.mp3
playbin2 is employed!
fsl_player_init(): Successfully initialize!
fsl_player_set_media_location(): filename=/usr/sample.mp3
[Stopped ][Vol=01][00:00:00/00:00:00][fps:0]state change failed from 2 to 4
try to play failed
get GST_MESSAGE_ELEMENT missing-plugin, type=(string)decoder, detail=(GstCaps)application/x-id3, name=(string)"ID3\ tag\ demuxer";
Debug: gstdecodebin2.c(3576): gst_decode_bin_expose (): /GstPlayBin2:playbin0/GstURIDecodeBin:uridecodebin0/GstDecodeBin2:decodebin20:
no suitable plugins found
Error: Your GStreamer installation is missing a plug-in.
fsl_player_stop()
FSL_PLAYER_UI_MSG_INTERNAL_ERROR: internal error message received.
fsl_player_stop()
player_exit(): No more multimedia files, exit.
FSL_PLAYER_01.00_LINUX build on Oct 27 2014 19:42:55
[h]display the operation Help
[p]Play
[s]Stop
[e]Seek
[a]Pause when playing, play when paused
[v]Volume
[m]Switch to mute or not
[>]Play next file
[<]Play previous file
[r]Switch to repeated mode or not
[f]Set full screen or not
[z]resize the width and height
[t]Rotate
[c]Setting play rate
[i]Display the metadata
[x]eXit
g_main_loop_thread_fun() quit!
fsl_player_deinit
I've finally got this working after a somewhat epic struggle.
Basically, the gst-fsl-plugins 3.0.11 makefile was not including the mp3decoder directory when it was being built and so.... the mp3 decoder never got built.
After this it was just a matter of getting the build dependencies right between qt and the gstreamer packages.
In the end, beepdec.mp3 was not the correct mp3 plugin to use and in fact the correct plugin to use was mfw_mp3decoder. I have no idea why other people are using this beepdec.mp3 plugin as it seems deprecated.
Finally, I had wrong paths in my beep_registry.arm12.cf file. Slightly confusing how this was required even though I wasn't using the beepdec.mp3 codec.