MSCALE_DDR_Tool: LPDDR4 stress test fails with iMX8M+ Custom board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MSCALE_DDR_Tool: LPDDR4 stress test fails with iMX8M+ Custom board

Jump to solution
2,543 Views
ramachandran_di
Contributor II

Dear Team,

We developed custom board using iMX8M+ and 8GB LDDR4 RAM-MT53E2G32D4NQ-046 WT:A.

We booted the board with kernel (5.10.35) and BSP successfully.

And now we are trying to optimize the LPDDR4timing parameters/stress test using the tool "MSCALE_DDR_Tool". After calibration we tried stress test with different options as below.

It was failing with option "Stop When Fail" and passing with option"Disable memory cache"

Refer "DDR_imx8+_8GB"for failure

Refer"Mscale_ddr_tool _v3.30"for pass test

Refer"LPDDR4_2000MHz_8GB"for script generated from RPA excel for8GB memory.

Could you explain clearly on these test cases and why it fails for some options?

We are using the latest versions of RPA(V7) and MSCALE(3.3) tool.

Thanks,

Divya

 

0 Kudos
Reply
1 Solution
2,511 Views
ramachandran_di
Contributor II

Dear Team,

We are using iMX8MP and we were able to resolve the issue by changing the MR registers in RPA excel.Now all memory stress tests are passing.

 

Thanks

Divya

View solution in original post

3 Replies
2,512 Views
ramachandran_di
Contributor II

Dear Team,

We are using iMX8MP and we were able to resolve the issue by changing the MR registers in RPA excel.Now all memory stress tests are passing.

 

Thanks

Divya

2,113 Views
karthikssk
Contributor I

Hi Divya,

Could you please let us know what you updated in the MR registers, because same issue we are seeing in our design as well, here we see that linux comes up and then when we run stress test the test crashes after 20min.

Please can you provide some more inputs on this on fine tuning the ddr

 

Regards,

Karthik

0 Kudos
Reply
2,514 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Could you tell us which product are you using?i.MX8MQ or i.MX8MP or others.

0 Kudos
Reply