MCIMX6ULL-EVK + LCD 8K3T board hangs during boot-up

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MCIMX6ULL-EVK + LCD 8K3T board hangs during boot-up

1,649 Views
rseymour
Contributor I

Hi All,

Please could someone help, I'm new to Linux !! Would be great to start with an out of the box working platform.

Boot error:

U-Boot 2016.03-imx_v2016.03_4.1.15_2.0.0_ga+g0ec2a01 (Nov 05 2016 - 01:13:31 -0500)

CPU: Freescale i.MX6ULL rev1.0 at 396MHz
CPU: Commercial temperature grade (0C to 95C) at 33C
Reset cause: POR
Board: MX6ULL 14x14 EVK
I2C: ready
DRAM: 512 MiB
MMC: FSL_SDHC: 0, FSL_SDHC: 1
*** Warning - bad CRC, using default environment

Display: TFT43AB (480x272)
Video: 480x272x24
In: serial
Out: serial
Err: serial
switch to partitions #0, OK
mmc1 is current device
Net: FEC1
Normal Boot
Hit any key to stop autoboot: 0
switch to partitions #0, OK
mmc1 is current device
switch to partitions #0, OK
mmc1 is current device
reading boot.scr
** Unable to read file boot.scr **
reading zImage
6635528 bytes read in 957 ms (6.6 MiB/s)
Booting from mmc ...
reading imx6ull-14x14-evk.dtb
35921 bytes read in 20 ms (1.7 MiB/s)
Kernel image @ 0x80800000 [ 0x000000 - 0x654008 ]
## Flattened Device Tree blob at 83000000
Booting using the fdt blob at 0x83000000
Using Device Tree in place at 83000000, end 8300bc50

Starting kernel ...

Cheers, Richard

0 Kudos
Reply
7 Replies

1,474 Views
igorpadykov
NXP Employee
NXP Employee

Hi Richard

one can try Demo Image, use Mfg Tool for programming

i.MX 6ULL Linux Binary Demo Files

i.MX Series Manufacturing Toolkit for Linux 4.1.15_2.0.0 Release

More linux documentation:

i.MX Software and Development Tools | NXP 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,474 Views
rseymour
Contributor I

 Thanks for your reply.. I have tried MfgTools.. with and without Rootfs.

And I get the following error:

Something to do with PMIC. not sure about the fine detail at the mo!!

Any idea ?

U-Boot 2016.03-imx_v2016.03_4.1.15_2.0.0_ga+g0ec2a01 (Sep 16 2016 - 18:28:25 -0500)

 

CPU:   Freescale i.MX6ULL rev1.0 at 396 MHz

Reset cause: POR

Board: MX6ULL 14X14 DDR3 ARM2

I2C:   ready

DRAM:  1 GiB

force_idle_bus: sda=0 scl=0 sda.gp=0x3 scl.gp=0x2

wait_for_sr_state: Arbitration lost sr=f2 cr=98 state=202

wait_for_sr_state: failed sr=a2 cr=88 state=2000 i2c_imx_stop:trigger stop failed

i2c_init_transfer: failed for chip 0x8 retry=0

force_idle_bus: sda=0 scl=0 sda.gp=0x3 scl.gp=0x2

wait_for_sr_state: Arbitration lost sr=f2 cr=98 state=202

wait_for_sr_state: failed sr=a2 cr=88 state=2000 i2c_imx_stop:trigger stop failed

i2c_init_transfer: failed for chip 0x8 retry=1

force_idle_bus: sda=0 scl=0 sda.gp=0x3 scl.gp=0x2

wait_for_sr_state: Arbitration lost sr=f2 cr=98 state=202

wait_for_sr_state: failed sr=a2 cr=88 state=2000 i2c_imx_stop:trigger stop failed

i2c_init_transfer: failed for chip 0x8 retry=2

force_idle_bus: sda=0 scl=0 sda.gp=0x3 scl.gp=0x2

i2c_init_transfer: give up i2c_regs=0x21a0000 Can't find PMIC:PFUZE100 initcall sequence bff96f18 failed at call 87803a3c (err=-1) ### ERROR ### Please RESET the board ###

Cheers Richard

0 Kudos
Reply

1,474 Views
igorpadykov
NXP Employee
NXP Employee

Hi Richard

from log:

"Board: MX6ULL 14X14 DDR3 ARM2"

this is different board than  MCIMX6ULL EVK and images are

different for those boards.

Best regards
igor

0 Kudos
Reply

1,474 Views
rseymour
Contributor I

Hi igor,

I’m using the following tools: L4.1.15_2.0.0-ga_mfg-tools. Correct tools ?

Also, the board hangs using the original sdcard as per my initial post.

Please advise.. I’m new to Linux, but OK with embedded systems etc..

Many thanks,

Richard

0 Kudos
Reply

1,474 Views
igorpadykov
NXP Employee
NXP Employee

Hi Richard

 

could you provide board marking.
One can try to follow:
0 Kudos
Reply

1,474 Views
rseymour
Contributor I

Hi Igor,

Please find the board images/ID attached.

Is it common that the supplied sdcard image has errors booting ?

Thanks for your help, due to being poorly I have been off work for awhile so trying to get up to speed with

Linux development. The goal is to add hardware, modify the devkit and write some C code/device drivers/tasks etc

Interested in IoT; Lora, WiFi etc.

I hope to get the SDK /JTAG operational soon !

Cheers,

Richard

0 Kudos
Reply

1,474 Views
igorpadykov
NXP Employee
NXP Employee

Hi Richard

could you try with:

i.MX 6ULL Linux Binary Demo Files

>Is it common that the supplied sdcard image has errors booting ?

not, as Demo Images from i.MX Software and Development Tools | NXP 

are tested with reference boards.

Best regards
igor

0 Kudos
Reply