Dear pals,
I have been working on building QT-embedded with LTIB for iMX53 SABRE tablet. And I m running into the following error which
is hard to undesrstand.
-------------------------------------------------------------------------------------------------------------------------------------
/../libs/gstbufmeta -I../../../../libs/vss -I../../../../libs/hbuf_alloc -g -O2 -I/home/wintu/ltib/rootfs/usr/include/mm_ghdr -DARM -D_GNUC_ -MT libmfw_gst_vpu_enc_la-mfw_gst_vpu_encoder.lo -MD -MP -MF .deps/libmfw_gst_vpu_enc_la-mfw_gst_vpu_encoder.Tpo -c mfw_gst_vpu_encoder.c -fPIC -DPIC -o .libs/libmfw_gst_vpu_enc_la-mfw_gst_vpu_encoder.o
mfw_gst_vpu_encoder.c:70:1: warning: "GST_ERROR" redefined
In file included from /home/wintu/ltib/rootfs/usr/include/gstreamer-0.10/gst/gst.h:47,
from mfw_gst_vpu_encoder.c:45:
/home/wintu/ltib/rootfs/usr/include/gstreamer-0.10/gst/gstinfo.h:794:1: warning: this is the location of the previous definition
mfw_gst_vpu_encoder.c: In function 'mfw_gst_vpuenc_vpuinitialize':
mfw_gst_vpu_encoder.c:1057: error: too few arguments to function 'vpu_EncRegisterFrameBuffer'
mfw_gst_vpu_encoder.c: In function 'mfw_gst_vpuenc_copy_sink_start_frame':
mfw_gst_vpu_encoder.c:1197: warning: pointer/integer type mismatch in conditional expression
mfw_gst_vpu_encoder.c:1197: warning: assignment makes integer from pointer without a cast
mfw_gst_vpu_encoder.c: In function 'mfw_gst_vpuenc_class_init':
mfw_gst_vpu_encoder.c:2272: warning: assignment from incompatible pointer type
mfw_gst_vpu_encoder.c:2273: warning: assignment from incompatible pointer type
mfw_gst_vpu_encoder.c: In function 'mfw_gst_vpuenc_buffer_alloc':
mfw_gst_vpu_encoder.c:2407: warning: initialization from incompatible pointer type
mfw_gst_vpu_encoder.c:2414: warning: assignment makes pointer from integer without a cast
mfw_gst_vpu_encoder.c:2421: warning: assignment from incompatible pointer type
mfw_gst_vpu_encoder.c:2423: warning: assignment from incompatible pointer type
mfw_gst_vpu_encoder.c:2424: warning: assignment from incompatible pointer type
make[1]: *** [libmfw_gst_vpu_enc_la-mfw_gst_vpu_encoder.lo] Error 1
make[1]: Leaving directory `/home/wintu/ltib/rpm/BUILD/gst-fsl-plugin-2.0.1/src/video/vpu_enc/src'
make: *** [all-recursive] Error 1
error: Bad exit status from /home/wintu/ltib/tmp/rpm-tmp.20278 (%build)
RPM build errors:
Bad exit status from /home/wintu/ltib/tmp/rpm-tmp.20278 (%build)
Build time for gst-fsl-plugin: 13 seconds
Failed building gst-fsl-plugin
f_buildrpms() returned an error, exiting
traceback:
main:560
Started: Tue Jan 8 05:48:05 2013
Ended: Tue Jan 8 05:48:19 2013
Elapsed: 14 seconds
These packages failed to build:
gst-fsl-plugin
Build Failed
Exiting on error or interrupt
--------------------------------------------------------
Could someone help me please..
Thanks in advance...
Winston.
解決済! 解決策の投稿を見る。
which BSP ar you using? For i.MX53 , you can download the BSP from here:
http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=IMX53_SW
Basically, there are two BSP version. One is 11.09 and one is 11.05. So please use the same version for both BSP and Codec package. e.g. if you use 11.05 BSP source code, please use the same 11.05 Codec source code.
Please use the recent codec package. It also contains new gst plugins and instructions how
to install them.
Dear Yuri Muhin,
Thanks for the reply. As u sad I installed latest plugins. but the same error is coming.
drivers/mxc/ssi/ssi.c: In function 'get_ssi_fifo_addr':
drivers/mxc/ssi/ssi.c:111: error: dereferencing pointer to incomplete type
drivers/mxc/ssi/ssi.c: In function 'get_ssi_base_addr':
drivers/mxc/ssi/ssi.c:128: error: dereferencing pointer to incomplete type
I think its regarding SSI driver. while compiling the kernel. And I m using the BSP relese 11.05.
Thanks n regards,
Winston
Hi Winston,
I had the same problem with my i.mx6. Fixed it by including following line into mxc/ssi/ssi.c
#include <linux/fsl_devices.h>
Thank you Sebastian Strissel, Now its compiling perfectly.. I have not yet tested the audio... Once i play a .wav song I will let you know...
> And I m using the BSP relese 11.05.
Why don't use 11.09 with the recent patches ( exactly for 11.09) ?
Dear Yuri Muhin,
I tried using 11.09 BSP too. But exact same error that of SSI. And in patches folder there are no patches regarding SSI driver. Is there any other way we can get audio in imx53. ?
Dear Winston Rodrigues,
I´m having the same error here. Could you fix it?
Dear icantreed,
No luck till now.. If u have found the problem, please post it.
Dear jimmychan ,
You are right... :smileyhappy: I was using BSP 11.09... So i downloaded 11.05 and compiled it.
It went well. But theres another problem here while compiling SSI ( sound ) driver ( in MXC Support Drivers-> MXC SSI Support-> SSI Support) ..
I need audio badly.. Or can u suggest any other driver ?? I'm working on SABRE tablet..
Here is last few lines of output...
make[1]: `include/generated/mach-types.h' is up to date.
CALL scripts/checksyscalls.sh
CHK include/generated/compile.h
GZIP kernel/config_data.gz
IKCFG kernel/config_data.h
CC kernel/configs.o
LD kernel/built-in.o
CC drivers/mxc/ssi/ssi.o
CC drivers/mxc/vpu/mxc_vpu.o
CC drivers/mxc/vpu/mxc_vl2cc.o
drivers/mxc/ssi/ssi.c: In function 'get_ssi_fifo_addr':
drivers/mxc/ssi/ssi.c:111: error: dereferencing pointer to incomplete type
drivers/mxc/ssi/ssi.c: In function 'get_ssi_base_addr':
drivers/mxc/ssi/ssi.c:128: error: dereferencing pointer to incomplete type
drivers/mxc/ssi/ssi.c: In function 'ssi_rx_fifo_counter':
drivers/mxc/ssi/ssi.c:568: warning: overflow in implicit constant conversion
drivers/mxc/ssi/ssi.c:572: warning: overflow in implicit constant conversion
drivers/mxc/ssi/ssi.c: In function 'ssi_tx_fifo_counter':
drivers/mxc/ssi/ssi.c:939: warning: overflow in implicit constant conversion
drivers/mxc/ssi/ssi.c:943: warning: overflow in implicit constant conversion
make[3]: *** [drivers/mxc/ssi/ssi.o] Error 1
make[2]: *** [drivers/mxc/ssi] Error 2
make[2]: *** Waiting for unfinished jobs....
CC drivers/video/logo/logo_linux_mono.o
CC drivers/video/logo/logo.o
LD drivers/video/logo/built-in.o
LD drivers/video/built-in.o
LD drivers/mxc/vpu/vpu.o
LD drivers/mxc/vpu/built-in.o
make[1]: *** [drivers/mxc] Error 2
make: *** [drivers] Error 2
error: Bad exit status from /home/wintu/ltib/tmp/rpm-tmp.30321 (%build)
RPM build errors:
Bad exit status from /home/wintu/ltib/tmp/rpm-tmp.30321 (%build)
Build time for kernel-2.6.35: 4316 seconds
Failed building kernel-2.6.35
f_buildrpms() returned an error, exiting
traceback:
main:560
Started: Tue Jan 15 05:07:36 2013
Ended: Tue Jan 15 06:19:33 2013
Elapsed: 4317 seconds
These packages failed to build:
kernel-2.6.35
Build Failed
Exiting on error or interrupt
I get error regarding dereferenced pointer. Could you please check it out. ..
which BSP ar you using? For i.MX53 , you can download the BSP from here:
http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=IMX53_SW
Basically, there are two BSP version. One is 11.09 and one is 11.05. So please use the same version for both BSP and Codec package. e.g. if you use 11.05 BSP source code, please use the same 11.05 Codec source code.
Dear jimmychan ,
You are right... :smileyhappy: I was using BSP 11.09... So i downloaded 11.05 and compiled it.
It went well. But theres another problem here while compiling SSI ( sound ) driver ( in MXC Support Drivers-> MXC SSI Support-> SSI Support) ..
I get error regarding dereferenced pointer. Could you please check it out. ..
I need audio badly.. Or can u suggest any other driver ?? I'm working on SABRE tablet..
Here is last few lines of output...
make[1]: `include/generated/mach-types.h' is up to date.
CALL scripts/checksyscalls.sh
CHK include/generated/compile.h
GZIP kernel/config_data.gz
IKCFG kernel/config_data.h
CC kernel/configs.o
LD kernel/built-in.o
CC drivers/mxc/ssi/ssi.o
CC drivers/mxc/vpu/mxc_vpu.o
CC drivers/mxc/vpu/mxc_vl2cc.o
drivers/mxc/ssi/ssi.c: In function 'get_ssi_fifo_addr':
drivers/mxc/ssi/ssi.c:111: error: dereferencing pointer to incomplete type
drivers/mxc/ssi/ssi.c: In function 'get_ssi_base_addr':
drivers/mxc/ssi/ssi.c:128: error: dereferencing pointer to incomplete type
drivers/mxc/ssi/ssi.c: In function 'ssi_rx_fifo_counter':
drivers/mxc/ssi/ssi.c:568: warning: overflow in implicit constant conversion
drivers/mxc/ssi/ssi.c:572: warning: overflow in implicit constant conversion
drivers/mxc/ssi/ssi.c: In function 'ssi_tx_fifo_counter':
drivers/mxc/ssi/ssi.c:939: warning: overflow in implicit constant conversion
drivers/mxc/ssi/ssi.c:943: warning: overflow in implicit constant conversion
make[3]: *** [drivers/mxc/ssi/ssi.o] Error 1
make[2]: *** [drivers/mxc/ssi] Error 2
make[2]: *** Waiting for unfinished jobs....
CC drivers/video/logo/logo_linux_mono.o
CC drivers/video/logo/logo.o
LD drivers/video/logo/built-in.o
LD drivers/video/built-in.o
LD drivers/mxc/vpu/vpu.o
LD drivers/mxc/vpu/built-in.o
make[1]: *** [drivers/mxc] Error 2
make: *** [drivers] Error 2
error: Bad exit status from /home/wintu/ltib/tmp/rpm-tmp.30321 (%build)
RPM build errors:
Bad exit status from /home/wintu/ltib/tmp/rpm-tmp.30321 (%build)
Build time for kernel-2.6.35: 4316 seconds
Failed building kernel-2.6.35
f_buildrpms() returned an error, exiting
traceback:
main:560
Started: Tue Jan 15 05:07:36 2013
Ended: Tue Jan 15 06:19:33 2013
Elapsed: 4317 seconds
These packages failed to build:
kernel-2.6.35
Build Failed
Exiting on error or interrupt