Link for downloading the MFGtool for Windows

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Link for downloading the MFGtool for Windows

29,022 Views
adityanagal
Contributor III

Hi ,

As pe the IMX_Linux_user_Guide section 4.2 , there is a MFGtool available for the Windows Operating System . Could anyone please share the path of the executable.

Regards,

Aditya Nagal

2 Replies

5,371 Views
pm_2552
Contributor III

Is the MfgTool utility available for Mac?

0 Kudos
Reply

14,624 Views
igorpadykov
NXP Employee
NXP Employee

Hi Aditya

please refer to link

http://www.nxp.com/products/software-and-tools/software-development-tools/i.mx-software-and-tools/i....

use mfg tool, corresponding to linux kernel, for example for L4.1.15_2.0.0  :

http://www.nxp.com/webapp/Download?colCode=IMX6_L4-1-15_2-0-0_MFG-TOOL&appType=license&location=null... 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------