Keyboard Indicator/Toggle Button on top bar Sato Gnome Desktop

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Keyboard Indicator/Toggle Button on top bar Sato Gnome Desktop

2,596件の閲覧回数
marco_padovani
Contributor II

Hi, 

i'm working with yocto project on the imx6 processor. I created the sato image where a GNOME desktop manager is used. On the top bar there are:

- Home button 

- Change Windows button

- Mouse indicator

- Time

I would also like to insert the keyboard indicator button, whit the possibility of pressing that butto to enable or disable the virtual keyboard. (fig.1 What do i have, fig.2 what i would like)

I don't know if this option is already present, but i have already created a script (with matchbox command) that make the enable/disable toggle of the virtual keyboard, but i managed to insert it as an "app" and not in the top bar (fig.3 keyboard toggle as an app).

If i connect an external keyboard in the situation of "fig.1", the keyboard function normally but without indicator.

My priority is to integrate a button keyboard indicator in the top bar that enable or disable the virtual keyboard.

Anyone can help me?

Thanks, 

Marco

ラベル(5)
タグ(5)
0 件の賞賛
返信
4 返答(返信)

2,353件の閲覧回数
marco_padovani
Contributor II

Hi, 

i resolved! 

I added in matchbox-session-sato file the applet "keyboard" and now the top bar have the keyboard icon!

Thanks to all,

Marco

0 件の賞賛
返信

2,353件の閲覧回数
radhikasomaiya
Senior Contributor II

Hi marco.padovani@sacmi.it,

Can you please give us some details like which linux version you are using to build sato image and the board which you are using?

Regards,

Radhika Somaiya.

0 件の賞賛
返信

2,353件の閲覧回数
marco_padovani
Contributor II

Hi Radhika, 

i'm using a Yocto Krogoth and a Congatec Module with iMX6 Solo. I found that keyboard indicator was a Xsever applet, but can i start an applet after Xserver goes on?

Thanks for your support.

Regards,

Marco

0 件の賞賛
返信

2,353件の閲覧回数
jamesbone
NXP TechSupport
NXP TechSupport

You can try this plugin from ArchLinux.

There is also this one from Ubuntu, but it looks more like Cinnamon rather than Xfce.

0 件の賞賛
返信