Is it possible for the iMX6 to display two differnet images on the 2 RGB buses at the same time?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is it possible for the iMX6 to display two differnet images on the 2 RGB buses at the same time?

695 Views
hishamelmeligi
Contributor II

I need to use the 2xRGB buses in a project. Could you please confirm that the i.MX6 can support 2xRGB screens ? Here in the NXP document: Video/Image Codec and Data Pipeline slide 57 (the image below) the two RGB buses are enabled.

Inline image 1
2 Replies

525 Views
igorpadykov
NXP Employee
NXP Employee

Hi Hisham

yes i.MX6 IPU can support this. Please check presentation on

https://community.nxp.com/docs/DOC-100482 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

525 Views
hishamelmeligi
Contributor II

Thank you.

0 Kudos