Hello all,
I've been trying to set up Murata's LBEE6ZZ1FD module with i.MX8QuadMax Multisensory Enablement Kit. The kit came with LBEE6ZZ1FD. However, release notes from IMXPRERELEASE page state that the officially supported wifi & bluetooth board is Qualcomm QCA6174. (So, I assume the firmware involves ATH10k/QCA6174 drivers already)
Trying to install LBEE6ZZ1FD's BCM89359 firmware to linux, release note says extra efforts might be needed, - hence, limited access board support packages-, I've integrated firmware-bcmd-1.363.22.bin to yocto from an external website and successfully installed it to /lib/firmware/bcm.
Still no sign of any driver messages (dmesg), nor any sign of bluetooth device recognition through hciconfig.
Digging through information, I found Murata's partnership with iMX, I came across a User Guide from Murata. Device trees, kernel images and firmware are given for several boards (iMX6s and iMX7s), but not for the iMX.8 QuadMax MEK (prerelease).
https://wireless.murata.com/datasheet?/RFM/data/murata_quick_start_guide_linux.pdf
Do I need to wait for the official release to be able to use this module? This might be Murata's concern, but I want to see if NXP community faces the same issue. If anybody from NXP could enlighten, that would save us some time.
Thanks in advance.
Hello Mustafa,
Please use NXP’s L4.14.98 BSP to build an image for your target. That BSP supports Murata’s 1FD module.
Best regards,
Romit
Hi
Where can I purchase Murata 1CQ (Qca6174A).
The murata web site has minimum quantity requirement.
But I just need one for evaluation.
Hi Bill,
Have you found where to purchase Murata 1CQ (Qca6174A) ?
I can’t find where to purchase.
Hi Mustafa
as stated in attached Release Notes p.9 supported and tested
only Murata 1CQ (Qca6174A), documentation is available on
Alpha / Beta BSPs for Microprocessors|NXP
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------