Inconsistency in I2C Interface

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Inconsistency in I2C Interface

ソリューションへジャンプ
683件の閲覧回数
sachinmohankura
Contributor I

Hi,

We notice inconsistency in data received from touch controller.

  • We get valid data for few cycle
  • We get data read error for few touch input
  • We get NAK for data read from touch after address cycle.
  • We get ACK for the data but data read is FF all the time( here the I2C clock is held low for one or more cycle in between 8 bit read)

 

I have summarized all data in Touch panel I2C Issue.PPT and LA waveform capture(PNG Image).

Regards,

Sachin

0 件の賞賛
1 解決策
611件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Sachin

issue may be caused by signals noise or operating systems delays, so one can try to

decrease operating i2c frequency, add delays and descrease pull resistors values.

May be recommended to try with baremetal sdk (or freertos)

Github SDK
https://github.com/backenklee/swp-report/tree/master/iMX6_Platform_SDK

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
1 返信
612件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Sachin

issue may be caused by signals noise or operating systems delays, so one can try to

decrease operating i2c frequency, add delays and descrease pull resistors values.

May be recommended to try with baremetal sdk (or freertos)

Github SDK
https://github.com/backenklee/swp-report/tree/master/iMX6_Platform_SDK

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛