In order to pass the PCIE eye diagram test, how do I modify the value of PCIE Gen-1 and Gen-2 register?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

In order to pass the PCIE eye diagram test, how do I modify the value of PCIE Gen-1 and Gen-2 register?

985 Views
charleshuang
Senior Contributor II

1. Could you tell me the register address of pcie Gen-1 and Gen-2?

2. If I want to modify pcie Gen-1 and Gen-2 register parameter values, how do I modify in the program file?

Thank you.

Best Regards,

Alex Cheng

0 Kudos
4 Replies

486 Views
igorpadykov
NXP Employee
NXP Employee

Hi charles,

please check AN4784 and link below

How to setup i.MX6Dual/Quad and i.MX6Solo/DualLite Linux software for PCIe compliance Test?

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos

486 Views
charleshuang
Senior Contributor II

Hi Chipexpert,

If I follow your compliance test method, do I need to consider the setting value of PCIe Gen-1 and Gen-2 register about SI test?

If the answer is no, I want to modify PCIe Gen-1 and Gen-2 register parameter values. How do I modify in the program file?

Thanks.

0 Kudos

486 Views
igorpadykov
NXP Employee
NXP Employee

Hi charles,

please look at AN4784 it shows

settings for both Gen1 and Gen2.

Best regards

chip

486 Views
charleshuang
Senior Contributor II

Hi chip,

I know. Thank you for your reply.

Best Regards,

Charles

0 Kudos