IMx platfrom SDK for Nitrogen Lite

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMx platfrom SDK for Nitrogen Lite

515 Views
prasannaprabhu7
Contributor III

I have a Nitrogen lite board from Boundary devices and with imx6 solo processor, I did compile the whole and I have different folders in board/ folder.. As Nitrogen Lite board config is same as that of Sabre SD , I chose board/mx6sdl/sabre_ai/ and checked the mux configurations, but UART Mux Pins did not match up, I did change the same -compiled it and flashed it to a SD card and sad to find no out put. Can anyone help me fixing this?

(FYI, I did current UART2 Mux configurations to the one which is suggested for Nitrogen Lite board,also change the same in .xml file in one of the revisions.)

My question is did any one did test platform SDK in Nitrogen devices? Or is that I am missing something?

Regards,

Prasanna

Labels (4)
0 Kudos
1 Reply

352 Views
gary_bisson
Senior Contributor III

Hi,

Unfortunately the i.MX6 platform SDK is only meant for Freescale platforms whereas the Nitrogen6_Lite is a Boundary Devices platform. Nitrogen6_Lite is a lot different from the SabreSD.

A board configuration must therefore be added to the SDK with an updated muxing for it to work.

Regards,

Gary

0 Kudos