IMX8QXP watchdog enable

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX8QXP watchdog enable

342 Views
gravity_one
Contributor III

Dear Guys,

 

I want to enable SOC watchdog, and refer to link: https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/SCFW-Enable-PMIC-external-watchdog-for-i...

but i do not know how to test?

Q1, SOC kernel halted whether PMIC watchdog will reset SOC?

Q2, SOC kernel halted whether SUC still will run?

Q3, i want to prevent Linux kernel system into halt, can this PMIC watchdog be achieved?

 

Brs,

Gravity

 

 

0 Kudos
1 Reply

330 Views
Harvey021
NXP TechSupport
NXP TechSupport

Hi @gravity_one 

SoC watch dog is enabled by default in SCFW, if SCFW crashes, it will reset the whole chip.

For A35 or M4 side, they can also enable their own watchdog, then when no service to the watchdog, the A35 or M4 will reset,

this will not cause whole SoC reset.

/unit_tests/watchdog/wdt_driver_test.out 5 5 0

this is the test command to enable the Linux kernel's watchdog.

 

Best regards

Harvey

 

0 Kudos