IMX8QM hardware design LPDDR4

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

IMX8QM hardware design LPDDR4

跳至解决方案
1,743 次查看
timur_kh
Contributor II

Hello everyone!
The schematic of IMX8QM (SPF-29420_C5) on pages 14-15 shows an example of an LPDDR4 connection. Do I understand correctly that the DDR_CH[1:0].DQ_[15:0] and DR_CH[1:0].DQ_[31:16] ports can be connected depending on the footprint (simplify PCB design)? If Yes, then this is configure in the Config Tools for i.MX v8?

Second question. In the diagram on page 15, the names of the LPDDR4 channels do not match, i.e. the MX8QP channel A is connected to the LPDDR4 channel B and vice versa, this is also done to simplify the design of the PCB?

Third question. In my device there is DR_CS 1_CS 0_A, but there is no DDR_CH1_CH1_A. How do I properly connect DDR_CS1_CS0_A?

0 项奖励
回复
1 解答
1,736 次查看
igorpadykov
NXP Employee
NXP Employee

Hi timur_kh

 

> Do I understand correctly that the DDR_CH[1:0].DQ_[15:0] and DR_CH[1:0].DQ_[31:16] ports

>can be connected depending on the footprint (simplify PCB design)?

 

yes

 

>Second question. In the diagram on page 15, the names of the LPDDR4 channels do not match, i.e. the >MX8QP channel A is connected to the LPDDR4 channel B and vice versa, this is also done to simplify the >design of the PCB?

 

yes

 

>Third question. In my device there is DR_CS 1_CS 0_A, but there is no DDR_CH1_CH1_A.

>How do I properly connect DDR_CS1_CS0_A?

 

what do you mean exactly, in SPF-29420_C5 there is also no DDR_CH1_CH1_A.

 

Best regards
igor

在原帖中查看解决方案

0 项奖励
回复
3 回复数
1,732 次查看
timur_kh
Contributor II

Oh, I made a typo.
Please look at the attached picture.

0 项奖励
回复
1,719 次查看
igorpadykov
NXP Employee
NXP Employee

so what ddr part used in the case, in general in each lpddr4 datasheet section

"Package Block Diagrams" one can find recommended connections.

So if there are no CKE1, CS1 seems this is single rank part, use only CKE0, CS0.

 

Best regards
igor

 

0 项奖励
回复
1,737 次查看
igorpadykov
NXP Employee
NXP Employee

Hi timur_kh

 

> Do I understand correctly that the DDR_CH[1:0].DQ_[15:0] and DR_CH[1:0].DQ_[31:16] ports

>can be connected depending on the footprint (simplify PCB design)?

 

yes

 

>Second question. In the diagram on page 15, the names of the LPDDR4 channels do not match, i.e. the >MX8QP channel A is connected to the LPDDR4 channel B and vice versa, this is also done to simplify the >design of the PCB?

 

yes

 

>Third question. In my device there is DR_CS 1_CS 0_A, but there is no DDR_CH1_CH1_A.

>How do I properly connect DDR_CS1_CS0_A?

 

what do you mean exactly, in SPF-29420_C5 there is also no DDR_CH1_CH1_A.

 

Best regards
igor

0 项奖励
回复