IMX8QM U disk can not be mount

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX8QM U disk can not be mount

1,543件の閲覧回数
jack-cap
Contributor III

Hi NXP teams

Recently,we are working on imx8qm mek board.When I plug in an U disk,it can be Correct identification of USB flash disk in kernel,But it can not be mount.

My software platform is :  Android 9 normal version.

I use usbotg3 as otg port.

the modify as below:

&usbotg3 {
dr_mode = "otg";
status = "okay";
};

pastedImage_1.png

some kernel log as below:

plug in U disk

[ 1122.244716] usb 1-1: new high-speed USB device number 3 using cdns-usb3
[ 1122.397250] usb 1-1: New USB device found, idVendor=abcd, idProduct=1234
[ 1122.403984] usb 1-1: New USB device strings: Mfr=1, Product=2, SerialNumber=3
[ 1122.411367] usb 1-1: Product: UDisk
[ 1122.415841] usb 1-1: Manufacturer: General
[ 1122.420061] usb 1-1: SerialNumber: Љ
[ 1122.429024] usb-storage 1-1:1.0: USB Mass Storage device detected
[ 1122.435481] scsi host1: usb-storage 1-1:1.0
[ 1123.461542] scsi 1:0:0:0: Direct-Access General UDisk 5.00 PQ: 0 ANSI: 2
[ 1123.474433] sd 1:0:0:0: [sda] 7864320 512-byte logical blocks: (4.03 GB/3.75 GiB)
[ 1123.482886] sd 1:0:0:0: [sda] Write Protect is off
[ 1123.488124] sd 1:0:0:0: [sda] No Caching mode page found
[ 1123.494394] sd 1:0:0:0: [sda] Assuming drive cache: write through
[ 1123.503604] sda: sda1 sda4
[ 1123.511734] sd 1:0:0:0: [sda] Attached SCSI removable disk

Could you help me check it ?

BRs

thanks

ラベル(2)
タグ(1)
0 件の賞賛
返信
2 返答(返信)

1,389件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi yingjin

what android release used in the case, reason may be that not all releases were tested

with i.MX8QM processor. One can check Release Notes in Android documentation

on below link for supported processors in each release

i.MX Software and Development Tools | NXP 

Additional details, like below can be found in Table 2 Features

pastedImage_2.jpg

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,389件の閲覧回数
jack-cap
Contributor III

Hi  igor

the android versionwe use is  Android P9.0.0_2.0.1

I will check it.

BRs

thanks

0 件の賞賛
返信