Hello,
1. I have generated the SD image for my custom board based on IMX8M plus processor. Below is the SD image generated in our build with size 260 MB with below file extension.
customized-SD-image-usd.wic.zst
2. After this I flashed this image to 32GB Sandisk SD card using the command provided in the document as shown in the below screenshot.
Note:
- Formatted the SD card to "FAT32" before flashing the actual SD image.
- Replaced the sdX as "sde" with the one which was detected by host machine for uSD.
zstdcat <customized-SD-image name-usd.wic.zst> | sudo dd of=/dev/sdX bs=1M conv=fsync
3. Then we inserted this flashed SD card to the custom board and tried to boot using SD mode with below attached SD boot settings.
![swathi_2-1702444861834.png swathi_2-1702444861834.png](https://community.nxp.com/t5/image/serverpage/image-id/254105iD352AA66C3D49CBA/image-size/medium?v=v2&px=400)
4. But we are unable to boot completely from SD card and observed below mentioned errors from the console.
Log:
Failed to load 'boot.scr'
Error reading cluster
** Unable to read file Image **
Failed to load 'Image'
END BOOTING
u-boot=>
u-boot=> mmc part
Partition Map for MMC device 1 -- Partition Type: DOS
Part Start Sector Num Sectors UUID Type
** Can't read partition table on 1:0 **
u-boot=>
Can you please suggest some commands/methods to export the already flashed SD card content.
Do I have to use any particular Filesystem Type while formatting the SD card, please help me to fix this issue.