IMX8MM PMIC_ON_REQ

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX8MM PMIC_ON_REQ

1,698 Views
santhosh2
Contributor IV

Is there any way to toggle the  PMIC_ON_REQ using software in IMX8MM

 

Regards

Santhosh

0 Kudos
Reply
7 Replies

1,687 Views
Yuri
NXP Employee
NXP Employee

@santhosh2 
Hello,

  
  The PMIC_ON_REQ signal can be controlled by the LPCR[TOP] and
LPCR[DP_EN] bits, say, when the 'poweroff' command is issued in Linux.

   For power on only ONOFF pin can be used.

Regards,
Yuri.

0 Kudos
Reply

1,682 Views
santhosh2
Contributor IV

Hello Yuri,

I have tried this method, But the PMIC_ON_REQ pin toggles only when the switch is pressed as mentioned in the data sheet.

PMIC_ON_REQ.png

Since I want to Control this PMIC_ON_REQ via software to reset the entire PMIC without using the switch, Is there any other way?

Regards

Santhosh

Tags (1)
0 Kudos
Reply

1,672 Views
Yuri
NXP Employee
NXP Employee

@santhosh2 

  Also, LPCR[DP_EN]  should be set.

 

~Yuri.

0 Kudos
Reply

1,663 Views
santhosh2
Contributor IV

hello yuri,

I tried it is not working for me, Any other things needs to be done

Regards

santhosh

0 Kudos
Reply

1,649 Views
Yuri
NXP Employee
NXP Employee

@santhosh2 
Hello,

   is Linux command "poweroff" working on Your board?

Regards,
Yuri.

0 Kudos
Reply

1,636 Views
santhosh2
Contributor IV

Power off command is available, but when poweroff command fired, the system power's off but reboot doesn't happen, Please advice any next step to try?

 

poweroff1.pngpoweroff2.png

Tags (1)
0 Kudos
Reply

1,627 Views
Yuri
NXP Employee
NXP Employee

@santhosh2 
Hello,

   let me know how LPCR[TOP] , LPCR[DP_EN] are written in Your tests.

Regards,
Yuri.

0 Kudos
Reply