IMX7 ULP EVK ANDROID

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX7 ULP EVK ANDROID

1,709件の閲覧回数
Hakan
Contributor I

Hi,

I dowlanded imx-android-10.0.0_2.6.0.tar.gz and compiled aosp for imx7ulp evk. Then, I flashed images using fsl-sdcard-partition.sh script. But I saw an error. The error is  android::init::FirstStageMount::InitRequiredDevices(): partition(s) not found in /sys, waiting for their uevent(s): boot, dtbo, metadr. How can i solve it ?

 ./device/fsl/common/tools/fsl-sdcard-partition.sh -f imx7ulp -c 28 -D out/target/product/evk_7ulp/ /dev/mmcblk0

Log 

CPU: i.MX7ULP rev2.1 at 500 MHz
Reset cause: POR
Boot mode: Dual boot
PMC1: LDO bypass mode
Model: NXP i.MX7ULP EVK
DRAM: 1 GiB
MMC: FSL_SDHC: 0
Loading Environment from MMC... *** Warning - bad CRC, using default environment

[*]-Video Link 0 (720 x 1280)
[0] lcdif@40AA0000, video
[1] mipi_dsi@40A90000, video_bridge
[2] rm68200_panel, panel
In: serial
Out: serial
Err: serial
flash target is MMC:0
Net: No ethernet found.
Fastboot: Normal
Normal Boot
Hit any key to stop autoboot: 0
RNG already instantiated 0x40000033
Error: blob decap job failed 0x2000071a
Error during blob decap operation: 0x2000071a
In boota get fastboot lock status error. Set lock status
RNG already instantiated 0x40000033
RNG already instantiated 0x40000033
verify OK, boot 'boot'
kernel @ 62808000 (10892688)
ramdisk @ 63800000 (776992)
fdt @ 66808000 (23789)
RNG already instantiated 0x40000033
## Booting Android Image at 0x62807800 ...
## Flattened Device Tree blob at 66808000
Booting using the fdt blob at 0x66808000
XIP Kernel Image
Using Device Tree in place at 66808000, end 66810cec

Starting kernel ...

[ 0.000000] Booting Linux on physical CPU 0xf00
[ 0.000000] Linux version 5.4.70 (hakan@aydin) (arm-eabi-gcc (GNU Toolchain for the A-profile Architecture 8.3-2019.03 (arm-rel-8.36)) 8.3.0, GNU ld (GNU To3
[ 0.000000] CPU: ARMv7 Processor [410fc075] revision 5 (ARMv7), cr=10c5387d
[ 0.000000] CPU: div instructions available: patching division code
[ 0.000000] CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache
[ 0.000000] OF: fdt: Machine model: NXP i.MX7ULP EVKB
[ 0.000000] earlycon: lpuart32 at MMIO 0x402d0000 (options '')
[ 0.000000] printk: bootconsole [lpuart32] enabled
[ 0.000000] Memory policy: Data cache writealloc
[ 0.000000] cma: Reserved 320 MiB at 0x82000000
[ 0.000000] percpu: Embedded 20 pages/cpu s52300 r8192 d21428 u81920
[ 0.000000] Built 1 zonelists, mobility grouping on. Total pages: 259890
[ 0.000000] Kernel command line: console=ttyLP0,115200 earlycon init=/init androidboot.console=ttyLP0 consoleblank=0 androidboot.hardware=freescale vmalloc=e
[ 0.000000] Dentry cache hash table entries: 131072 (order: 7, 524288 bytes, linear)
[ 0.000000] Inode-cache hash table entries: 65536 (order: 6, 262144 bytes, linear)
[ 0.000000] mem auto-init: stack:off, heap alloc:off, heap free:off
[ 0.000000] Memory: 684212K/1047552K available (14336K kernel code, 1019K rwdata, 5136K rodata, 1024K init, 497K bss, 35660K reserved, 327680K cma-reserved,)
[ 0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=1, Nodes=1
[ 0.000000] rcu: Preemptible hierarchical RCU implementation.
[ 0.000000] rcu: RCU restricting CPUs from NR_CPUS=4 to nr_cpu_ids=1.
[ 0.000000] Tasks RCU enabled.
[ 0.000000] rcu: RCU calculated value of scheduler-enlistment delay is 10 jiffies.
[ 0.000000] rcu: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=1
[ 0.000000] NR_IRQS: 16, nr_irqs: 16, preallocated irqs: 16
[ 0.000000] random: get_random_bytes called from start_kernel+0x33c/0x504 with crng_init=0
[ 0.000000] Switching to timer-based delay loop, resolution 333ns
[ 0.000013] sched_clock: 32 bits at 3000kHz, resolution 333ns, wraps every 715827882841ns
[ 0.008159] clocksource: imx-tpm: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 637086815595 ns
[ 0.018713] Calibrating delay loop (skipped), value calculated using timer frequency.. 6.00 BogoMIPS (lpj=30000)
[ 0.028629] pid_max: default: 32768 minimum: 301
[ 0.033462] LSM: Security Framework initializing
[ 0.037881] SELinux: Initializing.
[ 0.041455] Mount-cache hash table entries: 2048 (order: 1, 8192 bytes, linear)
[ 0.048616] Mountpoint-cache hash table entries: 2048 (order: 1, 8192 bytes, linear)
[ 0.057737] CPU: Testing write buffer coherency: ok
[ 0.063041] /cpus/cpu@f00 missing clock-frequency property
[ 0.068278] CPU0: thread -1, cpu 0, socket 15, mpidr 80000f00
[ 0.075292] Setting up static identity map for 0x60100000 - 0x60100060
[ 0.081816] rcu: Hierarchical SRCU implementation.
[ 0.087138] smp: Bringing up secondary CPUs ...
[ 0.091414] smp: Brought up 1 node, 1 CPU
[ 0.095397] SMP: Total of 1 processors activated (6.00 BogoMIPS).
[ 0.101536] CPU: All CPU(s) started in SVC mode.
[ 0.106133] CPU0: update max cpu_capacity 1024
[ 0.106889] devtmpfs: initialized
[ 0.128699] VFP support v0.3: implementor 41 architecture 2 part 30 variant 7 rev 5
[ 0.136945] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 19112604462750000 ns
[ 0.146606] futex hash table entries: 256 (order: 2, 16384 bytes, linear)
[ 0.172225] pinctrl core: initialized pinctrl subsystem
[ 0.178944] NET: Registered protocol family 16
[ 0.197905] DMA: preallocated 256 KiB pool for atomic coherent allocations
[ 0.205437] audit: initializing netlink subsys (disabled)
[ 0.212048] cpuidle: using governor menu
[ 0.220745] audit: type=2000 audit(0.170:1): state=initialized audit_enabled=0 res=1
[ 0.261542] mxs_phy 40350000.usb-phy: 40350000.usb-phy supply phy-3p0 not found, using dummy regulator
[ 0.342933] No ATAGs?
[ 0.343055] hw-breakpoint: found 5 (+1 reserved) breakpoint and 4 watchpoint registers.
[ 0.353096] hw-breakpoint: maximum watchpoint size is 8 bytes.
[ 0.361409] imx7ulp-pinctrl 40ac0000.pinctrl: initialized IMX pinctrl driver
[ 0.369674] imx mu driver is registered.
[ 0.373785] imx rpmsg driver is registered.
[ 0.378966] printk: console [pstore-1] enabled
[ 0.383583] pstore: Registered ramoops as persistent store backend
[ 0.389565] ramoops: using 0x100000@0x99b00000, ecc: 0
[ 0.398485] MU is ready for cross core communication!
[ 0.437769] cryptd: max_cpu_qlen set to 1000
[ 0.461275] vgaarb: loaded
[ 0.465506] SCSI subsystem initialized
[ 0.469906] usbcore: registered new interface driver usbfs
[ 0.475457] usbcore: registered new interface driver hub
[ 0.480661] usbcore: registered new device driver usb
[ 0.488387] i2c i2c-2: LPI2C adapter registered
[ 0.494851] i2c i2c-1: LPI2C adapter registered
[ 0.499630] mc: Linux media interface: v0.10
[ 0.503717] videodev: Linux video capture interface: v2.00
[ 0.509330] pps_core: LinuxPPS API ver. 1 registered
[ 0.514043] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <[email protected]>
[ 0.523230] PTP clock support registered
[ 0.529013] MIPI CSI2 driver module loaded
[ 0.532939] Advanced Linux Sound Architecture Driver Initialized.
[ 0.540413] Bluetooth: Core ver 2.22
[ 0.543784] NET: Registered protocol family 31
[ 0.548155] Bluetooth: HCI device and connection manager initialized
[ 0.554557] Bluetooth: HCI socket layer initialized
[ 0.559342] Bluetooth: L2CAP socket layer initialized
[ 0.564367] Bluetooth: SCO socket layer initialized
[ 0.572713] clocksource: Switched to clocksource imx-tpm
[ 0.751081] VFS: Disk quotas dquot_6.6.0
[ 0.754964] VFS: Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)
[ 0.764226] thermal_sys: Registered thermal governor 'step_wise'
[ 0.764694] NET: Registered protocol family 2
[ 0.776082] tcp_listen_portaddr_hash hash table entries: 512 (order: 0, 6144 bytes, linear)
[ 0.784378] TCP established hash table entries: 8192 (order: 3, 32768 bytes, linear)
[ 0.792016] TCP bind hash table entries: 8192 (order: 4, 65536 bytes, linear)
[ 0.799317] TCP: Hash tables configured (established 8192 bind 8192)
[ 0.805705] UDP hash table entries: 512 (order: 2, 16384 bytes, linear)
[ 0.812114] UDP-Lite hash table entries: 512 (order: 2, 16384 bytes, linear)
[ 0.819483] NET: Registered protocol family 1
[ 0.824658] PCI: CLS 0 bytes, default 64
[ 0.828836] Trying to unpack rootfs image as initramfs...
[ 0.907914] Freeing initrd memory: 760K
[ 0.918418] Bus freq driver module loaded
[ 0.924307] Initialise system trusted keyrings
[ 0.928810] workingset: timestamp_bits=14 max_order=18 bucket_order=4
[ 0.947924] Registering sdcardfs 0.1
[ 0.951753] jffs2: version 2.2. (NAND) �© 2001-2006 Red Hat, Inc.
[ 0.958766] fuse: init (API version 7.31)
[ 1.037220] Key type asymmetric registered
[ 1.041079] Asymmetric key parser 'x509' registered
[ 1.046245] bounce: pool size: 64 pages
[ 1.049840] io scheduler mq-deadline registered
[ 1.054458] io scheduler kyber registered
[ 1.067477] pwm-backlight backlight: backlight supply power not found, using dummy regulator
[ 1.077153] mipi_dsi_northwest 40a90000.mipi_dsi: i.MX MIPI DSI driver probed
[ 1.084750] adv7535 probing phase
[ 1.087824] adv7535 2-003d: main addr = 0x3d
[ 1.092551] i2c i2c-2: chip_rev = 0x14
[ 1.096632] adv7535 2-003d: dsi cec addr = 0x78
[ 1.114602] adv7535 2-003d: adv7535 probe finished
[ 1.121599] mxsfb 40aa0000.lcdif: 40aa0000.lcdif supply lcd not found, using dummy regulator
[ 1.257507] mipi_dsi_northwest 40a90000.mipi_dsi: MIPI DSI dispdv inited
[ 1.264015] mxsfb 40aa0000.lcdif: registered mxc display driver mipi_dsi_northwest
[ 1.313331] sii902x bound to mxs-lcdif from 40aa0000.lcdif
[ 1.318598] mxsfb 40aa0000.lcdif: initialized
[ 1.337965] printk: console [ttyLP0] enabled0x402d0010 (irq = 39, base_baud = 1500000) is a FSL_LPUART
[ 1.337965] printk: console [ttyLP0] enabled
[ 1.346362] printk: bootconsole [lpuart32] disabled
[ 1.346362] printk: bootconsole [lpuart32] disabled
[ 1.356891] fsl-lpuart 402d0000.serial: DMA tx channel request failed, operating without tx DMA
[ 1.365735] fsl-lpuart 402d0000.serial: DMA rx channel request failed, operating without rx DMA
[ 1.375507] 40a60000.serial: ttyLP2 at MMIO 0x40a60010 (irq = 45, base_baud = 3000000) is a FSL_LPUART
[ 1.386787] imx sema4 driver is registered.
[ 1.415564] brd: module loaded
[ 1.429946] loop: module loaded
[ 1.434953] imx ahci driver is registered.
[ 1.446232] libphy: Fixed MDIO Bus: probed
[ 1.451326] tun: Universal TUN/TAP device driver, 1.6
[ 1.456948] CAN device driver interface
[ 1.462992] PPP generic driver version 2.4.2
[ 1.467640] PPP BSD Compression module registered
[ 1.472364] PPP Deflate Compression module registered
[ 1.477572] PPP MPPE Compression module registered
[ 1.482369] NET: Registered protocol family 24
[ 1.486901] PPTP driver version 0.8.5
[ 1.491158] usbcore: registered new interface driver r8152
[ 1.496839] usbcore: registered new interface driver lan78xx
[ 1.502587] usbcore: registered new interface driver asix
[ 1.508235] usbcore: registered new interface driver ax88179_178a
[ 1.514452] usbcore: registered new interface driver cdc_ether
[ 1.520373] usbcore: registered new interface driver smsc95xx
[ 1.526244] usbcore: registered new interface driver net1080
[ 1.531974] usbcore: registered new interface driver cdc_subset
[ 1.537998] usbcore: registered new interface driver zaurus
[ 1.543676] usbcore: registered new interface driver MOSCHIP usb-ethernet driver
[ 1.551167] usbcore: registered new interface driver cdc_ncm
[ 1.556859] ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
[ 1.563411] ehci-pci: EHCI PCI platform driver
[ 1.567930] ehci-mxc: Freescale On-Chip EHCI Host driver
[ 1.573799] usbcore: registered new interface driver usb-storage
[ 1.583536] input: rpmsg-keys as /devices/soc0/rpmsg-keys/input/input0
[ 1.591068] usbcore: registered new interface driver xpad
[ 1.596755] usbcore: registered new interface driver usb_acecad
[ 1.602873] usbcore: registered new interface driver aiptek
[ 1.608513] usbcore: registered new interface driver gtco
[ 1.614085] usbcore: registered new interface driver hanwang
[ 1.619809] usbcore: registered new interface driver kbtab
[ 1.626316] input: fts_ts as /devices/soc0/40800000.bus/40a50000.i2c/i2c-1/1-0038/input/input1
[ 1.896619] input: step_detector as /devices/soc0/rpmsg-sensor/input/input2
[ 1.904238] input: step_counter as /devices/soc0/rpmsg-sensor/input/input3
[ 1.913696] i2c /dev entries driver
[ 1.919112] uvcvideo: Unable to create debugfs directory
[ 1.924616] usbcore: registered new interface driver uvcvideo
[ 1.930363] USB Video Class driver (1.1.1)
[ 1.935122] __power_supply_register: Expected proper parent device for 'battery'
[ 1.943554] __power_supply_register: Expected proper parent device for 'usb'
[ 1.954602] device-mapper: uevent: version 1.0.3
[ 1.959890] device-mapper: ioctl: 4.41.0-ioctl (2019-09-16) initialised: [email protected]
[ 1.969636] Bluetooth: HCI UART driver ver 2.3
[ 1.974277] Bluetooth: HCI UART protocol H4 registered
[ 1.979420] Bluetooth: HCI UART protocol BCSP registered
[ 1.984886] Bluetooth: HCI UART protocol LL registered
[ 1.990088] Bluetooth: HCI UART protocol Three-wire (H5) registered
[ 1.996442] Bluetooth: HCI UART protocol Marvell registered
[ 2.002429] usbcore: registered new interface driver btusb
[ 2.008964] sdhci: Secure Digital Host Controller Interface driver
[ 2.015199] sdhci: Copyright(c) Pierre Ossman
[ 2.019551] sdhci-pltfm: SDHCI platform and OF driver helper
[ 2.026911] hidraw: raw HID events driver (C) Jiri Kosina
[ 2.038066] usbcore: registered new interface driver usbhid
[ 2.043712] usbhid: USB HID core driver
[ 2.048496] ashmem: initialized
[ 2.052380] imx-rproc imx7ulp-cm4: failed to find syscon
[ 2.058016] imx-rproc imx7ulp-cm4: mbox_request_channel_byname() could not locate channel named "txdb"
[ 2.067369] imx-rproc imx7ulp-cm4: No txdb, ret 0
[ 2.072456] remoteproc remoteproc0: imx-rproc is available
[ 2.078002] remoteproc remoteproc0: powering up imx-rproc
[ 2.083440] remoteproc remoteproc0: Synchronizing with preloaded co-processor
[ 2.090597] remoteproc remoteproc0: no dtb rsrc-table
[ 2.095685] imx-rproc imx7ulp-cm4: Invalid rsrc table header
[ 2.101385] imx-rproc imx7ulp-cm4: imx_rproc_start: IPC only
[ 2.107081] remoteproc remoteproc0: remote processor imx-rproc is now up
[ 2.118173] galcore: clk_get vg clock failed, disable vg!
[ 2.124236] Galcore version 6.4.3.p1.305572
[ 2.251203] [drm] Initialized vivante 1.0.0 20170808 for 41800000.gpu on minor 0
[ 2.260787] usbcore: registered new interface driver snd-usb-audio
[ 2.275043] imx-audio-rpmsg sound-rpmsg: no reserved DMA memory for rpmsg device
[ 2.282562] imx-audio-rpmsg sound-rpmsg: ASoC: failed to init link rpmsg hifi: -517
[ 2.290397] imx-audio-rpmsg sound-rpmsg: snd_soc_register_card failed (-517)
[ 2.298809] NET: Registered protocol family 26
[ 2.303338] netem: version 1.3
[ 2.306394] u32 classifier
[ 2.309102] input device check on
[ 2.312793] Actions configured
[ 2.317921] xt_time: kernel timezone is -0000
[ 2.322567] gre: GRE over IPv4 demultiplexor driver
[ 2.327528] IPv4 over IPsec tunneling driver
[ 2.333284] Initializing XFRM netlink socket
[ 2.337611] IPsec XFRM device driver
[ 2.342217] NET: Registered protocol family 10
[ 2.349095] Segment Routing with IPv6
[ 2.353241] mip6: Mobile IPv6
[ 2.357664] sit: IPv6, IPv4 and MPLS over IPv4 tunneling driver
[ 2.366174] NET: Registered protocol family 17
[ 2.370671] NET: Registered protocol family 15
[ 2.375289] can: controller area network core (rev 20170425 abi 9)
[ 2.381611] NET: Registered protocol family 29
[ 2.386172] can: raw protocol (rev 20170425)
[ 2.390445] can: broadcast manager protocol (rev 20170425 t)
[ 2.396201] can: netlink gateway (rev 20190810) max_hops=1
[ 2.402250] Bluetooth: RFCOMM TTY layer initialized
[ 2.407335] Bluetooth: RFCOMM socket layer initialized
[ 2.412475] Bluetooth: RFCOMM ver 1.11
[ 2.416274] Bluetooth: BNEP (Ethernet Emulation) ver 1.3
[ 2.421582] Bluetooth: BNEP filters: protocol multicast
[ 2.426847] Bluetooth: BNEP socket layer initialized
[ 2.431810] Bluetooth: HIDP (Human Interface Emulation) ver 1.2
[ 2.437766] Bluetooth: HIDP socket layer initialized
[ 2.442853] l2tp_core: L2TP core driver, V2.0
[ 2.447227] l2tp_ppp: PPPoL2TP kernel driver, V2.0
[ 2.452018] lib80211: common routines for IEEE802.11 drivers
[ 2.461684] Registering SWP/SWPB emulation handler
[ 2.470172] registered taskstats version 1
[ 2.474541] Loading compiled-in X.509 certificates
[ 2.479681] Key type ._fscrypt registered
[ 2.483833] Key type .fscrypt registered
[ 2.487762] Key type fscrypt-provisioning registered
[ 2.496642] pstore: Using crash dump compression: deflate
[ 2.510941] imx-audio-rpmsg sound-rpmsg: no reserved DMA memory for rpmsg device
[ 2.518715] imx-audio-rpmsg sound-rpmsg: ASoC: failed to init link rpmsg hifi: -517
[ 2.526481] imx-audio-rpmsg sound-rpmsg: snd_soc_register_card failed (-517)
[ 2.546293] imx-audio-rpmsg sound-rpmsg: no reserved DMA memory for rpmsg device
[ 2.554046] imx-audio-rpmsg sound-rpmsg: ASoC: failed to init link rpmsg hifi: -517
[ 2.561709] imx-audio-rpmsg sound-rpmsg: snd_soc_register_card failed (-517)
[ 2.574048] imx-audio-rpmsg sound-rpmsg: no reserved DMA memory for rpmsg device
[ 2.581573] imx-audio-rpmsg sound-rpmsg: ASoC: failed to init link rpmsg hifi: -517
[ 2.589385] imx-audio-rpmsg sound-rpmsg: snd_soc_register_card failed (-517)
[ 2.598246] cfg80211: Loading compiled-in X.509 certificates for regulatory database
[ 2.611625] cfg80211: Loaded X.509 cert 'sforshee: 00b28ddf47aef9cea7'
[ 2.618701] platform regulatory.0: Direct firmware load for regulatory.db failed with error -2
[ 2.628233] ALSA device list:
[ 2.631215] No soundcards found.
[ 2.634928] platform regulatory.0: Falling back to sysfs fallback for: regulatory.db
[ 2.645328] Freeing unused kernel memory: 1024K
[ 2.653392] Run /init as init process
[ 2.662786] random: fast init done
[ 2.671086] init: init first stage started!
[ 2.687949] init: [libfs_mgr]ReadDefaultFstab(): failed to find device default fstab
[ 2.696885] init: Using Android DT directory /proc/device-tree/firmware/android/
[ 2.853886] init: bool android::init::FirstStageMount::InitRequiredDevices(): partition(s) not found in /sys, waiting for their uevent(s): boot, dtbo, metadr

ラベル(1)
タグ(1)
0 件の賞賛
返信
0 返答(返信)