IMX6SOLO GPU GALCORE probe failed

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX6SOLO GPU GALCORE probe failed

854件の閲覧回数
agnel_terry
Contributor III

I have a custom board with IMX6SOLO,

In which when I do an insmod galcore.ko I get the following error.

[ 612.024652] galcore: loading out-of-tree module taints kernel.
[ 612.040708] ERROR: could not get clock /soc/gpu@00130000:gpu3d_shader_clk(4)
[ 612.061742] galcore: clk_get gpu3d_shader_clk failed, disable 3d!
[ 612.067905] galcore: clk_get vg clock failed, disable vg!
[ 612.074807] Galcore version 6.2.4.150331
[ 612.723487] [galcore]: Feature database is not found,chipModel=0x0, chipRevision=0x0,

productID=0x0, ecoID=0x0, customerID=0x0
[ 612.799677] galcore: probe of 130000.gpu failed with error -22

 

The Kernel Version I use is 4.9.123

The build environment is Buildroot.

My Device tree config is as follows

gpu@00130000 {
compatible = "fsl,imx6q-gpu";
reg = <0x00130000 0x4000>, <0x00134000 0x4000>,
<0x02204000 0x4000>, <0x10000000 0x0>,
<0x0 0x8000000>;
reg-names = "iobase_3d", "iobase_2d",
"iobase_vg", "phys_baseaddr",
"contiguous_mem";
interrupts = <0 9 IRQ_TYPE_LEVEL_HIGH>,
<0 10 IRQ_TYPE_LEVEL_HIGH>,
<0 11 IRQ_TYPE_LEVEL_HIGH>;
interrupt-names = "irq_3d", "irq_2d", "irq_vg";
clocks = <&clks IMX6QDL_CLK_GPU2D_AXI>, <&clks IMX6QDL_CLK_OPENVG_AXI>,
<&clks IMX6QDL_CLK_GPU3D_AXI>, <&clks IMX6QDL_CLK_GPU2D_CORE>,
<&clks IMX6QDL_CLK_GPU3D_CORE>, <&clks IMX6QDL_CLK_GPU3D_SHADER>;
clock-names = "gpu2d_axi_clk", "openvg_axi_clk",
"gpu3d_axi_clk", "gpu2d_clk",
"gpu3d_clk", "gpu3d_shader_clk";
resets = <&src 0>, <&src 3>, <&src 3>;
reset-names = "gpu3d", "gpu2d", "gpuvg";
power-domains = <&gpc 1>;
};

This works in Imx6Q and not in IMX6SOLO , can you please tell why its failing in IMX6SOLO

Thanks and Regards

Terry

 

 

 

0 件の賞賛
返信
2 返答(返信)

851件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Terry

 

nxp does not support buildroot, also L4.9.123 does not support i.MX6 as described on

below link

 

1.jpg

 

https://www.nxp.com/design/software/embedded-software/i-mx-software/embedded-linux-for-i-mx-applicat...

 

One can test it on nxp sabresd board using any i.MX6 Demo Images from above link and

Chapter 5 Enabling Solo Emulation  i.MX Linux User’s Guide​

 

Best regards
igor

0 件の賞賛
返信

842件の閲覧回数
agnel_terry
Contributor III

Thank you Igor.

0 件の賞賛
返信