hi!
I am using INTEL pc82573E(pcie to 1000Gbit ethernet) on our custom IMX6Q board based on SabreSD board. but it seems that could not recognise the devcie properly.
the kernel is Linux 3.0.35-imx,and we choose board (mx6q_sabresd) on LTIB config.
here is what i have done:
add a star to:
System Type -> Freescale MXC Implementations -> PCI Express support
Bus support -> Message Signaled Interrupts (MSI and MSI-X)
Bus support -> PCI Express Support
Device Drivers -> Network Device support -> Ethernet (1000 Mbit)
Device Drivers -> Network Device support -> Ethernet (1000 Mbit) -> Realtek 8169 gigabit ethernet support
Device Drivers -> Network Device support -> Ethernet (1000 Mbit) -> Intel(R) PRO/1000 Gigabit Ethernet support
Device Drivers -> Network Device support -> Ethernet (1000 Mbit) -> Intel(R) PRO/1000 PCI-Express Gigabit Ethernet support
Device Drivers -> Network Device support -> Ethernet (1000 Mbit) -> IP1000 Gigabit Ethernet support
Device Drivers -> Network Device support -> Ethernet (1000 Mbit) -> Intel(R) 82575/82576 PCI-Express Gigabit Ethernet support
Device Drivers -> Network Device support -> Ethernet (1000 Mbit) -> Intel(R) 82576 Virtual Function Ethernet support
and remove the star from: make menuconfig -> Device Drivers -> Network Device support -> Ethernet (10 or 100Mb)
after compile the kernel i use MfgTool2 to load the uImage to the emmc on board.
After reset the board, here is the log about pcie on system boot:
---------------------------------------------------------------------------
iMX6 PCIe PCIe RC mode imx_pcie_pltfm_probe entering.
PCIE: imx_pcie_pltfm_probe start link up.
IMX PCIe port: link up.
PCI: bus0: Fast back to back transfers disabled
PCI: bus1: Fast back to back transfers enabled
pci 0000:00:00.0: BAR 0: assigned [mem 0x01000000-0x010fffff 64bit pref]
pci 0000:00:00.0: BAR 0: set to [mem 0x01000000-0x010fffff 64bit pref] (PCI address [0x1000000-0x10fffff])
pci 0000:00:00.0: BAR 6: assigned [mem 0x01100000-0x0110ffff pref]
pci 0000:00:00.0: PCI bridge to [bus 01-01]
pci 0000:00:00.0: bridge window [io disabled]
pci 0000:00:00.0: bridge window [mem disabled]
pci 0000:00:00.0: bridge window [mem pref disabled]
PCI: enabling device 0000:00:00.0 (0000 -> 0003)
IMX usb wakeup probe
add wake up source irq 75
**
**
e1000: Intel(R) PRO/1000 Network Driver - version 7.3.21-k8-NAPI
e1000: Copyright (c) 1999-2006 Intel Corporation.
e1000e: Intel(R) PRO/1000 Network Driver - 1.3.10-k2
e1000e: Copyright(c) 1999 - 2011 Intel Corporation.
Intel(R) Gigabit Ethernet Network Driver - version 3.0.6-k2
Copyright (c) 2007-2011 Intel Corporation.
Intel(R) Virtual Function Network Driver - version 1.0.8-k0
Copyright (c) 2009 - 2010 Intel Corporation.
-----------------------------------------------------
when i login into the system, i use the ifconfig command,but there is no eth device:
-------------------------
root@freescale ~$ ifconfig
root@freescale ~$
-------------------------
while when i use the lspci,here is the output:
---------------------------------------
root@freescale ~$ lspci
00:00.0 Class 0604: 16c3:abcd
root@freescale ~$ lspci -mk
00:00.0 "Class 0604" "16c3" "abcd" "0000" "0000" "pcieport"
---------------------------------------
i am a newer to pcie, so i have no idea to locate the problem !
Any advise would be greatful!
Best Regards
geliter
Hi zhaosong
it may be suggested to get updated intel driver for that chip or try
more new kernel, which has more devices supported
L3.10.17_1.0.0_IMX6QDLS_BUNDLE : Source Code Download Steps Documentation and Demo Images.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
hi igor!
i could not found the imx-3.10.17-1.0.0-ga-mfg-tools.tar.gz on the internet.
would you please give me a link to that tools,so that i could try the yocto images!
thanks!
Best regards
geliter
Hi geliter
please look below
IMX_6_MFG_L3.10.17_1.0.0_TOOL : i.MX 6Family Manufacturing Toolkit for L3.10.17
~igor
hi igor!
sorry for delay reply! my problem is still not resolved.
i have tried the ubuntu system,and could get more information through the lspci -v .
could see any thing is wrong on the information below
i will try other kernels later.
---------------------------------------------------------------------------------------------------
root@linaro-ubuntu-desktop:~# lspci -v
00:00.0 PCI bridge: Device 16c3:abcd (rev 01) (prog-if 00 [Normal decode])
Flags: fast devsel
Memory at 01000000 (64-bit, prefetchable) [disabled] [size=1M]
Bus: primary=00, secondary=00, subordinate=00, sec-latency=0
I/O behind bridge: 00000000-00000fff
Memory behind bridge: 00000000-000fffff
Prefetchable memory behind bridge: 00000000-000fffff
[virtual] Expansion ROM at 01100000 [disabled] [size=64K]
Capabilities: [40] Power Management version 3
Capabilities: [50] MSI: Enable- Count=1/1 Maskable+ 64bit+
Capabilities: [70] Express Root Port (Slot-), MSI 00
Capabilities: [100] Advanced Error Reporting
Capabilities: [140] Virtual Channel
Kernel driver in use: pcieport
----------------------------------------------------------------------------------------------------
Best regards
geliter
Hi Zhasong, in addition to Igor's suggestions, I just want to add that :
IMX PCIe port: link up
seems to indicate that PCIe is seeing your card properly but
later on when you issue lspci , it doesn't look like it is
listing your card :
root@freescale ~$ lspci
00:00.0 Class 0604: 16c3:abcd
I believe this is the pcie root. Do you ever get your ethernet card's id as
a result of lspci ?
Which kernel version are you using ? You can also try the mainline
kernel if you haven't yet.
Lastly, if this is your custom board, verify the power on
gpio is defined properly for the kernel. Are you able to
use any other pcie card successfully on your custom board ?
Hope this helps
Regards
Sinan Akman
hi Sinan Akman!
I have not get the ethernet card's id as a result of lspci. unfortunately,i have only this pcie card on my hand.
while the vesion of the kernel is
-------------------------------------------------------------------------
root@linaro-ubuntu-desktop:~# cat /proc/version
Linux version 3.0.35-2666-gbdde708 (root@imx) (gcc version 4.6.2 20110630 (prerelease) (Freescale MAD -- Linaro 2011.07 -- Built at 2011/08/10 09:20) ) #5 SMP PREEMPT Sun Jan 4 18:23:53 CST 2015
-------------------------------------------------------------------------
maybe this kernel is two old.
i will check the power on gpio for the kernel and try more kernel.
Thanks for your suggestion!
Best regards
geliter