IMX6D PCIe I/O DC Parameters

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX6D PCIe I/O DC Parameters

497件の閲覧回数
tomsaluzzo
Contributor III

Refer to page 39 of the IMX6DQAEC (Rev 4) Datasheet. Section 4.6.2 lists the DC parameters for GPIO pads. Do the DC parameters listed in Section 4.6.2 apply to pads that are in power domains powered from the VDDHIGH_CAP (2.5V) internal LDO? In other words, do the DC parameters in section 4.6.2 apply to the I/O lines of the PCIE Module (which is powered from VDDHIGH_CAP = 2.5V)?

ラベル(1)
0 件の賞賛
返信
1 返信

431件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Tom

Table 22. GPIO I/O DC Parameters have "OVDD" as voltage - this

is power domain for pad listed in Table 100. 21 x 21 mm Functional Contact Assignments

as "Power Group". PCIe are analog signals, not GPIOs comply with PCIe specifications.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信