Thank you for your reply.
The environment and setup are the same. The only difference I know is the Dual lite has 1GB of ram and the solo is 512MB but the everything is setup to only use 512.
I found out that the SOLO has an issue as well that it will sometimes stop updating the display. The processor is still running but the display becomes frozen. The back light is also flashing a few times before the display stops updating. Seems like a memory issue that something is being written to at the same time or overwritten. I'm using a bdi3000 to attempt to debug but when it crashes the back trace doesn't go up very far if any frames at all. Any thoughts on what could be checked to see if memory is getting stepped on?
Thank you,
Micah Rudy