IMX6 - IPU CSI IC MEM path with output greater than 1024

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

IMX6 - IPU CSI IC MEM path with output greater than 1024

820 次查看
allan-navarro
Contributor I

Hello 

I'm using the CSI IC MEM path to scale the images coming directly from the CSI without going to memory first. I know the limitation of 1024 pixels and I know it's possible to split the buffer into two stripes to handle greater sizes. I'm wondering if it is possible to make this split when image comes from the CSI and not from memory?

I'm using the ioctl VIDIOC_S_INPUT to choose the path and also setting  fmt.fmt.pix to the desired scaled output. I'm curious how can I specify this task split?

Embedded SW Engineer at RidgeRun

Contact us: support@ridgerun.com
Developers wiki: https://developer.ridgerun.com/
Website: www.ridgerun.com
标记 (2)
0 项奖励
回复
1 回复

794 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

As far as I know this is a limitation of IPU, but it sounds possible what you asked but when the IPU appears it won't work.

regards

0 项奖励
回复