IMX28 USB Package CRC ERROR

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

IMX28 USB Package CRC ERROR

1,537 次查看
liuxing
Contributor II

Hi All,

    We encounter a very strange issue.We set up USB communication via IMX28 Host and device side.But we can see a lot of CRC errors from USB analyzer.

    We analyze the error package and find the  CRC value in the package is the CRC value befor final XOR.

    How to debug this issue?  Is there any register about the usb package CRC?

     pastedImage_1.png

    pastedImage_2.png

标签 (1)
0 项奖励
回复
2 回复数

1,281 次查看
liuxing
Contributor II

Hi All,

   We find that the all error packages are sent from usb device to usb host.

0 项奖励
回复

1,280 次查看
igorpadykov
NXP Employee
NXP Employee

Hi liu

one can look for steps of USB configuring in app note

http://cache.nxp.com/files/32bit/doc/app_note/AN4589.pdf

also please try to test i.MX28 usb module using testmodes

test, generating test patterns,(attached are for i.MX6),

one can add these codes to i.MX28 obds stmp_usb.c

Lab and Test Software (1)

"IMX_OBDS  : On-Board Diagnostic Suit for the i.MX28"

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=MCIMX28EVKJ&fpsp=1&tab=Design_Tools_T...

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复