How to test the GPU of imx

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to test the GPU of imx

1,304 Views
westbrook
Contributor III

Hi Guys,

I am using imx6 solo with X11, kernel 4.9.11, gpu driver 6.2.2 in kernel, and I add following gpu packages to filesystem:

imx-gpu-viv-6.2.2

gpu-viv-g2d-6.2.2

xf86-video-imx-viv-6.2.2.p0

 

From /var/log/Xorg.0.log, I can see that the GPU driver loaded successfully. I want to know, how to test the GPU functions, it should be some demos?

Thank you in advance.

BR,

Xiao

Labels (1)
0 Kudos
2 Replies

1,010 Views
igorpadykov
NXP Employee
NXP Employee

Hi Xiao

one can test with gpu unit test:

imx-test.git - i.MX Driver Test Application Software 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos

1,010 Views
westbrook
Contributor III

Hi Igor,

Thanks for your quick reply, I will try this tool.

Best Regards,
Xiao

0 Kudos