Hi
I want to connet the printer by USB or LAN on IMX6DL.
The rootfs is built normally, so it doesn't have cups,right?
Could I follow the step mentioned in Linux cups | NXP for fsl-yocto-L4.1.15_2.0.0-ga?
On the other hand, Some HP printers need hplip and hplip-plugin.
How to install those into the system?
Regards
Mihan
Hi 铭恒 李
one can follow yocto tutorials:
https://community.nxp.com/docs/DOC-95333
i.MX Yocto Project: How can I (quickly) modify the kernel and test it?
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi
I got cups and hplip by adding IMAGE_INSTALL_append = " cups" and IMAGE_INSTALL_append = " hplip" in local.conf.
but when I run hp-check, there are some errors about missing required dependencies
some dependencies are not in list