Hi All,
I am trying wl12xx wifi enable in dts files
wlan_en_reg: fixedregulator {
compatible = "regulator-fixed";
regulator-min-microvolt = <1800000>;
regulator-max-microvolt = <1800000>;
regulator-name = "wlan_enable_regulator";
gpios = <&gpio1 15 0>; //active high
startup-delay-us = <70000>;
enable-active-high;
};
&usdhc1 {
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_usdhc1>;
bus-width = <4>;
always_present;
cd-permanent;
cap-power-off-card;
status = "okay";
vmmc-supply = <&wlan_en_reg>;
non-removable; /* non-removable is not a variable, the fact it is */
/* listed is all that is used by driver */
enable-sdio-wakeup;
status = "okay";
#address-cells = <1>;
#size-cells = <0>;
wlcore: wlcore@0 {
compatible = "ti,wl1271";
interrupt-parent = <&gpio1>;
interrupts = <14 IRQ_TYPE_LEVEL_HIGH>;
clocks = <&refclock>;
clock-names = "refclock";
refclock: refclock {
compatible = "ti,wilink-clock";
#clock-cells = <0>;
clock-frequency = <38400000>;
};
};
};
pinctrl_usdhc1: usdhc1grp {
fsl,pins = <
MX6QDL_PAD_SD1_CMD__SD1_CMD 0x17059
MX6QDL_PAD_SD1_CLK__SD1_CLK 0x10059
MX6QDL_PAD_SD1_DAT0__SD1_DATA0 0x17059
MX6QDL_PAD_SD1_DAT1__SD1_DATA1 0x17059
MX6QDL_PAD_SD1_DAT2__SD1_DATA2 0x17059
MX6QDL_PAD_SD1_DAT3__SD1_DATA3 0x17059
MX6QDL_PAD_SD2_DAT0__GPIO1_IO15 0x80000000
MX6QDL_PAD_SD2_DAT1__GPIO1_IO14 0x80000000
>;
};
In this case i got
gpio-15 (wlan_enable_regulato) out lo
in cat /sys/kernel/debug/gpio
After changing
gpios = <&gpio1 15 0>; | //active high |
in to
gpios = <&gpio1 15 1>; | //active high |
also i am getting same as above in sysfs entries but i want out hi instead of out lo how can i get it .
i am using wifi_r8.6 compat wireless.
And
here vmmc-supply = <&wlan_en_reg>; is for io or for wifi module.
i have 2 power supplies 1) 3.3v for wifi module and 2) 1.8 for i/o lines hopw can i configure those two things in sdhc1.
what is vmmc-supply and vqmmc-supply in sdhc or mmc dts properties, if any one knows kindly help me i am new to the dts files.
Thanks & Regards,
Lavanya
已解决! 转到解答。
HI All,
If we want to change out lo to out hi for gpio in 3.14 kernel version we need to enable SION bit in iomux pad settings.
SION is Software Input ON Feild. which allows us to read the value for GPIO .
After enabling SION i can able to see the changes in my Gpio value in /sys/kernel/debug/gpio.
HI All,
If we want to change out lo to out hi for gpio in 3.14 kernel version we need to enable SION bit in iomux pad settings.
SION is Software Input ON Feild. which allows us to read the value for GPIO .
After enabling SION i can able to see the changes in my Gpio value in /sys/kernel/debug/gpio.