I need to run a 32-bit application on the imx8m plus board but that needs multilib support.While bitbaking, I had an error with the devIL recipe, which I fixed by a method followed by the same issue fixed in the community, after which I received a linker error with imx-gpu-sdk saying that the lIL lib was not found.How can I fix this error?
DemoApp.Util.Graphics.a -lIL DemoFramework/FslDemoHost/Console/libFslDemoHost.Console.a DemoFramework/FslDemoPlatform/Link/libFslDemoPlatform.Link.a DemoFramework/FslDemoPlatform/libFslDemoPlatform.a DemoFramework/FslDemoHost/Base/libFslDemoHost.Base.a DemoFramework/FslDemoApp/Base/libFslDemoApp.Base.a DemoFramework/FslNativeWindow/Base/libFslNativeWindow.Base.a DemoFramework/FslDemoApp/Shared/libFslDemoApp.Shared.a DemoFramework/FslGraphics/libFslGraphics.a DemoFramework/FslDemoService/CpuStats/Impl/libFslDemoService.CpuStats.Impl.a DemoFramework/FslService/Impl/libFslService.Impl.a DemoFramework/FslService/Consumer/libFslService.Consumer.a DemoFramework/FslVersion/libFslVersion.a DemoFramework/FslBase/libFslBase.a -s -lfmt && :
| /home/mysticp0004/var-fsl-yocto/build_xwayland/tmp/work/armv8a-mx8mp-fslc-linux/imx-gpu-sdk/6.0.2-r0/recipe-sysroot-native/usr/bin/aarch64-fslc-linux/../../libexec/aarch64-fslc-linux/gcc/aarch64-fslc-linux/11.3.0/ld: cannot find -lIL: No such file or directory
| collect2: error: ld returned 1 exit status
| [1450/2889] Building CXX object DemoFramework/FslUtil/Vulkan1_0/UnitTest/Helper/CMakeFiles/FslUtil.Vulkan1_0.UnitTest.Helper.dir/home/mysticp0004/var-fsl-yocto/build_xwayland/tmp/work/armv8a-mx8mp-fslc-linux/imx-gpu-sdk/6.0.2-r0/git/DemoFramework/FslUtil/Vulkan1_0/UnitTest/Helper/source/FslUtil/Vulkan1_0/UnitTest/Helper/Dummy.cpp.o
| [1451/2889] Building CXX object DemoFramework/FslUtil/Vulkan1_0/UnitTest/CMakeFiles/FslUtil.Vulkan1_0.UnitTest.dir/home/mysticp0004/var-fsl-yocto/build_xwayland/tmp/work/armv8a-mx8mp-fslc-linux/imx-gpu-sdk/6.0.2-r0/git/DemoFramework/FslUtil/Vulkan1_0/UnitTest/source/FslUtil/Vulkan1_0/UnitTest/Util/Test_DeviceMemoryUtil.cpp.o
| [1452/2889] Building CXX object DemoFramework/FslUtil/Vulkan1_0/UnitTest/CMakeFiles/FslUtil.Vulkan1_0.UnitTest.dir/home/mysticp0004/var-fsl-yocto/build_xwayland/tmp/work/armv8a-mx8mp-fslc-linux/imx-gpu-sdk/6.0.2-r0/git/DemoFramework/FslUtil/Vulkan1_0/UnitTest/source/FslUtil/Vulkan1_0/UnitTest/Util/Test_VUBufferMemory.cpp.o
| ninja: build stopped: subcommand failed.
| WARNING: The build command 'cmake --build . --target install -- -j 4' failed with '1'. It was run with CWD: '/home/mysticp0004/var-fsl-yocto/build_xwayland/tmp/work/armv8a-mx8mp-fslc-linux/imx-gpu-sdk/6.0.2-r0/git/build/Yocto/Ninja/release'