How maximum FPC cable distance should I use for MIPI DSI LCD ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How maximum FPC cable distance should I use for MIPI DSI LCD ?

ソリューションへジャンプ
1,799件の閲覧回数
talel_hajsalem
Contributor III

Hello,

I'm working on a custom IMX8MM board, and I have an LCD display.

when using a 5cm FPC cable and its working, but when using 10cm or 20cm it does not work.

If I decrement the pixel clock it sometimes work.

How maximum length should I don't pass?

Thanks,

Talel

ラベル(1)
0 件の賞賛
1 解決策
1,792件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Talel

 

cable length depends on many factors, including cable material, signal losses in board/cable and

connectors, impedance matching, so I am afraid there is no simple formula to calculate. 

One can try to find it experimentally controlling signal quality by oscilloscope or try to perform ibis modelling.

 

Best regards
igor

元の投稿で解決策を見る

0 件の賞賛
1 返信
1,793件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Talel

 

cable length depends on many factors, including cable material, signal losses in board/cable and

connectors, impedance matching, so I am afraid there is no simple formula to calculate. 

One can try to find it experimentally controlling signal quality by oscilloscope or try to perform ibis modelling.

 

Best regards
igor

0 件の賞賛