How does imx6 solo support two lvds with different standard output

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How does imx6 solo support two lvds with different standard output

707 Views
songyonglai
Contributor II

Hi all:

   I want to use two lvds  on IMX6 DL , lvds0 and lvds1 with different standard output, for example ,lvds0 XGA output, lvds1    WSVGA output, and with different output , so I try the uboot paramter bootargs :

setenv bootargs ${bootargs} video=mxcfb0:dev=ldb,LDB-XGA,if=RGB24 ldb=sep1 video=mxcfb1:dev=ldb,LDB-WSVGA,if=RGB24  root=/dev/mmcblk0p1 rootwait rw  '

but It does work , only mxcfb1 has output ,  I use the L3.0.35_4.1.0_130816_source sdk,Can somebody help me,, thanks very much

0 Kudos
1 Reply

403 Views
igorpadykov
NXP Employee
NXP Employee

Hi song

seems it is necessary to modify sources as suggested on post [14.08.2013 0:34]  

https://community.nxp.com/docs/DOC-93449

and add struct :fb_videomode timings for new WSVGA lcd, as in example

https://community.freescale.com/thread/383078

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos