Hang when up AP6256 Wifi module

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Hang when up AP6256 Wifi module

1,386 Views
DungTA98
Contributor II

Hi,

 

I'm trying to port the AP6256 Wifi module to a board that uses i.MX 8M Mini.
When I use in kernel 4.9, wifi module works well. But  I use it in kernel 5.15, it hang when I run

ifconfig wlan0 up

This is my log with kernel 4.9 (Wifi module works well)

root@mys-8mmx:~# ifconfig wlan0 up
[ 69.855899] [dhd] dhd_open: Enter wlan0
[ 69.859776] [dhd] dhd_open : no mutex held. set lock
[ 69.864775] [dhd]
[ 69.864775] Dongle Host Driver, version 100.10.545.12 (r826445-20200708-1)
[ 69.873672] [dhd-wlan0] wl_android_wifi_on : in g_wifi_on=0
[ 69.879272] [dhd] wifi_platform_set_power = 1, delay: 200 msec
[ 69.885131] [dhd] ======== PULL WL_REG_ON(42) HIGH! ========
[ 70.279593] mmc0: queuing unknown CIS tuple 0x80 (2 bytes)
[ 70.292059] mmc0: queuing unknown CIS tuple 0x80 (3 bytes)
[ 70.303921] mmc0: queuing unknown CIS tuple 0x80 (3 bytes)
[ 70.320842] mmc0: queuing unknown CIS tuple 0x80 (7 bytes)
[ 70.340306] mmc0: queuing unknown CIS tuple 0x81 (9 bytes)
[ 70.638913] [dhd] sdioh_start: set sd_f2_blocksize 256
[ 70.644964] [dhd]
[ 70.644964]
[ 70.644964] dhd_bus_devreset: == Power ON ==
[ 70.652862] [dhd] F1 signature read @0x18000000=0x15294345
[ 70.661067] [dhd] F1 signature OK, socitype:0x1 chip:0x4345 rev:0x9 pkg:0x2
[ 70.668487] [dhd] DHD: dongle ram size is set to 819200(orig 819200) at 0x198000
[ 70.675949] [dhd] dhd_bus_devreset: making DHD_BUS_DOWN
[ 70.681240] [dhd] dhdsdio_probe_init: making DHD_BUS_DOWN
[ 70.689418] [dhd] dhd_conf_read_config : Ignore config file /lib/firmware/bcmd/config.txt
[ 70.697650] [dhd] dhd_conf_set_path_params : Final fw_path=/lib/firmware/bcmd/fw_bcm43456c5_ag_apsta.bin
[ 70.707146] [dhd] dhd_conf_set_path_params : Final nv_path=/lib/firmware/bcmd/nvram_ap6256.txt
[ 70.715765] [dhd] dhd_conf_set_path_params : Final clm_path=/lib/firmware/bcmd/clm_bcm43456c5_ag.blob
[ 70.725012] [dhd] dhd_conf_set_path_params : Final conf_path=/lib/firmware/bcmd/config.txt
[ 70.733743] [dhd] dhd_os_open_image1: /lib/firmware/bcmd/fw_bcm43456c5_ag_apsta.bin (612864 bytes) open success
[ 70.787000] [dhd] dhd_os_open_image1: /lib/firmware/bcmd/nvram_ap6256.txt (2874 bytes) open success
[ 70.798461] [dhd] NVRAM version: AP6256_NVRAM_V1.4_06112021
[ 70.804532] [dhd] dhdsdio_write_vars: Download, Upload and compare of NVRAM succeeded.
[ 70.900899] [dhd] dhd_bus_init: enable 0x06, ready 0x06 (waited 0us)
[ 70.909093] [dhd] dhd_tcpack_suppress_set: TCP ACK Suppress mode 2 -> mode 1
[ 70.916896] [dhd] dhd_apply_default_clm: Ignore clm file /lib/firmware/bcmd/clm_bcm43456c5_ag.blob
[ 70.926436] [dhd] Firmware up: op_mode=0x0002, MAC=d4:9c:dd:3d:7c:6c
[ 70.936159] [dhd] dhd_preinit_ioctls: event_log_max_sets: 26 ret: -23
[ 70.946099] [dhd] Driver: 100.10.545.12 (r826445-20200708-1)
[ 70.946099] Firmware: wl0: Jun 25 2021 17:13:38 version 7.45.96.94 (7bb6b14@SYNA) (r745790) FWID 01-2bdfb64c es7.c5.n4.a3
[ 70.946099] CLM: 9.2.9 (2016-02-03 04:34:31)
[ 70.967976] [dhd] dhd_txglom_enable: enable 1
[ 70.972353] [dhd] dhd_conf_set_txglom_params : txglom_mode=multi-desc
[ 70.978808] [dhd] dhd_conf_set_txglom_params : txglomsize=36, deferred_tx_len=0
[ 70.986144] [dhd] dhd_conf_set_txglom_params : txinrx_thres=128, dhd_txminmax=-1
[ 70.993608] [dhd] dhd_conf_set_txglom_params : tx_max_offset=0, txctl_tmo_fix=300
[ 71.001117] [dhd] dhd_conf_get_disable_proptx : fw_proptx=1, disable_proptx=-1
[ 71.011255] [dhd] dhd_pno_init: Support Android Location Service
[ 71.033819] [dhd] dhd_preinit_ioctls: Failed to get preserve log # !
[ 71.060560] [dhd] dhd_conf_map_country_list : CN/38
[ 71.060566] [dhd] dhd_wlfc_enable: ret=0
[ 71.060595] [dhd] CFG80211-ERROR) wl_cfg80211_event : Event handler is not created
[ 71.065470] [dhd] dhd_conf_set_country : set country CN, revision 38
[ 71.069446] [dhd] CFG80211-ERROR) wl_cfg80211_event : Event handler is not created
[ 71.091451] [dhd] dhd_conf_set_country : Country code: CN (CN/38)
[ 71.102099] [dhd-wlan0] wl_android_wifi_on : Success
[ 71.127522] [dhd] _dhd_wlfc_mac_entry_update():1866, entry(32)
[ 71.152079] [dhd] dhd_open : the lock is released.
[ 71.156889] [dhd] dhd_open: Exit wlan0 ret=0
[ 71.161181] [dhd] [wlan0] tx queue started

In kernel 5.15, it hang after

[ 71.127522] [dhd] _dhd_wlfc_mac_entry_update():1866, entry(32)

Can you help me?

Many thank,
Dung Tran Anh

Labels (1)
0 Kudos
Reply
2 Replies

1,379 Views
jimmychan
NXP TechSupport
NXP TechSupport

It seems is the firmware and the driver issues. Please check with the wifi module supplier that the firmware could work on L5.15.

0 Kudos
Reply

1,375 Views
DungTA98
Contributor II

I think the driver have not issue. When I ran modprobe bcmdhd, the wifi module initialized fine.

modprobe bcmdhd

6.630814] [dhd] dhd_module_init: in Dongle Host Driver, version 100.10.545.12 (r826445-20200708-1)
[ 6.651701] [dhd] ======== dhd_wlan_init_plat_data ========
[ 6.657866] [dhd] dhd_wlan_init_gpio: WL_REG_ON=42
[ 6.663846] [dhd] dhd_wifi_platform_load: Enter
[ 6.669474] [dhd] Power-up adapter 'DHD generic adapter'
[ 6.747286] [dhd] wifi_platform_set_power = 1, delay: 200 msec
[ 6.768108] [dhd] ======== PULL WL_REG_ON(42) HIGH! ========
[ 7.282590] [dhd] wifi_platform_bus_enumerate device present 1
[ 7.288506] [dhd] ======== Card detection to detect SDIO card! ========
[ 7.310839] [dhd] bcmsdh_register: register client driver
[ 7.316759] [dhd] bcmsdh_sdmmc_probe: Enter num=1
[ 7.321843] [dhd] bcmsdh_sdmmc_probe: Enter num=2
[ 7.326682] [dhd] bus num (host idx)=0, slot num (rca)=1
[ 7.332213] [dhd] found adapter info 'DHD generic adapter'
[ 7.338647] [dhd] sdioh_attach: set sd_f2_blocksize 256
[ 7.344040] [dhd] sdioh_attach: sd clock rate = 0
[ 7.349184] [dhd] dhdsdio_probe : no mutex held. set lock
[ 7.354745] [dhd] F1 signature read @0x18000000=0x15294345
[ 7.362635] [dhd] F1 signature OK, socitype:0x1 chip:0x4345 rev:0x9 pkg:0x2
[ 7.370097] [dhd] DHD: dongle ram size is set to 819200(orig 819200) at 0x198000
[ 7.377711] [dhd] dhd_conf_set_chiprev : chip=0x4345, chiprev=9
[ 7.384685] [dhd] CFG80211-ERROR) wl_cfg80211_netdev_notifier_call : wdev null. Do nothing
[ 7.393048] [dhd] CFG80211-ERROR) wl_cfg80211_netdev_notifier_call : wdev null. Do nothing
[ 7.393053] [dhd] CFG80211-ERROR) wl_cfg80211_netdev_notifier_call : wdev null. Do nothing
[ 7.414211] dhd_attach(): thread:dhd_watchdog_thread:257 started
[ 7.422768] dhd_attach(): thread:dhd_dpc:258 started
[ 7.428082] dhd_attach(): thread:dhd_rxf:259 started
[ 7.433189] [dhd] dhd_deferred_work_init: work queue initialized
[ 7.439271] [dhd] dhd_tcpack_suppress_set: TCP ACK Suppress mode 0 -> mode 2
[ 7.446461] [dhd] sdioh_cis_read: func_cis_ptr[0]=0x10ac
[ 7.457672] [dhd] dhdsdio_probe_init: making DHD_BUS_DOWN
[ 7.463441] [dhd] Dongle Host Driver, version 100.10.545.12 (r826445-20200708-1)
[ 7.471657] [dhd] Register interface [wlan0] MAC: d4:9c:dd:3d:7c:6c

[ 7.479834] [dhd] dhd_bus_devreset: == Power OFF ==
[ 7.485059] [dhd] dhd_bus_stop: making DHD_BUS_DOWN
[ 7.490080] [dhd] dhd_bus_devreset: making dhdpub up FALSE
[ 7.495607] [dhd] dhd_txglom_enable: enable 0
[ 7.500055] [dhd] dhd_bus_devreset: making DHD_BUS_DOWN
[ 7.500063] [dhd] dhd_bus_devreset: WLAN OFF DONE
[ 7.500229] [dhd] wifi_platform_set_power = 0, delay: 0 msec
[ 7.500233] [dhd] ======== PULL WL_REG_ON(42) LOW! ========
[ 7.500244] [dhd] dhdsdio_probe : the lock is released.
[ 7.500422] [dhd] dhd_module_init: Exit err=0

And I ran iw dev, I seen wlan0 informations.

 

0 Kudos
Reply