HOW TO GET WEIM 32BIT DATA IN MX51

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

HOW TO GET WEIM 32BIT DATA IN MX51

Jump to solution
1,763 Views
arunkmrvn
Contributor II

hi eveyone,

I am using i.mx51 processor connected to FPGA through EMI bus. I want to read and write 32bit data from the FPGA. But Whenever i am going to read, i am getting only 16bit word. Right now i am using multiplexed asynchronous mode  to get 32bit word data. The Registers for configuration is all changed to 32bit. Please see the below confgurations and suggest me anyone, how to get 32bit data from EMI bus.

#define CSGCR1    0x00

#define CSGCR2    0x04

#define CSRCR1    0x08

#define CSRCR2    0x0C

#define CSWCR1    0x10

#define WEIM_CS5_OFFSET 0X78

__raw_writel(0x00F33089, (u32)weim_vbaddr + WEIM_CS5_OFFSET + CSGCR1);

__raw_writel(0x00000002, (u32)weim_vbaddr + WEIM_CS5_OFFSET + CSGCR2);

__raw_writel(0x32260000, (u32)weim_vbaddr + WEIM_CS5_OFFSET + CSRCR1);

__raw_writel(0, (u32)weim_vbaddr + WEIM_CS5_OFFSET + CSRCR2);

__raw_writel(0x72080F00, (u32)weim_vbaddr + WEIM_CS5_OFFSET + CSWCR1);


Read function in driver
static int mxc_emi_read(struct file *file, int *buf,size_t count, loff_t *f_pos)

{

    printk("Emi chipselect5 Read called\n");

    u32 temp;

    u32 address = buf[0];

    temp  =  readl(cs5addr+address);

    printk(KERN_INFO "Data read inside kernel %x\n",temp);

    return temp;

}

What changes have to made to read the 32bit data from FPGA ?

Labels (4)
0 Kudos
Reply
1 Solution
1,540 Views
Yuri
NXP Employee
NXP Employee

Hello,

from the table 52 of the Datasheet :

A[15:0] - EIM_DA[15:0]

A[27:16] -  NANDF_D[11:0]

D[7:0] - EIM_DA[7:0]

D[15:8] - EIM_DA[15:8]

D[23:16] - NANDF_D[7:0]

D[31:24] - NANDF_D[15:8]

Regards,

Yuri.

View solution in original post

7 Replies
1,540 Views
Yuri
NXP Employee
NXP Employee

Hello,

  Please check pin configuration for Multiplexed Address/Data Mode, using
Table 52 (WEIM Interface Pinout in Various Configurations) of the i.MX51
Datasheet.

http://cache.nxp.com/files/dsp/doc/data_sheet/IMX51CEC.pdf?pspll=1 

  Please pay attention on influence of the AUS bit in Chip Select 5 General Configuration

Register 1 (CS5GCR1) - looks like it is set in Your case.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,540 Views
arunkmrvn
Contributor II

I mean, is there any possibility to get 32bit data in EIM DA[0-16] and EIM D[16-31] only. I used some of NAND_F pins as GPIO. So, is there any possibility.

0 Kudos
Reply
1,540 Views
Yuri
NXP Employee
NXP Employee

Hello,

all possible configurations are shown in Table 52 (WEIM Interface Pinout in

Various Configurations) of the i.MX51  Datasheet.

http://cache.nxp.com/files/dsp/doc/data_sheet/IMX51CEC.pdf?pspll=1

Regards,

Yuri.

0 Kudos
Reply
1,540 Views
arunkmrvn
Contributor II

hi yuri,

Its worked after mapped NAND_F lines to hardware. Thanks for your

support

Thanks & Regards,

ARUNKUMAR

0 Kudos
Reply
1,540 Views
arunkmrvn
Contributor II

Hi Yuri Muhin,

I am using in

FPGA lines are mapped to EIM-DA(0-15), EIMD(16-31), EIMA(16-27) and LBA, OE, WE signals.

Address -> EIMDA(0-15) + EIMA(16-27)

Data -> EIMDA(0-15) + EIMD(16-31)

I am using asynchronous communication in multiplexed mode (MUM=1), EIMDA0-DA15 pins (Address & Data ) to get first 16bit Data and EIMD16-D31 (Data) Next 16 bit Data and AUS bit is set. (AUS=1).

This is my pin configuration file

#ifndef __ASM_ARCH_MXC_MX51_PINS_H__

#define __ASM_ARCH_MXC_MX51_PINS_H__

#include "iomux.h"

/*!

* @file arch-mxc/mx51_pins.h

*

* @brief MX51 I/O Pin List

*

* @ingroup GPIO_MX51

*/

#ifndef __ASSEMBLY__

// #define PAD_I_START_MX51        0x3F0

#define PAD_I_START_MX51        0x3F8

#define INPUT_CTL_START_MX51        0x8C4

#define INPUT_CTL_START_MX51_TO1    0x928

#define MUX_I_END_MX51        (PAD_I_START_MX51 - 4)

#define _MXC_BUILD_PIN_MX51(gp, gi, ga, mi, pi) \

    (((gp) << MUX_IO_P) | ((gi) << MUX_IO_I) | \

    ((mi) << MUX_I) | \

    ((pi - PAD_I_START_MX51) << PAD_I) | \

    ((ga) << GPIO_I))

#define _MXC_BUILD_GPIO_PIN_MX51(gp, gi, ga, mi, pi) \

    _MXC_BUILD_PIN_MX51(gp, gi, ga, mi, pi)

#define _MXC_BUILD_NON_GPIO_PIN_MX51(mi, pi) \

    _MXC_BUILD_PIN_MX51(NON_GPIO_PORT, 0, 0, mi, pi)

/*!

* This enumeration is constructed based on the Section

* "sw_pad_ctl & sw_mux_ctl details" of the MX51 IC Spec. Each enumerated

* value is constructed based on the rules described above.

*/

enum iomux_pins_mx51 {

    MX51_PIN_EIM_DA0 = _MXC_BUILD_NON_GPIO_PIN_MX51(0x1C, 0x7A8),

    MX51_PIN_EIM_DA1 = _MXC_BUILD_NON_GPIO_PIN_MX51(0x20, 0x7A8),

    MX51_PIN_EIM_DA2 = _MXC_BUILD_NON_GPIO_PIN_MX51(0x24, 0x7A8),

    MX51_PIN_EIM_DA3 = _MXC_BUILD_NON_GPIO_PIN_MX51(0x28, 0x7A8),

    MX51_PIN_EIM_DA4 = _MXC_BUILD_NON_GPIO_PIN_MX51(0x2C, 0x7AC),

    MX51_PIN_EIM_DA5 = _MXC_BUILD_NON_GPIO_PIN_MX51(0x30, 0x7AC),

    MX51_PIN_EIM_DA6 = _MXC_BUILD_NON_GPIO_PIN_MX51(0x34, 0x7AC),

    MX51_PIN_EIM_DA7 = _MXC_BUILD_NON_GPIO_PIN_MX51(0x38, 0x7AC),

    MX51_PIN_EIM_DA8 = _MXC_BUILD_NON_GPIO_PIN_MX51(0x3C, 0x7B0),

    MX51_PIN_EIM_DA9 = _MXC_BUILD_NON_GPIO_PIN_MX51(0x40, 0x7B0),

    MX51_PIN_EIM_DA10 = _MXC_BUILD_NON_GPIO_PIN_MX51(0x44, 0x7B0),

    MX51_PIN_EIM_DA11 = _MXC_BUILD_NON_GPIO_PIN_MX51(0x48, 0x7B0),

    MX51_PIN_EIM_DA12 = _MXC_BUILD_NON_GPIO_PIN_MX51(0x4C, 0x7BC),

    MX51_PIN_EIM_DA13 = _MXC_BUILD_NON_GPIO_PIN_MX51(0x50, 0x7BC),

    MX51_PIN_EIM_DA14 = _MXC_BUILD_NON_GPIO_PIN_MX51(0x54, 0x7BC),

    MX51_PIN_EIM_DA15 = _MXC_BUILD_NON_GPIO_PIN_MX51(0x58, 0x7BC),

    MX51_PIN_EIM_D16 = _MXC_BUILD_GPIO_PIN_MX51(1, 0, 0, 0x5C, 0x3F0),

    MX51_PIN_EIM_D17 = _MXC_BUILD_GPIO_PIN_MX51(1, 1, 0, 0x60, 0x3F4),

    MX51_PIN_EIM_D18 = _MXC_BUILD_GPIO_PIN_MX51(1, 2, 0, 0x64, 0x3F8),

    MX51_PIN_EIM_D19 = _MXC_BUILD_GPIO_PIN_MX51(1, 3, 0, 0x68, 0x3FC),

    MX51_PIN_EIM_D20 = _MXC_BUILD_GPIO_PIN_MX51(1, 4, 0, 0x6C, 0x400),

    MX51_PIN_EIM_D21 = _MXC_BUILD_GPIO_PIN_MX51(1, 5, 0, 0x70, 0x404),

    MX51_PIN_EIM_D22 = _MXC_BUILD_GPIO_PIN_MX51(1, 6, 0, 0x74, 0x408),

    MX51_PIN_EIM_D23 = _MXC_BUILD_GPIO_PIN_MX51(1, 7, 0, 0x78, 0x40C),

    MX51_PIN_EIM_D24 = _MXC_BUILD_GPIO_PIN_MX51(1, 8, 0, 0x7C, 0x410),

    MX51_PIN_EIM_D25 = _MXC_BUILD_NON_GPIO_PIN_MX51(0x80, 0x414),

    MX51_PIN_EIM_D26 = _MXC_BUILD_NON_GPIO_PIN_MX51(0x84, 0x418),

    MX51_PIN_EIM_D27 = _MXC_BUILD_GPIO_PIN_MX51(1, 9, 0, 0x88, 0x41C),

    MX51_PIN_EIM_D28 = _MXC_BUILD_NON_GPIO_PIN_MX51(0x8C, 0x420),

    MX51_PIN_EIM_D29 = _MXC_BUILD_NON_GPIO_PIN_MX51(0x90, 0x424),

    MX51_PIN_EIM_D30 = _MXC_BUILD_NON_GPIO_PIN_MX51(0x94, 0x428),

    MX51_PIN_EIM_D31 = _MXC_BUILD_NON_GPIO_PIN_MX51(0x98, 0x42C),

    MX51_PIN_EIM_A16 = _MXC_BUILD_GPIO_PIN_MX51(1, 10, 0, 0x9C, 0x430),

    MX51_PIN_EIM_A17 = _MXC_BUILD_GPIO_PIN_MX51(1, 11, 0, 0xA0, 0x434),

    MX51_PIN_EIM_A18 = _MXC_BUILD_GPIO_PIN_MX51(1, 12, 0, 0xA4, 0x438),

    MX51_PIN_EIM_A19 = _MXC_BUILD_GPIO_PIN_MX51(1, 13, 0, 0xA8, 0x43C),

    MX51_PIN_EIM_A20 = _MXC_BUILD_GPIO_PIN_MX51(1, 14, 0, 0xAC, 0x440),

    MX51_PIN_EIM_A21 = _MXC_BUILD_GPIO_PIN_MX51(1, 15, 0, 0xB0, 0x444),

    MX51_PIN_EIM_A22 = _MXC_BUILD_GPIO_PIN_MX51(1, 16, 0, 0xB4, 0x448),

    MX51_PIN_EIM_A23 = _MXC_BUILD_GPIO_PIN_MX51(1, 17, 0, 0xB8, 0x44C),

    MX51_PIN_EIM_A24 = _MXC_BUILD_GPIO_PIN_MX51(1, 18, 0, 0xBC, 0x450),

    MX51_PIN_EIM_A25 = _MXC_BUILD_GPIO_PIN_MX51(1, 19, 0, 0xC0, 0x454),

    MX51_PIN_EIM_A26 = _MXC_BUILD_GPIO_PIN_MX51(1, 20, 0, 0xC4, 0x458),

    MX51_PIN_EIM_A27 = _MXC_BUILD_GPIO_PIN_MX51(1, 21, 0, 0xC8, 0x45C),

    MX51_PIN_EIM_EB0 = _MXC_BUILD_NON_GPIO_PIN_MX51(0xCC, 0x460),

    MX51_PIN_EIM_EB1 = _MXC_BUILD_NON_GPIO_PIN_MX51(0xD0, 0x464),

    MX51_PIN_EIM_EB2 = _MXC_BUILD_GPIO_PIN_MX51(1, 22, 0, 0xD4, 0x468),

    MX51_PIN_EIM_EB3 = _MXC_BUILD_GPIO_PIN_MX51(1, 23, 0, 0xD8, 0x46C),

    MX51_PIN_EIM_OE = _MXC_BUILD_GPIO_PIN_MX51(1, 24, 0, 0xDC, 0x470),

    MX51_PIN_EIM_CS0 = _MXC_BUILD_GPIO_PIN_MX51(1, 25, 0, 0xE0, 0x474),

    MX51_PIN_EIM_CS1 = _MXC_BUILD_GPIO_PIN_MX51(1, 26, 0, 0xE4, 0x478),

    MX51_PIN_EIM_CS2 = _MXC_BUILD_GPIO_PIN_MX51(1, 27, 0, 0xE8, 0x47C),

    MX51_PIN_EIM_CS3 = _MXC_BUILD_GPIO_PIN_MX51(1, 28, 0, 0xEC, 0x480),

    MX51_PIN_EIM_CS4 = _MXC_BUILD_GPIO_PIN_MX51(1, 29, 0, 0xF0, 0x484),

    MX51_PIN_EIM_CS5 = _MXC_BUILD_GPIO_PIN_MX51(1, 30, 0, 0xF4, 0x488),

    MX51_PIN_EIM_DTACK = _MXC_BUILD_GPIO_PIN_MX51(1, 31, 0, 0xF8, 0x48C),

    MX51_PIN_EIM_LBA = _MXC_BUILD_GPIO_PIN_MX51(2, 1, 0, 0xFC, 0x494),

    MX51_PIN_EIM_CRE = _MXC_BUILD_GPIO_PIN_MX51(2, 2, 0, 0x100, 0x4A0),

    MX51_PIN_DRAM_CS1 = _MXC_BUILD_NON_GPIO_PIN_MX51(0x104, 0x4D0),

    MX51_PIN_NANDF_WE_B = _MXC_BUILD_GPIO_PIN_MX51(2, 3, 3, 0x108, 0x4E4),

    MX51_PIN_NANDF_RE_B = _MXC_BUILD_GPIO_PIN_MX51(2, 4, 3, 0x10C, 0x4E8),

    MX51_PIN_NANDF_ALE = _MXC_BUILD_GPIO_PIN_MX51(2, 5, 3, 0x110, 0x4EC),

    MX51_PIN_NANDF_CLE = _MXC_BUILD_GPIO_PIN_MX51(2, 6, 3, 0x114, 0x4F0),

    MX51_PIN_NANDF_WP_B = _MXC_BUILD_GPIO_PIN_MX51(2, 7, 3, 0x118, 0x4F4),

    MX51_PIN_NANDF_RB0 = _MXC_BUILD_GPIO_PIN_MX51(2, 8, 3, 0x11C, 0x4F8),

    MX51_PIN_NANDF_RB1 = _MXC_BUILD_GPIO_PIN_MX51(2, 9, 3, 0x120, 0x4FC),

    MX51_PIN_NANDF_RB2 = _MXC_BUILD_GPIO_PIN_MX51(2, 10, 3, 0x124, 0x500),

    MX51_PIN_NANDF_RB3 = _MXC_BUILD_GPIO_PIN_MX51(2, 11, 3, 0x128, 0x504),

//     MX51_PIN_GPIO_NAND = _MXC_BUILD_GPIO_PIN_MX51(2, 12, 3, 0x12C, 0x514),

    MX51_PIN_GPIO_NAND = _MXC_BUILD_GPIO_PIN_MX51(3, 12, 3, 0x12C, 0x514),//power INT

    MX51_PIN_NANDF_RB4 = MX51_PIN_GPIO_NAND,

    MX51_PIN_NANDF_RB5 = _MXC_BUILD_GPIO_PIN_MX51(2, 13, 3, 0x130, 0x5D8),

    MX51_PIN_NANDF_RB6 = _MXC_BUILD_GPIO_PIN_MX51(2, 14, 3, 0x134, 0x5DC),

    MX51_PIN_NANDF_RB7 = _MXC_BUILD_GPIO_PIN_MX51(2, 15, 3, 0x138, 0x5E0),

    MX51_PIN_NANDF_CS0 = _MXC_BUILD_GPIO_PIN_MX51(2, 16, 3, 0x130, 0x518),

    MX51_PIN_NANDF_CS1 = _MXC_BUILD_GPIO_PIN_MX51(2, 17, 3, 0x134, 0x51C),

    MX51_PIN_NANDF_CS2 = _MXC_BUILD_GPIO_PIN_MX51(2, 18, 3, 0x138, 0x520),

    MX51_PIN_NANDF_CS3 = _MXC_BUILD_GPIO_PIN_MX51(2, 19, 3, 0x13C, 0x524),

    MX51_PIN_NANDF_CS4 = _MXC_BUILD_GPIO_PIN_MX51(2, 20, 3, 0x140, 0x528),

    MX51_PIN_NANDF_CS5 = _MXC_BUILD_GPIO_PIN_MX51(2, 21, 3, 0x144, 0x52C),

    MX51_PIN_NANDF_CS6 = _MXC_BUILD_GPIO_PIN_MX51(2, 22, 3, 0x148, 0x530),

    MX51_PIN_NANDF_CS7 = _MXC_BUILD_GPIO_PIN_MX51(2, 23, 3, 0x14C, 0x534),

    MX51_PIN_NANDF_RDY_INT = _MXC_BUILD_GPIO_PIN_MX51(2, 24, 3, 0x150, 0x538),

    MX51_PIN_NANDF_D15 = _MXC_BUILD_GPIO_PIN_MX51(2, 25, 3, 0x154, 0x53C),

    MX51_PIN_NANDF_D14 = _MXC_BUILD_GPIO_PIN_MX51(2, 26, 3, 0x158, 0x540),

    MX51_PIN_NANDF_D13 = _MXC_BUILD_GPIO_PIN_MX51(2, 27, 3, 0x15C, 0x544),

    MX51_PIN_NANDF_D12 = _MXC_BUILD_GPIO_PIN_MX51(2, 28, 3, 0x160, 0x548),

    MX51_PIN_NANDF_D11 = _MXC_BUILD_GPIO_PIN_MX51(2, 29, 3, 0x164, 0x54C),

    MX51_PIN_NANDF_D10 = _MXC_BUILD_GPIO_PIN_MX51(2, 30, 3, 0x168, 0x550),

    MX51_PIN_NANDF_D9 = _MXC_BUILD_GPIO_PIN_MX51(2, 31, 3, 0x16C, 0x554),

    MX51_PIN_NANDF_D8 = _MXC_BUILD_GPIO_PIN_MX51(3, 0, 3, 0x170, 0x558),

    MX51_PIN_NANDF_D7 = _MXC_BUILD_GPIO_PIN_MX51(3, 1, 3, 0x174, 0x55C),

    MX51_PIN_NANDF_D6 = _MXC_BUILD_GPIO_PIN_MX51(3, 2, 3, 0x178, 0x560),

    MX51_PIN_NANDF_D5 = _MXC_BUILD_GPIO_PIN_MX51(3, 3, 3, 0x17C, 0x564),

    MX51_PIN_NANDF_D4 = _MXC_BUILD_GPIO_PIN_MX51(3, 4, 3, 0x180, 0x568),

    MX51_PIN_NANDF_D3 = _MXC_BUILD_GPIO_PIN_MX51(3, 5, 3, 0x184, 0x56C),

    MX51_PIN_NANDF_D2 = _MXC_BUILD_GPIO_PIN_MX51(3, 6, 3, 0x188, 0x570),

    MX51_PIN_NANDF_D1 = _MXC_BUILD_GPIO_PIN_MX51(3, 7, 3, 0x18C, 0x574),

    MX51_PIN_NANDF_D0 = _MXC_BUILD_GPIO_PIN_MX51(3, 8, 3, 0x190, 0x578),

     MX51_PIN_CSI1_D8 = _MXC_BUILD_GPIO_PIN_MX51(0, 12, 4, 0x194, 0x57C),//power INT

    MX51_PIN_CSI1_D9 = _MXC_BUILD_GPIO_PIN_MX51(2, 13, 3, 0x198, 0x580),

    MX51_PIN_CSI1_D10 = _MXC_BUILD_NON_GPIO_PIN_MX51(0x19C, 0x584),

    MX51_PIN_CSI1_D11 = _MXC_BUILD_NON_GPIO_PIN_MX51(0x1A0, 0x588),

    MX51_PIN_CSI1_D12 = _MXC_BUILD_NON_GPIO_PIN_MX51(0x1A4, 0x58C),

    MX51_PIN_CSI1_D13 = _MXC_BUILD_NON_GPIO_PIN_MX51(0x1A8, 0x590),

    MX51_PIN_CSI1_D14 = _MXC_BUILD_NON_GPIO_PIN_MX51(0x1AC, 0x594),

    MX51_PIN_CSI1_D15 = _MXC_BUILD_NON_GPIO_PIN_MX51(0x1B0, 0x598),

    MX51_PIN_CSI1_D16 = _MXC_BUILD_NON_GPIO_PIN_MX51(0x1B4, 0x59C),

    MX51_PIN_CSI1_D17 = _MXC_BUILD_NON_GPIO_PIN_MX51(0x1B8, 0x5A0),

    MX51_PIN_CSI1_D18 = _MXC_BUILD_NON_GPIO_PIN_MX51(0x1BC, 0x5A4),

    MX51_PIN_CSI1_D19 = _MXC_BUILD_NON_GPIO_PIN_MX51(0x1C0, 0x5A8),

    MX51_PIN_CSI1_VSYNC = _MXC_BUILD_GPIO_PIN_MX51(2, 14, 3, 0x1C4, 0x5AC),

    MX51_PIN_CSI1_HSYNC = _MXC_BUILD_GPIO_PIN_MX51(2, 15, 3, 0x1C8, 0x5B0),

    MX51_PIN_CSI1_PIXCLK = _MXC_BUILD_NON_GPIO_PIN_MX51(NON_MUX_I, 0x5B4),

    MX51_PIN_CSI1_MCLK = _MXC_BUILD_NON_GPIO_PIN_MX51(NON_MUX_I, 0x5B8),

    MX51_PIN_CSI1_PKE0 = _MXC_BUILD_NON_GPIO_PIN_MX51(NON_MUX_I, 0x860),

    MX51_PIN_CSI2_D12 = _MXC_BUILD_GPIO_PIN_MX51(3, 9, 3, 0x1CC, 0x5BC),

    MX51_PIN_CSI2_D13 = _MXC_BUILD_GPIO_PIN_MX51(3, 10, 3, 0x1D0, 0x5C0),

    MX51_PIN_CSI2_D14 = _MXC_BUILD_GPIO_PIN_MX51(3, 11, 3, 0x1D4, 0x5C4),

    MX51_PIN_CSI2_D15 = _MXC_BUILD_GPIO_PIN_MX51(3, 12, 3, 0x1D8, 0x5C8),

    MX51_PIN_CSI2_D16 = _MXC_BUILD_GPIO_PIN_MX51(3, 11, 3, 0x1DC, 0x5CC),

    MX51_PIN_CSI2_D17 = _MXC_BUILD_GPIO_PIN_MX51(3, 12, 3, 0x1E0, 0x5D0),

    MX51_PIN_CSI2_D18 = _MXC_BUILD_GPIO_PIN_MX51(3, 11, 3, 0x1E4, 0x5D4),

    MX51_PIN_CSI2_D19 = _MXC_BUILD_GPIO_PIN_MX51(3, 12, 3, 0x1E8, 0x5D8),

    MX51_PIN_CSI2_VSYNC = _MXC_BUILD_GPIO_PIN_MX51(3, 13, 3, 0x1EC, 0x5DC),

    MX51_PIN_CSI2_HSYNC = _MXC_BUILD_GPIO_PIN_MX51(3, 14, 3, 0x1F0, 0x5E0),

    MX51_PIN_CSI2_PIXCLK = _MXC_BUILD_GPIO_PIN_MX51(3, 15, 3, 0x1F4, 0x5E4),

//     MX51_PIN_CSI2_PKE0 = _MXC_BUILD_NON_GPIO_PIN_MX51(NON_MUX_I, 0x81C),

    MX51_PIN_CSI2_PKE0 = _MXC_BUILD_NON_GPIO_PIN_MX51(NON_MUX_I, 0x820),

    MX51_PIN_I2C1_CLK = _MXC_BUILD_GPIO_PIN_MX51(3, 16, 3, 0x1F8, 0x5E8),

    MX51_PIN_I2C1_DAT = _MXC_BUILD_GPIO_PIN_MX51(3, 17, 3, 0x1FC, 0x5EC),

    MX51_PIN_AUD3_BB_TXD = _MXC_BUILD_GPIO_PIN_MX51(3, 18, 3, 0x200, 0x5F0),

    MX51_PIN_AUD3_BB_RXD = _MXC_BUILD_GPIO_PIN_MX51(3, 19, 3, 0x204, 0x5F4),

    MX51_PIN_AUD3_BB_CK = _MXC_BUILD_GPIO_PIN_MX51(3, 20, 3, 0x208, 0x5F8),

    MX51_PIN_AUD3_BB_FS = _MXC_BUILD_GPIO_PIN_MX51(3, 21, 3, 0x20C, 0x5FC),

    MX51_PIN_CSPI1_MOSI = _MXC_BUILD_GPIO_PIN_MX51(3, 22, 3, 0x210, 0x600),

    MX51_PIN_CSPI1_MISO = _MXC_BUILD_GPIO_PIN_MX51(3, 23, 3, 0x214, 0x604),

    MX51_PIN_CSPI1_SS0 = _MXC_BUILD_GPIO_PIN_MX51(3, 24, 3, 0x218, 0x608),

    MX51_PIN_CSPI1_SS1 = _MXC_BUILD_GPIO_PIN_MX51(3, 25, 3, 0x21C, 0x60C),

    MX51_PIN_CSPI1_RDY = _MXC_BUILD_GPIO_PIN_MX51(3, 26, 3, 0x220, 0x610),

    MX51_PIN_CSPI1_SCLK = _MXC_BUILD_GPIO_PIN_MX51(3, 27, 3, 0x224, 0x614),

      MX51_PIN_UART1_RXD = _MXC_BUILD_GPIO_PIN_MX51(3, 28, 4, 0x228, 0x618),//Touch

//      MX51_PIN_UART1_RXD = _MXC_BUILD_GPIO_PIN_MX51(3, 30, 3, 0x230, 0x620),

    MX51_PIN_UART1_TXD = _MXC_BUILD_GPIO_PIN_MX51(3, 29, 3, 0x22C, 0x61C),

    MX51_PIN_UART1_RTS = _MXC_BUILD_GPIO_PIN_MX51(3, 30, 3, 0x230, 0x620),

//    MX51_PIN_UART1_RTS = _MXC_BUILD_GPIO_PIN_MX51(3, 28, 4, 0x228, 0x618),

    MX51_PIN_UART1_CTS = _MXC_BUILD_GPIO_PIN_MX51(3, 31, 3, 0x234, 0x624),

    MX51_PIN_UART2_RXD = _MXC_BUILD_GPIO_PIN_MX51(0, 20, 3, 0x238, 0x628),

    MX51_PIN_UART2_TXD = _MXC_BUILD_GPIO_PIN_MX51(0, 21, 3, 0x23C, 0x62C),

    MX51_PIN_UART3_RXD = _MXC_BUILD_GPIO_PIN_MX51(0, 22, 3, 0x240, 0x630),

    MX51_PIN_UART3_TXD = _MXC_BUILD_GPIO_PIN_MX51(0, 23, 3, 0x244, 0x634),

    MX51_PIN_OWIRE_LINE = _MXC_BUILD_GPIO_PIN_MX51(0, 24, 3, 0x248, 0x638),

    MX51_PIN_KEY_ROW0 = _MXC_BUILD_NON_GPIO_PIN_MX51(0x24C, 0x63C),

    MX51_PIN_KEY_ROW1 = _MXC_BUILD_NON_GPIO_PIN_MX51(0x250, 0x640),

    MX51_PIN_KEY_ROW2 = _MXC_BUILD_NON_GPIO_PIN_MX51(0x254, 0x644),

    MX51_PIN_KEY_ROW3 = _MXC_BUILD_NON_GPIO_PIN_MX51(0x258, 0x648),

    MX51_PIN_KEY_COL0 = _MXC_BUILD_NON_GPIO_PIN_MX51(0x25C, 0x64C),

    MX51_PIN_KEY_COL1 = _MXC_BUILD_NON_GPIO_PIN_MX51(0x260, 0x650),

    MX51_PIN_KEY_COL2 = _MXC_BUILD_NON_GPIO_PIN_MX51(0x264, 0x654),

    MX51_PIN_KEY_COL3 = _MXC_BUILD_NON_GPIO_PIN_MX51(0x268, 0x658),

    MX51_PIN_KEY_COL4 = _MXC_BUILD_NON_GPIO_PIN_MX51(0x26C, 0x65C),

    MX51_PIN_KEY_COL5 = _MXC_BUILD_NON_GPIO_PIN_MX51(0x270, 0x660),

    MX51_PIN_USBH1_CLK = _MXC_BUILD_GPIO_PIN_MX51(0, 25, 2, 0x278, 0x678),

    MX51_PIN_USBH1_DIR = _MXC_BUILD_GPIO_PIN_MX51(0, 26, 2, 0x27C, 0x67C),

    MX51_PIN_USBH1_STP = _MXC_BUILD_GPIO_PIN_MX51(0, 27, 2, 0x280, 0x680),

    MX51_PIN_USBH1_NXT = _MXC_BUILD_GPIO_PIN_MX51(0, 28, 2, 0x284, 0x684),

    MX51_PIN_USBH1_DATA0 = _MXC_BUILD_GPIO_PIN_MX51(0, 11, 2, 0x288, 0x688),

    MX51_PIN_USBH1_DATA1 = _MXC_BUILD_GPIO_PIN_MX51(0, 12, 2, 0x28C, 0x68C),

    MX51_PIN_USBH1_DATA2 = _MXC_BUILD_GPIO_PIN_MX51(0, 13, 2, 0x290, 0x690),

    MX51_PIN_USBH1_DATA3 = _MXC_BUILD_GPIO_PIN_MX51(0, 14, 2, 0x294, 0x694),

    MX51_PIN_USBH1_DATA4 = _MXC_BUILD_GPIO_PIN_MX51(0, 15, 2, 0x298, 0x698),

    MX51_PIN_USBH1_DATA5 = _MXC_BUILD_GPIO_PIN_MX51(0, 16, 2, 0x29C, 0x69C),

    MX51_PIN_USBH1_DATA6 = _MXC_BUILD_GPIO_PIN_MX51(0, 17, 2, 0x2A0, 0x6A0),

    MX51_PIN_USBH1_DATA7 = _MXC_BUILD_GPIO_PIN_MX51(0, 18, 2, 0x2A4, 0x6A4),

    MX51_PIN_DI1_PIN11 = _MXC_BUILD_GPIO_PIN_MX51(2, 0, 4, 0x2A8, 0x6A8),

      MX51_PIN_DI1_PIN12 = _MXC_BUILD_GPIO_PIN_MX51(4, 1, 4, 0x2AC, 0x6AC),//ILL LED1

      MX51_PIN_DI1_PIN13 = _MXC_BUILD_GPIO_PIN_MX51(4, 2, 4, 0x2B0, 0x6B0),//ILL LED2

    MX51_PIN_DI1_D0_CS = _MXC_BUILD_GPIO_PIN_MX51(2, 3, 4, 0x2B4, 0x6B4),

    MX51_PIN_DI1_D1_CS = _MXC_BUILD_GPIO_PIN_MX51(2, 4, 4, 0x2B8, 0x6B8),

    MX51_PIN_DISPB2_SER_DIN = _MXC_BUILD_GPIO_PIN_MX51(2, 5, 4, 0x2BC, 0x6BC),//Probe

    MX51_PIN_DISPB2_SER_DIO = _MXC_BUILD_GPIO_PIN_MX51(2, 6, 4, 0x2C0, 0x6C0),

    MX51_PIN_DISPB2_SER_CLK = _MXC_BUILD_GPIO_PIN_MX51(2, 7, 4, 0x2C4, 0x6C4),

    MX51_PIN_DISPB2_SER_RS = _MXC_BUILD_GPIO_PIN_MX51(2, 8, 4, 0x2C8, 0x6C8),

    MX51_PIN_DISP1_DAT0 = _MXC_BUILD_NON_GPIO_PIN_MX51(0x2CC, 0x6CC),

    MX51_PIN_DISP1_DAT1 = _MXC_BUILD_NON_GPIO_PIN_MX51(0x2D0, 0x6D0),

    MX51_PIN_DISP1_DAT2 = _MXC_BUILD_NON_GPIO_PIN_MX51(0x2D4, 0x6D4),

    MX51_PIN_DISP1_DAT3 = _MXC_BUILD_NON_GPIO_PIN_MX51(0x2D8, 0x6D8),

    MX51_PIN_DISP1_DAT4 = _MXC_BUILD_NON_GPIO_PIN_MX51(0x2DC, 0x6DC),

    MX51_PIN_DISP1_DAT5 = _MXC_BUILD_NON_GPIO_PIN_MX51(0x2E0, 0x6E0),

    MX51_PIN_DISP1_DAT6 = _MXC_BUILD_NON_GPIO_PIN_MX51(0x2E4, 0x6E4),

    MX51_PIN_DISP1_DAT7 = _MXC_BUILD_NON_GPIO_PIN_MX51(0x2E8, 0x6E8),

    MX51_PIN_DISP1_DAT8 = _MXC_BUILD_NON_GPIO_PIN_MX51(0x2EC, 0x6EC),

    MX51_PIN_DISP1_DAT9 = _MXC_BUILD_NON_GPIO_PIN_MX51(0x2F0, 0x6F0),

    MX51_PIN_DISP1_DAT10 = _MXC_BUILD_NON_GPIO_PIN_MX51(0x2F4, 0x6F4),

    MX51_PIN_DISP1_DAT11 = _MXC_BUILD_NON_GPIO_PIN_MX51(0x2F8, 0x6F8),

    MX51_PIN_DISP1_DAT12 = _MXC_BUILD_NON_GPIO_PIN_MX51(0x2FC, 0x6FC),

    MX51_PIN_DISP1_DAT13 = _MXC_BUILD_NON_GPIO_PIN_MX51(0x300, 0x700),

    MX51_PIN_DISP1_DAT14 = _MXC_BUILD_NON_GPIO_PIN_MX51(0x304, 0x704),

    MX51_PIN_DISP1_DAT15 = _MXC_BUILD_NON_GPIO_PIN_MX51(0x308, 0x708),

    MX51_PIN_DISP1_DAT16 = _MXC_BUILD_NON_GPIO_PIN_MX51(0x30C, 0x70C),

    MX51_PIN_DISP1_DAT17 = _MXC_BUILD_NON_GPIO_PIN_MX51(0x310, 0x710),

    MX51_PIN_DISP1_DAT18 = _MXC_BUILD_NON_GPIO_PIN_MX51(0x314, 0x714),

    MX51_PIN_DISP1_DAT19 = _MXC_BUILD_NON_GPIO_PIN_MX51(0x318, 0x718),

    MX51_PIN_DISP1_DAT20 = _MXC_BUILD_NON_GPIO_PIN_MX51(0x31C, 0x71C),

    MX51_PIN_DISP1_DAT21 = _MXC_BUILD_NON_GPIO_PIN_MX51(0x320, 0x720),

    MX51_PIN_DISP1_DAT22 = _MXC_BUILD_NON_GPIO_PIN_MX51(0x324, 0x724),

    MX51_PIN_DISP1_DAT23 = _MXC_BUILD_NON_GPIO_PIN_MX51(0x328, 0x728),

    MX51_PIN_DI1_PIN3 = _MXC_BUILD_NON_GPIO_PIN_MX51(0x32C, 0x72C),

    MX51_PIN_DI1_PIN2 = _MXC_BUILD_NON_GPIO_PIN_MX51(0x330, 0x734),

    MX51_PIN_DI_GP1 = _MXC_BUILD_NON_GPIO_PIN_MX51(0x334, 0x73C),

    MX51_PIN_DI_GP2 = _MXC_BUILD_NON_GPIO_PIN_MX51(0x338, 0x740),

    MX51_PIN_DI_GP3 = _MXC_BUILD_NON_GPIO_PIN_MX51(0x33C, 0x744),

    MX51_PIN_DI2_PIN4 = _MXC_BUILD_NON_GPIO_PIN_MX51(0x340, 0x748),

    MX51_PIN_DI2_PIN2 = _MXC_BUILD_NON_GPIO_PIN_MX51(0x344, 0x74C),

    MX51_PIN_DI2_PIN3 = _MXC_BUILD_NON_GPIO_PIN_MX51(0x348, 0x750),

    MX51_PIN_DI2_DISP_CLK = _MXC_BUILD_NON_GPIO_PIN_MX51(0x34C, 0x754),

    MX51_PIN_DI_GP4 = _MXC_BUILD_NON_GPIO_PIN_MX51(0x350, 0x758),

    MX51_PIN_DISP2_DAT0 = _MXC_BUILD_NON_GPIO_PIN_MX51(0x354, 0x75C),

    MX51_PIN_DISP2_DAT1 = _MXC_BUILD_NON_GPIO_PIN_MX51(0x358, 0x760),

    MX51_PIN_DISP2_DAT2 = _MXC_BUILD_NON_GPIO_PIN_MX51(0x35C, 0x764),

    MX51_PIN_DISP2_DAT3 = _MXC_BUILD_NON_GPIO_PIN_MX51(0x360, 0x768),

    MX51_PIN_DISP2_DAT4 = _MXC_BUILD_NON_GPIO_PIN_MX51(0x364, 0x76C),

    MX51_PIN_DISP2_DAT5 = _MXC_BUILD_NON_GPIO_PIN_MX51(0x368, 0x770),

    MX51_PIN_DISP2_DAT6 = _MXC_BUILD_GPIO_PIN_MX51(0, 19, 5, 0x36C, 0x774),

    MX51_PIN_DISP2_DAT7 = _MXC_BUILD_GPIO_PIN_MX51(0, 29, 5, 0x370, 0x778),

    MX51_PIN_DISP2_DAT8 = _MXC_BUILD_GPIO_PIN_MX51(0, 30, 5, 0x374, 0x77C),

    MX51_PIN_DISP2_DAT9 = _MXC_BUILD_GPIO_PIN_MX51(0, 31, 5, 0x378, 0x780),

    MX51_PIN_DISP2_DAT10 = _MXC_BUILD_NON_GPIO_PIN_MX51(0x37C, 0x784),

    MX51_PIN_DISP2_DAT11 = _MXC_BUILD_NON_GPIO_PIN_MX51(0x380, 0x788),

    MX51_PIN_DISP2_DAT12 = _MXC_BUILD_NON_GPIO_PIN_MX51(0x384, 0x78C),

    MX51_PIN_DISP2_DAT13 = _MXC_BUILD_NON_GPIO_PIN_MX51(0x388, 0x790),

    MX51_PIN_DISP2_DAT14 = _MXC_BUILD_NON_GPIO_PIN_MX51(0x38C, 0x794),

    MX51_PIN_DISP2_DAT15 = _MXC_BUILD_NON_GPIO_PIN_MX51(0x390, 0x798),

    MX51_PIN_SD1_CMD = _MXC_BUILD_NON_GPIO_PIN_MX51(0x394, 0x79C),

    MX51_PIN_SD1_CLK = _MXC_BUILD_NON_GPIO_PIN_MX51(0x398, 0x7A0),

    MX51_PIN_SD1_DATA0 = _MXC_BUILD_NON_GPIO_PIN_MX51(0x39C, 0x7A4),

    MX51_PIN_SD1_DATA1 = _MXC_BUILD_NON_GPIO_PIN_MX51(0x3A0, 0x7A8),

    MX51_PIN_SD1_DATA2 = _MXC_BUILD_NON_GPIO_PIN_MX51(0x3A4, 0x7AC),

    MX51_PIN_SD1_DATA3 = _MXC_BUILD_NON_GPIO_PIN_MX51(0x3A8, 0x7B0),

    MX51_PIN_GPIO1_0 = _MXC_BUILD_GPIO_PIN_MX51(0, 0, 1, 0x3AC, 0x7B4),

    MX51_PIN_GPIO1_1 = _MXC_BUILD_GPIO_PIN_MX51(0, 1, 1, 0x3B0, 0x7B8),

    MX51_PIN_SD2_CMD = _MXC_BUILD_NON_GPIO_PIN_MX51(0x3B4, 0x7BC),

    MX51_PIN_SD2_CLK = _MXC_BUILD_NON_GPIO_PIN_MX51(0x3B8, 0x7C0),

    MX51_PIN_SD2_DATA0 = _MXC_BUILD_NON_GPIO_PIN_MX51(0x3BC, 0x7C4),

    MX51_PIN_SD2_DATA1 = _MXC_BUILD_NON_GPIO_PIN_MX51(0x3C0, 0x7C8),

    MX51_PIN_SD2_DATA2 = _MXC_BUILD_NON_GPIO_PIN_MX51(0x3C4, 0x7CC),

    MX51_PIN_SD2_DATA3 = _MXC_BUILD_NON_GPIO_PIN_MX51(0x3C8, 0x7D0),

    MX51_PIN_GPIO1_2 = _MXC_BUILD_GPIO_PIN_MX51(0, 2, 0, 0x3CC, 0x7D4),

    MX51_PIN_GPIO1_3 = _MXC_BUILD_GPIO_PIN_MX51(0, 3, 0, 0x3D0, 0x7D8),

    MX51_PIN_PMIC_INT_REQ = _MXC_BUILD_NON_GPIO_PIN_MX51(0x3D4, 0x7FC),

    MX51_PIN_GPIO1_4 = _MXC_BUILD_GPIO_PIN_MX51(0, 4, 0, 0x3D8, 0x804),

    MX51_PIN_GPIO1_5 = _MXC_BUILD_GPIO_PIN_MX51(0, 5, 0, 0x3DC, 0x808),

    MX51_PIN_GPIO1_6 = _MXC_BUILD_GPIO_PIN_MX51(0, 6, 0, 0x3E0, 0x80C),

    MX51_PIN_GPIO1_7 = _MXC_BUILD_GPIO_PIN_MX51(0, 7, 0, 0x3E4, 0x810),

    MX51_PIN_GPIO1_8 = _MXC_BUILD_GPIO_PIN_MX51(0, 8, 0, 0x3E8, 0x814),

    MX51_PIN_GPIO1_9 = _MXC_BUILD_GPIO_PIN_MX51(0, 9, 0, 0x3EC, 0x818),

   

    //qmax gpio pin assignments  added on Mar 16 2013 added by Elangovan&Ravivarman

//      MX51_PIN_UART1_TXD_TEST = _MXC_BUILD_GPIO_PIN_MX51(3, 29, 4, 0x3F0, 0x81C),

//     MX51_PIN_CSPI1_SS1_TEST = _MXC_BUILD_GPIO_PIN_MX51(3, 25, 4, 0x3F4, 0x820),

//      MX51_PIN_UART1_RXD = _MXC_BUILD_GPIO_PIN_MX51(3, 28, 4, 0x3F0, 0x81C),

   

};

/*!

* various IOMUX input select register index

*/

enum iomux_input_select_mx51 {

    MUX_IN_AUDMUX_P4_INPUT_DA_AMX_SELECT_I = 0,

    MUX_IN_AUDMUX_P4_INPUT_DB_AMX_SELECT_I,

    MUX_IN_AUDMUX_P4_INPUT_TXCLK_AMX_SELECT_INPUT,

    MUX_IN_AUDMUX_P4_INPUT_TXFS_AMX_SELECT_INPUT,

    MUX_IN_AUDMUX_P5_INPUT_DA_AMX_SELECT_INPUT,

    MUX_IN_AUDMUX_P5_INPUT_DB_AMX_SELECT_INPUT,

    MUX_IN_AUDMUX_P5_INPUT_RXCLK_AMX_SELECT_INPUT,

    MUX_IN_AUDMUX_P5_INPUT_RXFS_AMX_SELECT,

    MUX_IN_AUDMUX_P5_INPUT_TXCLK_AMX_SELECT_INPUT,

    MUX_IN_AUDMUX_P5_INPUT_TXFS_AMX_SELECT_INPUT,

    MUX_IN_AUDMUX_P6_INPUT_DA_AMX_SELECT_INPUT,

    MUX_IN_AUDMUX_P6_INPUT_DB_AMX_SELECT_INPUT,

    MUX_IN_AUDMUX_P6_INPUT_RXCLK_AMX_SELECT_INPUT,

    MUX_IN_AUDMUX_P6_INPUT_RXFS_AMX_SELECT_INPUT,

    MUX_IN_AUDMUX_P6_INPUT_TXCLK_AMX_SELECT_INPUT,

    MUX_IN_AUDMUX_P6_INPUT_TXFS_AMX_SELECT_INPUT,

    MUX_IN_CCM_IPP_DI_CLK_SELECT_INPUT,

    /* TO2 */

    MUX_IN_CCM_IPP_DI1_CLK_SELECT_INPUT,

    MUX_IN_CCM_PLL1_BYPASS_CLK_SELECT_INPUT,

    MUX_IN_CCM_PLL2_BYPASS_CLK_SELECT_INPUT,

    MUX_IN_CSPI_IPP_CSPI_CLK_IN_SELECT_INPUT,

    MUX_IN_CSPI_IPP_IND_MISO_SELECT_INPUT,

    MUX_IN_CSPI_IPP_IND_MOSI_SELECT_INPUT,

    MUX_IN_CSPI_IPP_IND_SS_B_1_SELECT_INPUT,

    MUX_IN_CSPI_IPP_IND_SS_B_2_SELECT_INPUT,

    MUX_IN_CSPI_IPP_IND_SS_B_3_SELECT_INPUT,

    MUX_IN_DPLLIP1_L1T_TOG_EN_SELECT_INPUT,

    /* TO2 */

    MUX_IN_ECSPI2_IPP_IND_SS_B_1_SELECT_INPUT,

    MUX_IN_ECSPI2_IPP_IND_SS_B_3_SELECT_INPUT,

    MUX_IN_EMI_IPP_IND_RDY_INT_SELECT_INPUT,

    MUX_IN_ESDHC3_IPP_DAT0_IN_SELECT_INPUT,

    MUX_IN_ESDHC3_IPP_DAT1_IN_SELECT_INPUT,

    MUX_IN_ESDHC3_IPP_DAT2_IN_SELECT_INPUT,

    MUX_IN_ESDHC3_IPP_DAT3_IN_SELECT_INPUT,

    MUX_IN_FEC_FEC_COL_SELECT_INPUT,

    MUX_IN_FEC_FEC_CRS_SELECT_INPUT,

    MUX_IN_FEC_FEC_MDI_SELECT_INPUT,

    MUX_IN_FEC_FEC_RDATA_0_SELECT_INPUT,

    MUX_IN_FEC_FEC_RDATA_1_SELECT_INPUT,

    MUX_IN_FEC_FEC_RDATA_2_SELECT_INPUT,

    MUX_IN_FEC_FEC_RDATA_3_SELECT_INPUT,

    MUX_IN_FEC_FEC_RX_CLK_SELECT_INPUT,

    MUX_IN_FEC_FEC_RX_DV_SELECT_INPUT,

    MUX_IN_FEC_FEC_RX_ER_SELECT_INPUT,

    MUX_IN_FEC_FEC_TX_CLK_SELECT_INPUT,

    MUX_IN_GPIO3_IPP_IND_G_IN_1_SELECT_INPUT,

    MUX_IN_GPIO3_IPP_IND_G_IN_2_SELECT_INPUT,

    MUX_IN_GPIO3_IPP_IND_G_IN_3_SELECT_INPUT,

    MUX_IN_GPIO3_IPP_IND_G_IN_4_SELECT_INPUT,

    MUX_IN_GPIO3_IPP_IND_G_IN_5_SELECT_INPUT,

    MUX_IN_GPIO3_IPP_IND_G_IN_6_SELECT_INPUT,

    MUX_IN_GPIO3_IPP_IND_G_IN_7_SELECT_INPUT,

    MUX_IN_GPIO3_IPP_IND_G_IN_8_SELECT_INPUT,

    /* TO2 */

    MUX_IN_GPIO3_IPP_IND_G_IN_12_SELECT_INPUT,

    MUX_IN_HSC_MIPI_MIX_IPP_IND_SENS1_DATA_EN_SELECT_INPUT,

    MUX_IN_HSC_MIPI_MIX_IPP_IND_SENS2_DATA_EN_SELECT_INPUT,

    /* TO2 */

    MUX_IN_HSC_MIPI_MIX_PAR_VSYNC_SELECT_INPUT,

    /* TO2 */

    MUX_IN_HSC_MIPI_MIX_PAR_DI_WAIT_SELECT_INPUT,

    MUX_IN_HSC_MIPI_MIX_PAR_SISG_TRIG_SELECT_INPUT,

    MUX_IN_I2C1_IPP_SCL_IN_SELECT_INPUT,

    MUX_IN_I2C1_IPP_SDA_IN_SELECT_INPUT,

    MUX_IN_I2C2_IPP_SCL_IN_SELECT_INPUT,

    MUX_IN_I2C2_IPP_SDA_IN_SELECT_INPUT,

    MUX_IN_IPU_IPP_DI_0_IND_DISPB_SD_D_SELECT_INPUT,

    MUX_IN_IPU_IPP_DI_1_IND_DISPB_SD_D_SELECT_INPUT,

    MUX_IN_KPP_IPP_IND_COL_6_SELECT_INPUT,

    MUX_IN_KPP_IPP_IND_COL_7_SELECT_INPUT,

    MUX_IN_KPP_IPP_IND_ROW_4_SELECT_INPUT,

    MUX_IN_KPP_IPP_IND_ROW_5_SELECT_INPUT,

    MUX_IN_KPP_IPP_IND_ROW_6_SELECT_INPUT,

    MUX_IN_KPP_IPP_IND_ROW_7_SELECT_INPUT,

    MUX_IN_UART1_IPP_UART_RTS_B_SELECT_INPUT,

    MUX_IN_UART1_IPP_UART_RXD_MUX_SELECT_INPUT,

    MUX_IN_UART2_IPP_UART_RTS_B_SELECT_INPUT,

    MUX_IN_UART2_IPP_UART_RXD_MUX_SELECT_INPUT,

    MUX_IN_UART3_IPP_UART_RTS_B_SELECT_INPUT,

    MUX_IN_UART3_IPP_UART_RXD_MUX_SELECT_INPUT,

    MUX_IN_USBOH3_IPP_IND_UH3_CLK_SELECT_INPUT,

    MUX_IN_USBOH3_IPP_IND_UH3_DATA_0_SELECT_INPUT,

    MUX_IN_USBOH3_IPP_IND_UH3_DATA_1_SELECT_INPUT,

    MUX_IN_USBOH3_IPP_IND_UH3_DATA_2_SELECT_INPUT,

    MUX_IN_USBOH3_IPP_IND_UH3_DATA_3_SELECT_INPUT,

    MUX_IN_USBOH3_IPP_IND_UH3_DATA_4_SELECT_INPUT,

    MUX_IN_USBOH3_IPP_IND_UH3_DATA_5_SELECT_INPUT,

    MUX_IN_USBOH3_IPP_IND_UH3_DATA_6_SELECT_INPUT,

    MUX_IN_USBOH3_IPP_IND_UH3_DATA_7_SELECT_INPUT,

    MUX_IN_USBOH3_IPP_IND_UH3_DIR_SELECT_INPUT,

    MUX_IN_USBOH3_IPP_IND_UH3_NXT_SELECT_INPUT,

    MUX_IN_USBOH3_IPP_IND_UH3_STP_SELECT_INPUT,

    MUX_INPUT_NUM_MUX,

};

#endif                /* __ASSEMBLY__ */

#endif                /* __ASM_ARCH_MXC_MX51_PINS_H__ */

0 Kudos
Reply
1,541 Views
Yuri
NXP Employee
NXP Employee

Hello,

from the table 52 of the Datasheet :

A[15:0] - EIM_DA[15:0]

A[27:16] -  NANDF_D[11:0]

D[7:0] - EIM_DA[7:0]

D[15:8] - EIM_DA[15:8]

D[23:16] - NANDF_D[7:0]

D[31:24] - NANDF_D[15:8]

Regards,

Yuri.

1,540 Views
arunkmrvn
Contributor II

Hi Yuri,

I followed what you told and as per table 52. I am trying to get 8 bit non-muxed data. using below configuration.

   __raw_writel(0x00463081, (u32)weim_vbaddr + WEIM_CS5_OFFSET + CSGCR1);

   __raw_writel(0x00000000, (u32)weim_vbaddr + WEIM_CS5_OFFSET + CSGCR2);

        __raw_writel(0x32260000, (u32)weim_vbaddr + WEIM_CS5_OFFSET + CSRCR1);

    __raw_writel(0, (u32)weim_vbaddr + WEIM_CS5_OFFSET + CSRCR2);

MUM =0, AUS=0, DSZ=110.

Add - > EIMDA[0-27]

Data -> EIMD[23-16]

But still i am getting 16 bit data.

I Stored 0x12345678 in FPGA.

I tried to access 8 bit. but still i am getting 0x1234 as a result.[dsz=110]

I tried to access 16 bit. but still i am getting 0x1234 as a result. [dsz=010, mum=0]

I tried to access 16 bit. but still i am getting 0x1234 as a result. [dsz=001, mum=1]

i thought, code is not compiled properly, so given debug message & printed raw data of configuration [GCR,RCR] also. Its changing fine, but still i am unable to find out error. what's happening ?

what's the possibility way to clear this error ?

please give your mail id. i'll send the source files.

0 Kudos
Reply