HAB CST 2.2 Missing CSF1_1_sha256_4096_65537_v3_usr_crt.pem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

HAB CST 2.2 Missing CSF1_1_sha256_4096_65537_v3_usr_crt.pem

ソリューションへジャンプ
707件の閲覧回数
michaelrobbelot
Contributor IV

I am working on implementing HAB for Widevine on JB4.3 and Linux 3.0 build and while working through the instructions in DOC-96451 I noticed that I don't seem to have the file CSF1_1_sha256_4096_65537_v3_usr_crt.pem referenced in the CSF description file. What I do have are the CA1 and SRKx keys as generated by the hab4_pdi_tree script. Did I miss a step or do I need to do something else to get this key file? Thank you.

Michael Robbeloth

ラベル(3)
0 件の賞賛
返信
1 解決策
585件の閲覧回数
michaelrobbelot
Contributor IV

The key_pass.txt file contained test instead of freescale_mx6.

Michael Robbeloth

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
586件の閲覧回数
michaelrobbelot
Contributor IV

The key_pass.txt file contained test instead of freescale_mx6.

Michael Robbeloth

0 件の賞賛
返信