Gstreamer not working second time

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Gstreamer not working second time

ソリューションへジャンプ
25,130件の閲覧回数
gonfer
Contributor V

Hi all,

I've been following this thread gstreamer: video fails to play when opened for second time but as I'm not sure if my problem is the same I'm opening a new one.

My problem is in a iMX28 custom board, and the code I'm running in my application is really trivial:

gst_init (NULL, NULL);

    /* Build the pipeline */

    pipeline = gst_parse_launch ("playbin2 uri=file:///mnt/gonzalo/Copreci-heart_x264_200x120_12000_15fps_320_22050.mp4", NULL);

    /* Start playing */

    gst_element_set_state (pipeline, GST_STATE_PLAYING);

    /* Wait until error or EOS */

    bus = gst_element_get_bus (pipeline);

    msg = gst_bus_timed_pop_filtered (bus, GST_CLOCK_TIME_NONE, GST_MESSAGE_ERROR | GST_MESSAGE_EOS);

    /* Free resources */

    if (msg != NULL)

gst_message_unref(msg);

    gst_object_unref(bus);

    gst_element_set_state(pipeline, GST_STATE_NULL);

    gst_object_unref(pipeline);

    gst_deinit();

First time I run this code in my application everything goes fine, the video is played nicely. Here is the log:

Aiur: 3.0.6

Core: MPEG4PARSER_06.04.27  build on Dec 20 2012 16:48:05

  mime: video/quicktime; audio/x-m4a; application/x-3gp

  file: /usr/lib/imx-mm/parser/lib_mp4_parser_arm9_elinux.so.3.1

Content Info:

        URI:

              file:///mnt/gonzalo/Copreci-heart_x264_200x120_12000_15fps_320_22050.mp4

        Idx File:

              /root/.aiur/.mnt.gonzalo.Copreci-heart_x264_200x120_12000_15fps_320_22050.mp4.ai

              dx

        Seekable  : Yes

        Size(byte): 18666817

Movie Info:

        Seekable  : Yes

        Live      : No

        Duration  : 0:01:41.000000000

        ReadMode  : File

        Track     : 2

Track 00 [video_000000] Enabled

        Duration: 0:01:41.000000000

        Language: eng

        Mime:

              video/x-h264, parsed=(boolean)true, width=(int)200, height=(int)120, framerate=(

              fraction)15/1, codec_data=(buffer)000000016742c00ddb0d11e59610000003001000000301

              e0f142ae0000000168ca8cb2

H264D_ARM9_02.06.01  build on Jul 12 2011 14:01:56.

MFW_GST_H264_DECODER_PLUGIN 3.0.6 build on Feb  5 2014 15:30:55.

Track 01 [audio_000000] Enabled

        Duration: 0:01:40.850000000

        Language: eng

        Mime:

              audio/mpeg, mpegversion=(int)1, framed=(boolean)true, channels=(int)2, rate=(int

              )22050, bitrate=(int)160013

MFW_GST_V4LSINK_PLUGIN 3.0.6 build on Feb  5 2014 15:30:44.

Beep: 3.0.6

Core: MP3 decoder Wrapper  build on Jan 16 2013 16:21:07

  mime: audio/mpeg, mpegversion = (int)1

  file: /usr/lib/imx-mm/audio-codec/wrap/lib_mp3d_wrap_arm9_elinux.so

CODEC: BLN_MAD-MMCODECS_MP3D_ARM_02.13.00_ARM9  build on Dec  5 2012 09:44:32.

>>V4L_SINK: Actually buffer status:

        hardware buffer : 21

        software buffer : 0

full screen size:480x272

[V4L Update Display]: left=0, top=0, width=480, height=272

Running time 0:01:40.940589569 render fps 14.157

Total rendered:1429

[--->FINALIZE aiurdemux

Second time my application runs the same code I get the following error:

(<unknown>:4591): GStreamer-CRITICAL **: gst_element_set_state: assertion `GST_IS_ELEMENT (element)' failed

(<unknown>:4591): GStreamer-CRITICAL **: gst_element_get_bus: assertion `GST_IS_ELEMENT (element)' failed

(<unknown>:4591): GStreamer-CRITICAL **: gst_bus_timed_pop_filtered: assertion `GST_IS_BUS (bus)' failed

(<unknown>:4591): GStreamer-CRITICAL **: gst_object_unref: assertion `object != NULL' failed

(<unknown>:4591): GStreamer-CRITICAL **: gst_element_set_state: assertion `GST_IS_ELEMENT (element)' failed

(<unknown>:4591): GStreamer-CRITICAL **: gst_object_unref: assertion `object != NULL' failed

If I restart my application, the previous code runs fine but once again, only the first time. I've also tried running the same code from a CHILD process. Doing it this way, the code DOESN'T FAIL, so looks something is not de-initializing properly. But in my application I don't want to run it in a child process, and would like to know what's wrong in this code.

Can someone help me?

Thanks in advance,

Gonzalo.

タグ(2)
0 件の賞賛
1 解決策
11,058件の閲覧回数
PeterChan
NXP Employee
NXP Employee

Hi Gonzalo,

I have attached the libmfw_gst_v4lsink.so extracted from the MM codec package 3.0.11. Please use this library file to replace the one in your rootfs. After the change, the repeat mode can work for your H.264 test vectors.

Thanks,

Peter

元の投稿で解決策を見る

0 件の賞賛
58 返答(返信)
3,682件の閲覧回数
PeterChan
NXP Employee
NXP Employee

According to Multimedia Feature Matrix, the maximum resolution of H.264 video decoding is 320 x 240  @ 30 fps in base profile.

3.   Video Codec Spec

Feature

Profile

Max Resolution

Min Resolution

Max Framerate

H/W or S/W

Comments

Implementation

Video

Decoder

MPEG4

SP

320*240

16 * 16

30 fps

S/W

Support H263BP

H.264

BP

320*240

16 * 16

30 fps

S/W

Video outside this specification may have unexpected behavior. Would you please transcode the H.264 video to 320*240 base profile and try again?

0 件の賞賛
3,682件の閲覧回数
YixingKong
Senior Contributor IV

Peter, do you think this DI can be closed or further action is needed?

Thanks,

Yixing

0 件の賞賛
3,682件の閲覧回数
PeterChan
NXP Employee
NXP Employee

Yixing,

Please keep this DI open since we are still debugging the root cause.

Thanks,

Peter

0 件の賞賛
3,682件の閲覧回数
gonfer
Contributor V

Hi Peter,

yes, I already knew the video codec specs.

And I've already done tens of tests using 320x240, 240x136 and lower resolutions, and found same results: MPEG4 performs much better than H.264, and it's hard to get a file with H.264 encoding that shows the [--->FINALIZE v4l_sink message at the end of every repetition (most of them don't play the second time).


Thanks,

Gonzalo.

0 件の賞賛
11,059件の閲覧回数
PeterChan
NXP Employee
NXP Employee

Hi Gonzalo,

I have attached the libmfw_gst_v4lsink.so extracted from the MM codec package 3.0.11. Please use this library file to replace the one in your rootfs. After the change, the repeat mode can work for your H.264 test vectors.

Thanks,

Peter

0 件の賞賛
3,682件の閲覧回数
gonfer
Contributor V

Hi Peter,

I've had a chance to work on this again after holidays, and it looks you found the solution !!!

Now it works fine for every repetition, using libmfw_gst_v4lsink.so from MM codec package 3.0.11 and the patched gplay. I've tried many mp4 files that previously showed this problem, and even files out of specification (> 320x240) are playing fine.


Thanks a lot for your work !!!!!!


Please, could you point me to a tarball or repository with MM codec package 3.0.11 to integrate in my current Ltib??


Thanks,

Gonzalo.

0 件の賞賛
3,682件の閲覧回数
PeterChan
NXP Employee
NXP Employee

Hi Gonzalo,

You can get the MM codec package 3.0.11 at Freescale Yocto mirror site

http://www.freescale.com/lgfiles/NMG/MAD/YOCTO//gst-fsl-plugins-3.0.11.tar.gz

Thanks,

Peter

3,682件の閲覧回数
gonfer
Contributor V

Once again, thanks a lot Peter !!!

I was getting insane looking into the Yocto recipes for a repository. But I've noticed there are 2 patches in Yocto:

- build-Fix-out-of-tree-build.patch

- Remove-use-of-obsolete-VIDIOC_DBG_G_CHIP_IDENT.patch

How do you build the MM codec package? Under Ltib? If so, could you share your spec file?

Thanks,

Gonzalo

0 件の賞賛
3,682件の閲覧回数
gonfer
Contributor V

I've found an issue while trying to compile fsl MM codec package 3.0.11:

.....

aiurdemux.c: In function 'aiurdemux_callback_getflag_pull':

aiurdemux.c:735:21: error: 'FILE_FLAG_NON_SEEKABLE' undeclared (first use in this function)

aiurdemux.c:735:21: note: each undeclared identifier is reported only once for each function it appears in

aiurdemux.c:736:21: error: 'FILE_FLAG_READ_IN_SEQUENCE' undeclared (first use in this function)

aiurdemux.c: In function 'aiurdemux_callback_getflag_push':

aiurdemux.c:893:21: error: 'FILE_FLAG_NON_SEEKABLE' undeclared (first use in this function)

aiurdemux.c:894:21: error: 'FILE_FLAG_READ_IN_SEQUENCE' undeclared (first use in this function)

aiurdemux.c: In function 'aiurdemux_loop_state_init':

aiurdemux.c:2320:14: error: 'FslFileStream' has no member named 'GetFlag'

aiurdemux.c:2330:14: error: 'FslFileStream' has no member named 'GetFlag'

aiurdemux.c: In function 'aiurdemux_parse_audio':

aiurdemux.c:3161:10: error: 'AUDIO_EC3' undeclared (first use in this function)

.......

It looks like the compiler is looking for these header files:

<ltib_dir>/rootfs/usr/include/imx-mm/parser/fsl_parser.h

<ltib_dir>/rootfs/usr/include/imx-mm/parser/fsl_media_types.h

<ltib_dir>/rootfs/usr/include/imx-mm/parser/fsl_types.h

and if they exist from a previous package (in my case, from 3.0.6) then compilation fails.

If these files are removed then compilation is succesfull but the new header files are NOT installed in <ltib_dir>/rootfs/usr/include/imx-mm/parser/ so a better workaround is to replace the OLD header files in <ltib_dir>/rootfs/usr/include/imx-mm/parser/ with the NEW header files from <ltib_dir>/rpm/BUILD/gst-fsl-plugins-3.0.11/inc/core_lib/parser

I don't know the root cause of this issue but this dirty-fix works fine. Now I have my custom board running  fsl MM codec package 3.0.11 under Ltib.

It would be nice if someone could take care of this problem and find a fix because (probably) more header files should be updated in the RFS.


Thanks,

Gonzalo.

0 件の賞賛
3,685件の閲覧回数
PeterChan
NXP Employee
NXP Employee

Hi Gonzalo,

The compile error is caused by the header file differences between libfslparser-3.0.6 and libfslparser-3.0.11. The proper way to resolve these errors is to get the libfslparser-3.0.11 & libfslcodec-3.0.11 and install them to the device rootfs. Unfortunately, both libraries are released in binary format (not tar.gz anymore) and there is no simple way to extract them. The method I use is to install and build the BSP L3.10.17 and locate their source from the working directory. Then, tarball the source with the appropriate filename and version and copy them to /var.tmp/pkgs. Finally,in LTIB install the libfslcodec-3.0.11, libfslparser-3.0.11 and then build the gst-fsl-plugins-3.0.11.

Hope you understand that I can't post the MM codec 3.0.11 here without license agreement/disclaimer.

Thanks,

Peter

3,685件の閲覧回数
gonfer
Contributor V

Hi Peter,

thanks for the tip. I've done as you suggested and compilation is successful.

Thanks,

Gonzalo

0 件の賞賛
3,683件の閲覧回数
dmitryfedotov
Contributor II

try to delete frescale codecs and use remaning.

0 件の賞賛
3,683件の閲覧回数
gonfer
Contributor V

Hi Dmitry,

when removing the Freescale's codecs I'm not able to get gplay running with the remaining ones in L2.6.35_1.1.0_130130_images_MX28.

But, please, see 9th post in this thread:

- vdqueue = gst_element_factory_make ("queue", "video-queue");

- vdsink = gst_element_factory_make ("mfw_v4lsink", "video-sink");

+ vdqueue = gst_element_factory_make ("ffmpegcolorspace", "video-queue");

+ vdsink = gst_element_factory_make ("fbdevsink", "video-sink");

If I use fbdevsink instead of mfw_v4lsink, then everything works fine (with a nearly 100% CPU load).

The probelm is that i need mfw_v4lsink, because it uses the PXP driver, and I need to use that driver to implement HW overlaying

Thanks,

Gonzalo.

0 件の賞賛
3,683件の閲覧回数
dmitryfedotov
Contributor II

attempt to play video without gplay. gstreamer can do it.

0 件の賞賛
3,683件の閲覧回数
dmitryfedotov
Contributor II

try to use yocto build system instead ltib.

gstreamer-0.10 via webkit doesn't play video on i.mx6 (yocto master, webkit-5.1.1) this link may help to you.

0 件の賞賛
3,693件の閲覧回数
gonfer
Contributor V

I've been trying to dig on this issue and it looks gst_deinit(); does not rewind everything done in gst_init(NULL,NULL);

So I've modified the previous code calling only once to gst_init(NULL,NULL); and removing the call to gst_deinit(); (like in the gstreamer SDK examples)

The result is the same (1st time OK, next time KO), but the problem is different. I've been comparing logs with different gstreamer debug levels, and it looks the problem is related to mfw_v4lsink.

Attached are the logs for the first and second run, with GST_DEBUG=mfw_v4lsink:5

This is extracted from the log of the first run:

.............

H264D_ARM9_02.06.01  build on Jul 12 2011 14:01:56.

MFW_GST_H264_DECODER_PLUGIN 3.0.6 build on Feb  5 2014 15:30:55.

Track 01 [audio_000000] Enabled

    Duration: 0:01:40.850000000

    Language: eng

    Mime:

          audio/mpeg, mpegversion=(int)1, framed=(boolean)true, channels=(int)2, rate=(int

          )22050, bitrate=(int)160013

0:00:01.392187502  1250   0x6eaa70 INFO             mfw_v4lsink mfw_gst_v4lsink.c:262:mfw_gst_get_first_odev: Get first device:/dev/video0, capabilities 0x4000202

0:00:01.393125002  1250   0x6eaa70 INFO             mfw_v4lsink mfw_gst_v4lsink.c:300:mfw_gst_v4l2sink_query_support_formats: supported format:[RGB3]24-bit RGB

0:00:01.393562502  1250   0x6eaa70 INFO             mfw_v4lsink mfw_gst_v4lsink.c:300:mfw_gst_v4l2sink_query_support_formats: supported format:[RGBP]16-bit RGB 5:6:5

0:00:01.393968752  1250   0x6eaa70 INFO             mfw_v4lsink mfw_gst_v4lsink.c:300:mfw_gst_v4l2sink_query_support_formats: supported format:[RGBO]16-bit RGB 5:5:5

0:00:01.394343752  1250   0x6eaa70 INFO             mfw_v4lsink mfw_gst_v4lsink.c:300:mfw_gst_v4l2sink_query_support_formats: supported format:[YU12]YUV 4:2:0 Planar

0:00:01.394718752  1250   0x6eaa70 INFO             mfw_v4lsink mfw_gst_v4lsink.c:300:mfw_gst_v4l2sink_query_support_formats: supported format:[422P]YUV 4:2:2 Planar

MFW_GST_V4LSINK_PLUGIN 3.0.6 build on Feb  5 2014 15:30:44.

0:00:01.404687502  1250   0x6eaa70 DEBUG            mfw_v4lsink mfw_gst_v4lsink.c:1469:mfw_gst_v4lsink_change_state: 

>>V4LSINK: State: 10

0:00:01.427281251  1250   0x6eaa70 DEBUG            mfw_v4lsink mfw_gst_v4lsink.c:1469:mfw_gst_v4lsink_change_state: 

>>V4LSINK: State: 19

0:00:02.205875000  1250   0x6ab1e8 DEBUG            mfw_v4lsink mfw_gst_v4lsink.c:2003:mfw_gst_v4lsink_buffer_alloc: crop_left_bypixel=16

0:00:02.213250000  1250   0x6ab1e8 DEBUG            mfw_v4lsink mfw_gst_v4lsink.c:2004:mfw_gst_v4lsink_buffer_alloc: crop_top_by_pixel=16

0:00:02.215937501  1250   0x6ab1e8 DEBUG            mfw_v4lsink mfw_gst_v4lsink.c:2005:mfw_gst_v4lsink_buffer_alloc: crop_right_bypixel=24

0:00:02.216343751  1250   0x6ab1e8 DEBUG            mfw_v4lsink mfw_gst_v4lsink.c:2006:mfw_gst_v4lsink_buffer_alloc: crop_bottom_by_pixel=24

0:00:02.216687501  1250   0x6ab1e8 DEBUG            mfw_v4lsink mfw_gst_v4lsink.c:2016:mfw_gst_v4lsink_buffer_alloc: aspectratio_n=1

0:00:02.217000001  1250   0x6ab1e8 DEBUG            mfw_v4lsink mfw_gst_v4lsink.c:2017:mfw_gst_v4lsink_buffer_alloc: aspectratio_d=1

0:00:02.217343751  1250   0x6ab1e8 DEBUG            mfw_v4lsink mfw_gst_v4lsink.c:2019:mfw_gst_v4lsink_buffer_alloc: Decoded Width = 240, Decoded Height = 160

0:00:02.219250001  1250   0x6ab1e8 DEBUG            mfw_v4lsink mfw_gst_v4lsink.c:2031:mfw_gst_v4lsink_buffer_alloc: Decoder maximal reserved 21 buffers.

0:00:02.219656251  1250   0x6ab1e8 DEBUG            mfw_v4lsink mfw_gst_v4lsink.c:2065:mfw_gst_v4lsink_buffer_alloc: Decoder maximal support 127 buffers.

0:00:02.220562501  1250   0x6ab1e8 INFO             mfw_v4lsink mfw_gst_v4lsink.c:262:mfw_gst_get_first_odev: Get first device:/dev/video0, capabilities 0x4000202

0:00:02.221093751  1250   0x6ab1e8 ERROR            mfw_v4lsink mfw_gst_v4l.c:825:mfw_gst_v4l2_set_rotation: set ctrl failed

0:00:02.221656251  1250   0x6ab1e8 LOG              mfw_v4lsink mfw_gst_v4l.c:931:mfw_gst_v4l2_output_setup: 21 hwbuffers sucessfully allocated.

0:00:02.222093751  1250   0x6ab1e8 ERROR            mfw_v4lsink mfw_gst_v4l.c:1213:mfw_gst_v4l2_set_fmt: Set frame sucessfully

>>V4L_SINK: Actually buffer status:

    hardware buffer : 21

    software buffer : 0

Beep: 3.0.6 

.............

and this is from the log of the second run:

.............

H264D_ARM9_02.06.01  build on Jul 12 2011 14:01:56.

MFW_GST_H264_DECODER_PLUGIN 3.0.6 build on Feb  5 2014 15:30:55.

Track 01 [audio_000000] Enabled

    Duration: 0:01:40.850000000

    Language: eng

    Mime:

          audio/mpeg, mpegversion=(int)1, framed=(boolean)true, channels=(int)2, rate=(int

          )22050, bitrate=(int)160013

MFW_GST_V4LSINK_PLUGIN 3.0.6 build on Feb  5 2014 15:30:44.

0:01:49.693843752  1250   0x118390 DEBUG            mfw_v4lsink mfw_gst_v4lsink.c:1469:mfw_gst_v4lsink_change_state: 

>>V4LSINK: State: 10

0:01:49.711218752  1250   0x118390 DEBUG            mfw_v4lsink mfw_gst_v4lsink.c:1469:mfw_gst_v4lsink_change_state: 

>>V4LSINK: State: 19

0:01:50.285562501  1250   0x71ff38 DEBUG            mfw_v4lsink mfw_gst_v4lsink.c:2003:mfw_gst_v4lsink_buffer_alloc: crop_left_bypixel=16

0:01:50.286031251  1250   0x71ff38 DEBUG            mfw_v4lsink mfw_gst_v4lsink.c:2004:mfw_gst_v4lsink_buffer_alloc: crop_top_by_pixel=16

0:01:50.289625001  1250   0x71ff38 DEBUG            mfw_v4lsink mfw_gst_v4lsink.c:2005:mfw_gst_v4lsink_buffer_alloc: crop_right_bypixel=24

0:01:50.291343751  1250   0x71ff38 DEBUG            mfw_v4lsink mfw_gst_v4lsink.c:2006:mfw_gst_v4lsink_buffer_alloc: crop_bottom_by_pixel=24

0:01:50.293593751  1250   0x71ff38 DEBUG            mfw_v4lsink mfw_gst_v4lsink.c:2016:mfw_gst_v4lsink_buffer_alloc: aspectratio_n=1

0:01:50.294812501  1250   0x71ff38 DEBUG            mfw_v4lsink mfw_gst_v4lsink.c:2017:mfw_gst_v4lsink_buffer_alloc: aspectratio_d=1

0:01:50.296593751  1250   0x71ff38 DEBUG            mfw_v4lsink mfw_gst_v4lsink.c:2019:mfw_gst_v4lsink_buffer_alloc: Decoded Width = 240, Decoded Height = 160

0:01:50.298562501  1250   0x71ff38 DEBUG            mfw_v4lsink mfw_gst_v4lsink.c:2031:mfw_gst_v4lsink_buffer_alloc: Decoder maximal reserved 21 buffers.

0:01:50.298968751  1250   0x71ff38 DEBUG            mfw_v4lsink mfw_gst_v4lsink.c:2065:mfw_gst_v4lsink_buffer_alloc: Decoder maximal support 127 buffers.

0:01:50.302437500  1250   0x71ff38 ERROR            mfw_v4lsink mfw_gst_v4l.c:619:mfw_gst_v4l2_open: Unable to open 

0:01:50.302843750  1250   0x71ff38 ERROR            mfw_v4lsink mfw_gst_v4l.c:825:mfw_gst_v4l2_set_rotation: set ctrl failed

0:01:50.303187500  1250   0x71ff38 ERROR            mfw_v4lsink mfw_gst_v4l.c:861:mfw_gst_v4l2_pxp_set_color: set ctrl 134217729 failed

0:01:50.303500000  1250   0x71ff38 ERROR            mfw_v4lsink mfw_gst_v4l.c:869:mfw_gst_v4l2_pxp_set_color: set ctrl 134217730 failed

0:01:50.303875000  1250   0x71ff38 ERROR            mfw_v4lsink mfw_gst_v4l.c:907:mfw_gst_v4l2_output_setup: set format failed 1

0:01:50.304218750  1250   0x71ff38 ERROR            mfw_v4lsink mfw_gst_v4l.c:1197:mfw_gst_v4l2_set_fmt: Error in mfw_gst_v4lsink_output_setup

VIDIOC_S_FMT output overlay: Bad file descriptor

>>V4L_SINK: Actually buffer status:

    hardware buffer : 21

    software buffer : 0

0:01:50.305218750  1250   0x71ff38 ERROR            mfw_v4lsink mfw_gst_v4l_buffer.c:490:mfw_gst_v4l2_new_hwbuffer: VIDIOC_QUERYBUF failed 0, device id:-1,  err:Bad file descriptor

Beep: 3.0.6 

.............

Major differences are marked in RED. The problem looks to be related with the second time /dev/video0 is opened.

Please, can someone point me how to continue debugging this?

Thanks,

Gonzalo.

0 件の賞賛
3,693件の閲覧回数
LeonardoSandova
Specialist I

Hi Gonzalo,

there is a long time I dont write a GST app, but at some point your code needs to run a loop:

/* Set the pipeline to "playing" state*/

  g_print ("Now playing: %s\n", argv[1]);

  gst_element_set_state (pipeline, GST_STATE_PLAYING);

  /* Iterate */

  g_print ("Running...\n");

  g_main_loop_run (loop);

  /* Out of the main loop, clean up nicely */

  g_print ("Returned, stopping playback\n");

  gst_element_set_state (pipeline, GST_STATE_NULL);

  g_print ("Deleting pipeline\n");

  gst_object_unref (GST_OBJECT (pipeline));

  g_source_remove (bus_watch_id);

  g_main_loop_unref (loop);

Do you have it this way?

0 件の賞賛
3,693件の閲覧回数
gonfer
Contributor V

Hi Leonardo, and thanks for answering !!!


You are right, there is no loop in my code.


I'm new to gstreamer and am following the examples in the SDK.

Basic tutorial 1: Hello World http://docs.gstreamer.com/pages/viewpage.action?pageId=327735

Basic tutorial 3: Dynamic pipelines http://docs.gstreamer.com/display/GstSDK/Basic+tutorial+3%3A+Dynamic+pipelines

and neither of them perform a glib main loop. They simply block on gst_bus_timed_pop_filtered just waiting for a message of the selected type to appear. Unfortunately, the code of both tutorials runs fine only for the first time (I haven't compared logs for tutorial #3, as I'm concentrating in tutorial #1 just for simplicity).

Thanks,

Gonzalo.

0 件の賞賛
3,693件の閲覧回数
gonfer
Contributor V

I've been trying to look for the reason of this error   VIDIOC_S_FMT output overlay: Bad file descriptor in my second post.

I've added printks to the PXP driver (mxs_pxp.c) in:

  • pxp_open: showing  pxp->users before opening, and showing an error message if the driver returns EBUSY (pxp->users > 1)
  • pxp_close: showing pxp->users before closening.

This is the log I get for the first run:

Aiur: 3.0.6

Core: MPEG4PARSER_06.04.27 build on Dec 20 2012 16:48:05

  mime: video/quicktime; audio/x-m4a; application/x-3gp

  file: /usr/lib/imx-mm/parser/lib_mp4_parser_arm9_elinux.so.3.1

Content Info:

  URI:

file:///mnt/gonzalo/Copreci-heart_x264_200x120_12000_15fps_320_22050.mp4

  Idx File:

/root/.aiur/.mnt.gonzalo.Copreci-heart_x264_200x120_12000_15fps_320_22050.mp4.ai

  dx

  Seekable : Yes

  Size(byte): 18666817

Movie Info:

  Seekable : Yes

  Live : No

  Duration : 0:01:41.000000000

  ReadMode : File

  Track : 2

Track 00 [video_000000] Enabled

  Duration: 0:01:41.000000000

  Language: eng

  Mime:

  video/x-h264, parsed=(boolean)true, width=(int)200, height=(int)120, framerate=(

  fraction)15/1, codec_data=(buffer)000000016742c00ddb0d11e59610000003001000000301

  e0f142ae0000000168ca8cb2

H264D_ARM9_02.06.01 build on Jul 12 2011 14:01:56.

MFW_GST_H264_DECODER_PLUGIN 3.0.6 build on Feb 5 2014 15:30:55.

Track 01 [audio_000000] Enabled

  Duration: 0:01:40.850000000

  Language: eng

  Mime:

  audio/mpeg, mpegversion=(int)1, framed=(boolean)true, channels=(int)2, rate=(int

  )22050, bitrate=(int)160013

[ 4577.800000] [pxp_open] pxp->users = 0

[ 4577.810000] [pxp_close] pxp->users = 1

MFW_GST_V4LSINK_PLUGIN 3.0.6 build on Feb 5 2014 15:30:44.

[ 4578.640000] [pxp_open] pxp->users = 0

>>V4L_SINK: Actually buffer status:

  hardware buffer : 21

  software buffer : 0

Beep: 3.0.6

Core: MP3 decoder Wrapper build on Jan 16 2013 16:21:07

  mime: audio/mpeg, mpegversion = (int)1

  file: /usr/lib/imx-mm/audio-codec/wrap/lib_mp3d_wrap_arm9_elinux.so

CODEC: BLN_MAD-MMCODECS_MP3D_ARM_02.13.00_ARM9 build on Dec 5 2012 09:44:32.

full screen size:480x272

[V4L Update Display]: left=0, top=0, width=480, height=272

Running time 0:01:40.943310657 render fps 14.226

Total rendered:1436

[--->FINALIZE aiurdemux

and this is the log for the second run:

Aiur: 3.0.6

Core: MPEG4PARSER_06.04.27 build on Dec 20 2012 16:48:05

  mime: video/quicktime; audio/x-m4a; application/x-3gp

  file: /usr/lib/imx-mm/parser/lib_mp4_parser_arm9_elinux.so.3.1

Content Info:

  URI:

file:///mnt/gonzalo/Copreci-heart_x264_200x120_12000_15fps_320_22050.mp4

  Idx File:

/root/.aiur/.mnt.gonzalo.Copreci-heart_x264_200x120_12000_15fps_320_22050.mp4.ai

  dx

  Seekable : Yes

  Size(byte): 18666817

Movie Info:

  Seekable : Yes

  Live : No

  Duration : 0:01:41.000000000

  ReadMode : File

  Track : 2

Track 00 [video_000000] Enabled

  Duration: 0:01:41.000000000

  Language: eng

  Mime:

  video/x-h264, parsed=(boolean)true, width=(int)200, height=(int)120, framerate=(

  fraction)15/1, codec_data=(buffer)000000016742c00ddb0d11e59610000003001000000301

  e0f142ae0000000168ca8cb2

H264D_ARM9_02.06.01 build on Jul 12 2011 14:01:56.

MFW_GST_H264_DECODER_PLUGIN 3.0.6 build on Feb 5 2014 15:30:55.

Track 01 [audio_000000] Enabled

  Duration: 0:01:40.850000000

  Language: eng

  Mime:

  audio/mpeg, mpegversion=(int)1, framed=(boolean)true, channels=(int)2, rate=(int

  )22050, bitrate=(int)160013

MFW_GST_V4LSINK_PLUGIN 3.0.6 build on Feb 5 2014 15:30:44.

[ 4680.520000] [pxp_open] pxp->users = 1

[ 4680.520000] [pxp_open] -> Returning -EBUSY

VIDIOC_S_FMT output overlay: Bad file descriptor

>>V4L_SINK: Actually buffer status:

  hardware buffer : 21

  software buffer : 0

Beep: 3.0.6

Core: MP3 decoder Wrapper build on Jan 16 2013 16:21:07

  mime: audio/mpeg, mpegversion = (int)1

  file: /usr/lib/imx-mm/audio-codec/wrap/lib_mp3d_wrap_arm9_elinux.so

CODEC: BLN_MAD-MMCODECS_MP3D_ARM_02.13.00_ARM9 build on Dec 5 2012 09:44:32.

[ 4681.550000] [pxp_open] pxp->users = 1

[ 4681.550000] [pxp_open] -> Returning -EBUSY


After first run /dev/video0 is not closed so when /dev/video0 is re-open in the second run the driver returns EBUSY and mfw_v4lsink fails.

I don't know how to continue debugging this issue so the question is, why /dev/video0 is not closed when the pipeline is unreferenced?

Thanks,

Gonzalo.

0 件の賞賛
3,693件の閲覧回数
LeonardoSandova
Specialist I

For some reason the playbin2 elements are not de-initializing completely, so reopening a device is causing an error. You may try this hello-world app and see if you find the same issue:

http://gstreamer.freedesktop.org/data/doc/gstreamer/head/manual/html/chapter-helloworld.html

Also, take at look at the gst-launch source code.

0 件の賞賛
3,693件の閲覧回数
gonfer
Contributor V

Hi Leonardo,

I don't know if you want me just to run the audio-player of the hello-world app or run my video getting rid of playbin2.

As I cannot confirm a complete de-initialisation of the audio player, I've done the second one using mfw_v4lsink, based on this code: All Boards Creating App Video

My code looks as follows:

===============================================================================================================

void on_pad_added (GstElement *element, GstPad *pad){

    g_debug ("Signal: pad-added");

    GstCaps *caps;

    GstStructure *str;

    caps = gst_pad_get_caps (pad);

    g_assert (caps != NULL);

    str = gst_caps_get_structure (caps, 0);

    g_assert (str != NULL);

    printf("STR[%s]\n", gst_structure_get_name (str));

    if (g_strrstr (gst_structure_get_name (str), "video")) {

        g_debug ("Linking video pad to dec_vd");

        // Link it actually

        GstPad *targetsink = gst_element_get_pad (decvd, "sink");

        g_assert (targetsink != NULL);

        gst_pad_link (pad, targetsink);

        gst_object_unref (targetsink);

    }

    if (g_strrstr (gst_structure_get_name (str), "audio")) {

        g_debug ("Linking audio pad to dec_ad");

        // Link it actually

        GstPad *targetsink = gst_element_get_pad (decad, "sink");

        g_assert (targetsink != NULL);

        gst_pad_link (pad, targetsink);

        gst_object_unref (targetsink);

    }

    gst_caps_unref (caps);

}

static gboolean bus_call (GstBus *bus, GstMessage *msg, gpointer data){

    GMainLoop *loop = (GMainLoop *) data;

    gchar  *debug;

    GError *error;

    switch (GST_MESSAGE_TYPE (msg)) {

        case GST_MESSAGE_EOS:

            g_print ("End of stream\n");

            g_main_loop_quit (loop);

            break;

        case GST_MESSAGE_ERROR:

            gst_message_parse_error (msg, &error, &debug);

            g_free (debug);

            g_printerr ("Error: %s\n", error->message);

            g_error_free (error);

            g_main_loop_quit (loop);

            break;

        default:

            break;

    }

    return TRUE;

}

int play_video (char* video_file){

GMainLoop *loop;

GstElement *pipeline;

GstBus *bus;

static int init = 1;

    loop = g_main_loop_new (NULL, FALSE);

    /* Create gstreamer elements */

    pipeline    = gst_pipeline_new ("media-player");

    source        = gst_element_factory_make ("filesrc",                "file-source");

    fqueue        = gst_element_factory_make ("multiqueue",            "file-queue");

    demuxer        = gst_element_factory_make ("qtdemux",                "avi-demuxer");

    decvd        = gst_element_factory_make ("mfw_h264decoder",         "video-decoder");

    vdqueue        = gst_element_factory_make ("queue",                  "video-queue");

    vdsink        = gst_element_factory_make ("mfw_v4lsink",            "video-sink");

    decad        = gst_element_factory_make ("mfw_mp3decoder",        "audio-decoder");

    adqueue        = gst_element_factory_make ("queue",                "audio-queue");

    adconv        = gst_element_factory_make ("audioconvert",            "audio-converter");

    adresamp    = gst_element_factory_make ("audioresample",           "audio-resampler");

    adsink        = gst_element_factory_make ("alsasink",               "audio-sink");            // "autoaudiosink"

    if (!pipeline)     {g_printerr ("Error: [pipeline] could not be created. Exiting.\n");        return -1;}

    if (!source)     {g_printerr ("Error: [source] could not be created. Exiting.\n");        return -1;}

    if (!fqueue)     {g_printerr ("Error: [fqueue] could not be created. Exiting.\n");        return -1;}

    if (!demuxer)     {g_printerr ("Error: [demuxer] could not be created. Exiting.\n");        return -1;}

    if (!decvd)     {g_printerr ("Error: [decvd] could not be created. Exiting.\n");        return -1;}

    if (!vdqueue)     {g_printerr ("Error: [vdqueue] could not be created. Exiting.\n");        return -1;}

    if (!vdsink)     {g_printerr ("Error: [vdsink] could not be created. Exiting.\n");        return -1;}

    if (!decad)     {g_printerr ("Error: [decad] could not be created. Exiting.\n");        return -1;}

    if (!adqueue)     {g_printerr ("Error: [adqueue] could not be created. Exiting.\n");        return -1;}

    if (!adconv)     {g_printerr ("Error: [adconv] could not be created. Exiting.\n");        return -1;}

    if (!adresamp)     {g_printerr ("Error: [adresamp] could not be created. Exiting.\n");        return -1;}

    if (!adsink)     {g_printerr ("Error: [adsink] could not be created. Exiting.\n");        return -1;}

    /* Set up the pipeline */

    /* we set the input filename to the source element */

    g_object_set (G_OBJECT (source), "location", video_file, NULL);

    /* we add a message handler */

    bus = gst_pipeline_get_bus (GST_PIPELINE (pipeline));

    gst_bus_add_watch (bus, bus_call, loop);

    gst_object_unref (bus);

    /* we add all elements into the pipeline */

    /* file-source | ogg-demuxer | vorbis-decoder | converter | alsa-output */

    gst_bin_add_many (GST_BIN (pipeline), source, fqueue, demuxer, decvd, vdqueue, vdsink, decad, adqueue, adconv, adresamp, adsink, NULL);

    /* we link the elements together */

    if (!gst_element_link (source,  fqueue))    {g_printerr ("Error: unable to link [source <> fqueue]. Exiting.\n");        return -1;}

    if (!gst_element_link (fqueue,  demuxer))    {g_printerr ("Error: unable to link [fqueue <> demuxer]. Exiting.\n");        return -1;}

    if (!gst_element_link (decvd,   vdqueue))    {g_printerr ("Error: unable to link [decvd <> vdqueue]. Exiting.\n");        return -1;}

    if (!gst_element_link (vdqueue, vdsink))    {g_printerr ("Error: unable to link [vdqueue <> vdsink]. Exiting.\n");        return -1;}

    if (!gst_element_link (decad,    adqueue))    {g_printerr ("Error: unable to link [decad <> adqueue]. Exiting.\n");        return -1;}

    if (!gst_element_link (adqueue,  adconv))    {g_printerr ("Error: unable to link [adqueue <> adconv]. Exiting.\n");        return -1;}

    if (!gst_element_link (adconv,   adresamp))    {g_printerr ("Error: unable to link [adconv <> adresamp]. Exiting.\n");        return -1;}

    if (!gst_element_link (adresamp, adsink))    {g_printerr ("Error: unable to link [adresamp <> adsink]. Exiting.\n");        return -1;}

    g_signal_connect (demuxer, "pad-added", G_CALLBACK (on_pad_added), NULL);

    /* note that the demuxer will be linked to the decoder dynamically.

        The reason is that Ogg may contain various streams (for example

        audio and video). The source pad(s) will be created at run time,

        by the demuxer when it detects the amount and nature of streams.

        Therefore we connect a callback function which will be executed

        when the "pad-added" is emitted.*/

    /* Set the pipeline to "playing" state*/

    g_print ("Now playing: %s\n", video_file);

    gst_element_set_state (pipeline, GST_STATE_PLAYING);

    /* Iterate */

    g_print ("Running...\n");

    g_main_loop_run (loop);

    /* Out of the main loop, clean up nicely */

    g_print ("Returned, stopping playback\n");

    gst_element_set_state (pipeline, GST_STATE_NULL);

    g_print ("Deleting pipeline\n");

    gst_object_unref (GST_OBJECT (pipeline));

    return 0;

}

int main (int  argc, char *argv[]){

    gst_init (NULL, NULL);

    while(1){

        play_video("/mnt/gonzalo/Copreci-heart_x264_200x120_12000_15fps_320_22050.mp4");

    }

    return -1;

}

===============================================================================================================

As in my previous tests using playbin2 , this code runs fine only for the first time. /dev/video0 remains open for ever and in the second run the driver returns EBUSY and mfw_v4lsink fails.

Thanks,

Gonzalo.

0 件の賞賛